Accommodations near Braunau

Accommodations near Braunau

Lodging

Website

Distance to seminar location

Sovea Hotel Braunau

www.sovea.at

0.1 km

Schüdlbauers Hotel

www.schuedlbauers.at

1.5 km

Hotel Gann

www.hotelgann.at

1.9 km

Das alte Gefängnis (the old prison)

www.dasaltegefaengnis.at

1.9 km

Schlosstaverne restaurant

www.pommers-schlosstaverne.at

2.3 km

Old town hotel Mayrbräu

www.mayrbraeu.at

2.4 km

Hotel am Theaterpark

www.hotel-neussl.at

2.4 km

Pension Göttler

www.goettler-simbach.de

4.9 km

Pension Moosbräu

www.moosbraeu.de

5.1 km

Motel Inn

www.motelinn.de

5.3 km

Interesting information about the region

Interesting information about the region

The Innviertel region is located in the northwest part of Upper Austria and includes the districts Braunau am Inn, Ried im Innkreis and Schärding. Unlike the rest of Upper Austria, this region was mostly part of Bavaria up until 1779 (Treaty of Teschen). Referring to this region as the Innviertel is something that is relatively new (before it was commonly called Innbaiern). The new term was created by the Austrian government after annexation in 1779, which also divided the territory into four quartersSee also: en.wikipedia.org/wiki/Innviertel. More information about this is available here:

http://www.innviertel-tourismus.at

Event address and organizers

Event address and organizers

The B&R summer workshop takes place annually at the HTBLA Braunau.

Event location

Organizer

HTLBA Braunau/Inn

Osternbergerstrasse 55

5280 Braunau

Austria

B&R Industrial Automation GmbH

B&R Strasse 1

5142 Eggelsberg

+43(0)7748/6586-0

Wybierz kraj i język

B&R Logo