DWL@DWL10000087531
Verze | Jazyk | Operační systém | Datum | Velikost | Typ | Stáhnout |
---|---|---|---|---|---|---|
2.3 | DE | WinCE5x, WinCE6x | 09.10.2013 | 712 KB | ZIP | BrTaskMan_CE_D_V2_3.zip |
2.3 | EN | WinCE5x, WinCE6x | 09.10.2013 | 709 KB | ZIP | BrTaskMan_CE_E_V2_3.zip |
Popis |
Task Manager With the B&R Task Manager you can display information about running programs, processes and services, the system performance and network load on a B&R device with Windows CE. Additionally you can terminate programs and processes and start and stop services. ********************************************** The B&R Task Manager runs only on B&R devices! ********************************************** ---------------------------------------------------------------- Version 2.3 / 2013-08-16 ---------------------------------------------------------------- Changes - Tab "Devices" shows also the power state of the devices. - The "Threads" dialog shows also the name of the current process, where the tread is running (marked with ! if this is not the owner process). - The Task Manager runs in trial mode (60 minutes) on non-B&R devices. Fixes - The Windows CE 5.0 version required the complete remaining CPU time to calculate the CPU usage in percent. Remark: This time was not taken into account for the CPU usage. |
|||||
Verze | Jazyk | Operační systém | Datum | Velikost | Typ | Stáhnout |
2.1.3 | DE | WinCE5x, WinCE6x | 04.07.2011 | 731 KB | ZIP | BrTaskMan_CE_D_V2_1_3.zip |
2.1.3 | EN | WinCE5x, WinCE6x | 04.07.2011 | 729 KB | ZIP | BrTaskMan_CE_E_V2_1_3.zip |
Popis |
Task Manager With the B&R Task Manager you can display information about running programs, processes and services, the system performance and network load, terminate programs and processes and start and stop services on a B&R device with Windows CE. |
|||||
Verze | Jazyk | Operační systém | Datum | Velikost | Typ | Stáhnout |
2.1 | DE | WinCE5x, WinCE6x | 14.04.2010 | 730 KB | ZIP | BrTaskMan_CE_D_V2_1.zip |
2.1 | EN | WinCE5x, WinCE6x | 14.04.2010 | 728 KB | ZIP | BrTaskMan_CE_E_V2_1.zip |
Popis |
Task Manager With the B&R Task Manager you can display information about running programs, processes and services, the system performance and network load, terminate programs and processes and start and stop services on a B&R device with Windows CE. |
|||||
Verze | Jazyk | Operační systém | Datum | Velikost | Typ | Stáhnout |
2.0.1 | DE | WinCE5x, WinCE6x | 22.04.2009 | 729 KB | ZIP | BrTaskMan_CE_D_V2_0_1.zip |
2.0.1 | EN | WinCE5x, WinCE6x | 22.04.2009 | 727 KB | ZIP | BrTaskMan_CE_E_V2_0_1.zip |
Popis |
Task Manager With the B&R Task Manager you can display information about running programs, processes and services, the system performance and network load, terminate programs and processes and start and stop services on a B&R device with Windows CE. |
|||||
Verze | Jazyk | Operační systém | Datum | Velikost | Typ | Stáhnout |
2.0 | DE | WinCE5x, WinCE6x | 28.04.2009 | 729 KB | ZIP | BrTaskMan_CE_D_V2_0.zip |
2.0 | EN | WinCE5x, WinCE6x | 28.04.2009 | 727 KB | ZIP | BrTaskMan_CE_E_V2_0.zip |
Popis |
Task Manager With the B&R Task Manager you can display information about running programs, processes and services, the system performance and network load, terminate programs and processes and start and stop services on a B&R device with Windows CE. |