Stepper Motor and DC motor library(Motorky)

DWL@DWL10000071830

Verze Jazyk
Operační systém
Datum
Velikost
Typ Stáhnout
2.17.0 * Sonstige 11.07.2014 366 KB ZIP Motorky_V2.17.0.zip
Popis Stepper Motor and DC motor library(Motorky)

SW: Automation Studio
HW: SG3, SG4 targets

The library provides functions for easily running
stepper motors but also DC motors connected via MM
modules.

A project showing its usage also exists in the "Demo Projects" section.

V2.17.0
New:
- converted to AS4
- minimum value of "init.units" is not limited to 1000 anymore
- SM: new parameter init.outputFilter
- cmd.position renamed to cmd.cyclicPosition

V2.16.0
- in rare cases no error text was displayed
- in rare cases "info.moveActive" remained set after error
acknowledgement
- the signs of "param.speed" and "param.homing.speed2" are now
ignored for homing

V2.15.0
New:
- MM: due to a bug in speed PID the controller not working very
well compared to V2.14.0

V2.10.0
New:
- DS, SM: "init.microsteps" introduced

V2.09.0
New:
- cmd.stop command now uses "param.deceleration" (and not
"init.maxAcceleration" like before)

V2.08.0
New:
- all movement types (absolute, additive, position, velocity)
can interrupt each other

V2.07.0
New:
- absolute and additive movements can be started during
movement
- DS: example in help corrected
- DS: MovTargetTime insreased by one TC

V2.05.0
New:
- SM: FUB can be now used also for ACOPOSmicro (stepper)
- SM: output filter reduces motor resonances. Due to this, the
Motorky library reaches higher speeds than Ramp mode
-"cmd.relative" renamed to "cmd.additive"
- example for FI uses ACOPOSinverter X64

V2.04.0
New:
- DS: DS1x19 module signalized errors when the DS FUB was called
in 1 ms

V2.03.0
New:
- on SW limits the library was braking with
"init.maxAcceleration" instead of "param.deceleration"

V2.02.0
New:
- data type of all HOMING_* constants changed from UINT to USINT

V2.01.0
New:
- SM, DS: scaling was not working

V2.00.0
New:
- working for AS3 and Compiler 4.1.1

V1.38.0
New:
- data type of all HOMING_* constants changed from UINT to USINT

V1.37.0
New:
- SM, DS: scaling was not working

V1.36.0
New:
- target position was sometimes not reached exactly
- with repeating relative movements, there was a cumulative
position error
- performance improvements
Verze Jazyk
Operační systém
Datum
Velikost
Typ Stáhnout
2.16.0 * Sonstige 09.12.2013 770 KB ZIP Motorky_V2.16.0.zip
Popis Stepper Motor and DC motor library(Motorky)

SW: Automation Studio
HW: SG3, SG4 targets

The library provides functions for easily running
stepper motors but also DC motors connected via MM
modules.

A project showing its usage also exists in the "Demo Projects" section.

V2.16.0
- in rare cases no error text was displayed
- in rare cases "info.moveActive" remained set after error
acknowledgement
- the signs of "param.speed" and "param.homing.speed2" are now
ignored for homing

V2.15.0
New:
- MM: due to a bug in speed PID the controller not working very
well compared to V2.14.0

V2.10.0
New:
- DS, SM: "init.microsteps" introduced

V2.09.0
New:
- cmd.stop command now uses "param.deceleration" (and not
"init.maxAcceleration" like before)

V2.08.0
New:
- all movement types (absolute, additive, position, velocity)
can interrupt each other

V2.07.0
New:
- absolute and additive movements can be started during
movement
- DS: example in help corrected
- DS: MovTargetTime insreased by one TC

V2.05.0
New:
- SM: FUB can be now used also for ACOPOSmicro (stepper)
- SM: output filter reduces motor resonances. Due to this, the
Motorky library reaches higher speeds than Ramp mode
-"cmd.relative" renamed to "cmd.additive"
- example for FI uses ACOPOSinverter X64

V2.04.0
New:
- DS: DS1x19 module signalized errors when the DS FUB was called
in 1 ms

V2.03.0
New:
- on SW limits the library was braking with
"init.maxAcceleration" instead of "param.deceleration"

V2.02.0
New:
- data type of all HOMING_* constants changed from UINT to USINT

V2.01.0
New:
- SM, DS: scaling was not working

V2.00.0
New:
- working for AS3 and Compiler 4.1.1

V1.38.0
New:
- data type of all HOMING_* constants changed from UINT to USINT

V1.37.0
New:
- SM, DS: scaling was not working

V1.36.0
New:
- target position was sometimes not reached exactly
- with repeating relative movements, there was a cumulative
position error
- performance improvements
Verze Jazyk
Operační systém
Datum
Velikost
Typ Stáhnout
2.15.0 * Sonstige 21.03.2013 770 KB ZIP Motorky_V2.15.0.zip
Popis Stepper Motor and DC motor library(Motorky)

SW: Automation Studio
HW: SG3, SG4 targets

The library provides functions for easily running
stepper motors but also DC motors connected via MM
modules.

A project showing its usage also exists in the "Demo Projects" section.

V2.10.0
New:
- DS, SM: "init.microsteps" introduced

V2.09.0
New:
- cmd.stop command now uses "param.deceleration" (and not
"init.maxAcceleration" like before)

V2.08.0
New:
- all movement types (absolute, additive, position, velocity)
can interrupt each other

V2.07.0
New:
- absolute and additive movements can be started during
movement
- DS: example in help corrected
- DS: MovTargetTime insreased by one TC

V2.05.0
New:
- SM: FUB can be now used also for ACOPOSmicro (stepper)
- SM: output filter reduces motor resonances. Due to this, the
Motorky library reaches higher speeds than Ramp mode
-"cmd.relative" renamed to "cmd.additive"
- example for FI uses ACOPOSinverter X64

V2.15.0
New:
- MM: due to a bug in speed PID the controller not working very
well compared to V2.14.0

V2.04.0
New:
- DS: DS1x19 module signalized errors when the DS FUB was called
in 1 ms

V2.03.0
New:
- on SW limits the library was braking with
"init.maxAcceleration" instead of "param.deceleration"

V2.02.0
New:
- data type of all HOMING_* constants changed from UINT to USINT

V2.01.0
New:
- SM, DS: scaling was not working

V2.00.0
New:
- working for AS3 and Compiler 4.1.1

V1.38.0
New:
- data type of all HOMING_* constants changed from UINT to USINT

V1.37.0
New:
- SM, DS: scaling was not working

V1.36.0
New:
- target position was sometimes not reached exactly
- with repeating relative movements, there was a cumulative
position error
- performance improvements
Verze Jazyk
Operační systém
Datum
Velikost
Typ Stáhnout
2.10.0 * Sonstige 27.07.2012 767 KB ZIP Motorky_V2.10.0.zip
Popis Stepper Motor and DC motor library(Motorky)

SW: Automation Studio
HW: SG3, SG4 targets

The library provides functions for easily running
stepper motors but also DC motors connected via MM
modules.

A project showing its usage also exists in the "Demo Projects" section.

V2.10.0
New:
- DS, SM: "init.microsteps" introduced

V2.09.0
New:
- cmd.stop command now uses "param.deceleration" (and not
"init.maxAcceleration" like before)

V2.08.0
New:
- all movement types (absolute, additive, position, velocity)
can interrupt each other

V2.07.0
New:
- absolute and additive movements can be started during
movement
- DS: example in help corrected
- DS: MovTargetTime insreased by one TC

V2.05.0
New:
- SM: FUB can be now used also for ACOPOSmicro (stepper)
- SM: output filter reduces motor resonances. Due to this, the
Motorky library reaches higher speeds than Ramp mode
-"cmd.relative" renamed to "cmd.additive"
- example for FI uses ACOPOSinverter X64

V2.04.0
New:
- DS: DS1x19 module signalized errors when the DS FUB was called
in 1 ms

V2.03.0
New:
- on SW limits the library was braking with
"init.maxAcceleration" instead of "param.deceleration"

V2.02.0
New:
- data type of all HOMING_* constants changed from UINT to USINT

V2.01.0
New:
- SM, DS: scaling was not working

V2.00.0
New:
- working for AS3 and Compiler 4.1.1

V1.38.0
New:
- data type of all HOMING_* constants changed from UINT to USINT

V1.37.0
New:
- SM, DS: scaling was not working

V1.36.0
New:
- target position was sometimes not reached exactly
- with repeating relative movements, there was a cumulative
position error
- performance improvements
Verze Jazyk
Operační systém
Datum
Velikost
Typ Stáhnout
2.07.0 * Sonstige 02.01.2012 768 KB ZIP Motorky_V2.07.0.zip
Popis Stepper Motor and DC motor library(Motorky)

SW: Automation Studio
HW: SG3, SG4 targets

The library provides functions for easily running
stepper motors but also DC motors connected via MM
modules.

A project showing its usage also exists in the "Demo Projects" section.

V2.07.0
New:
- absolute and additive movements can be started during
movement
- DS: example in help corrected
- DS: MovTargetTime insreased by one TC

V2.05.0
New:
- SM: FUB can be now used also for ACOPOSmicro (stepper)
- SM: output filter reduces motor resonances. Due to this, the
Motorky library reaches higher speeds than Ramp mode
-"cmd.relative" renamed to "cmd.additive"
- example for FI uses ACOPOSinverter X64

V2.04.0
New:
- DS: DS1x19 module signalized errors when the DS FUB was called
in 1 ms

V2.03.0
New:
- on SW limits the library was braking with
"init.maxAcceleration" instead of "param.deceleration"

V2.02.0
New:
- data type of all HOMING_* constants changed from UINT to USINT

V2.01.0
New:
- SM, DS: scaling was not working

V2.00.0
New:
- working for AS3 and Compiler 4.1.1

V1.38.0
New:
- data type of all HOMING_* constants changed from UINT to USINT

V1.37.0
New:
- SM, DS: scaling was not working

V1.36.0
New:
- target position was sometimes not reached exactly
- with repeating relative movements, there was a cumulative
position error
- performance improvements
Verze Jazyk
Operační systém
Datum
Velikost
Typ Stáhnout
2.05.0 * Sonstige 01.04.2011 683 KB ZIP Motorky_V2.05.0.zip
Popis Stepper Motor and DC motor library(Motorky)

SW: Automation Studio
HW: SG3, SG4 targets

The library provides functions for easily running
stepper motors but also DC motors connected via MM
modules.

A project showing its usage also exists in the "Demo Projects" section.

V2.05.0
New:
- SM: FUB can be now used also for ACOPOSmicro (stepper)
- SM: output filter reduces motor resonances. Due to this, the
Motorky library reaches higher speeds than Ramp mode
-"cmd.relative" renamed to "cmd.additive"
- example for FI uses ACOPOSinverter X64

V2.04.0
New:
- DS: DS1x19 module signalized errors when the DS FUB was called
in 1 ms

V2.03.0
New:
- on SW limits the library was braking with
"init.maxAcceleration" instead of "param.deceleration"

V2.02.0
New:
- data type of all HOMING_* constants changed from UINT to USINT

V2.01.0
New:
- SM, DS: scaling was not working

V2.00.0
New:
- working for AS3 and Compiler 4.1.1

V1.38.0
New:
- data type of all HOMING_* constants changed from UINT to USINT

V1.37.0
New:
- SM, DS: scaling was not working

V1.36.0
New:
- target position was sometimes not reached exactly
- with repeating relative movements, there was a cumulative
position error
- performance improvements
Verze Jazyk
Operační systém
Datum
Velikost
Typ Stáhnout
2.04.0 * Sonstige 12.11.2008 235 KB ZIP Motorky_V2.04.0.zip
Popis Stepper Motor and DC motor library(Motorky)

SW: Automation Studio
HW: SG3, SG4 targets

The library provides functions for easily running
stepper motors but also DC motors connected via MM
modules.

A project showing its usage also exists in the "Demo Projects" section.

V2.04.0
New:
- DS: DS1x19 module signalized errors when the DS FUB was called
in 1 ms

V2.03.0
New:
- on SW limits the library was braking with
"init.maxAcceleration" instead of "param.deceleration"

V2.02.0
New:
- data type of all HOMING_* constants changed from UINT to USINT

V2.01.0
New:
- SM, DS: scaling was not working

V2.00.0
New:
- working for AS3 and Compiler 4.1.1

V1.38.0
New:
- data type of all HOMING_* constants changed from UINT to USINT

V1.37.0
New:
- SM, DS: scaling was not working

V1.36.0
New:
- target position was sometimes not reached exactly
- with repeating relative movements, there was a cumulative
position error
- performance improvements
Verze Jazyk
Operační systém
Datum
Velikost
Typ Stáhnout
2.03.0 * Sonstige 12.11.2008 234 KB ZIP Motorky_V2.03.0.zip
Popis Stepper Motor and DC motor library(Motorky)

SW: Automation Studio
HW: SG3, SG4 targets

The library provides functions for easily running
stepper motors but also DC motors connected via MM
modules.

A project showing its usage also exists in the "Demo Projects" section.

V2.03.0
New:
- on SW limits the library was braking with
"init.maxAcceleration" instead of "param.deceleration"

V2.02.0
New:
- data type of all HOMING_* constants changed from UINT to USINT

V2.01.0
New:
- SM, DS: scaling was not working

V2.00.0
New:
- working for AS3 and Compiler 4.1.1

V1.38.0
New:
- data type of all HOMING_* constants changed from UINT to USINT

V1.37.0
New:
- SM, DS: scaling was not working

V1.36.0
New:
- target position was sometimes not reached exactly
- with repeating relative movements, there was a cumulative
position error
- performance improvements
Verze Jazyk
Operační systém
Datum
Velikost
Typ Stáhnout
2.02.0 * Sonstige 25.08.2008 231 KB ZIP Motorky_V2.02.0.zip
Popis Stepper Motor and DC motor library(Motorky)

SW: Automation Studio
HW: SG3, SG4 targets

The library provides functions for easily running
stepper motors but also DC motors connected via MM
modules.

A project showing its usage also exists in the "Demo Projects" section.

V2.02.0
New:
- data type of all HOMING_* constants changed from UINT to USINT

V2.01.0
New:
- SM, DS: scaling was not working

V2.00.0
New:
- working for AS3 and Compiler 4.1.1

V1.38.0
New:
- data type of all HOMING_* constants changed from UINT to USINT

V1.37.0
New:
- SM, DS: scaling was not working

V1.36.0
New:
- target position was sometimes not reached exactly
- with repeating relative movements, there was a cumulative
position error
- performance improvements
Verze Jazyk
Operační systém
Datum
Velikost
Typ Stáhnout
2.01.0 * Sonstige 30.06.2008 231 KB ZIP Motorky_V2.01.0.zip
Popis Stepper Motor and DC motor library (Motorky)

SW: Automation Studio 3
generated for Compiler 4.1.1
HW: SG3, SG4 targets

The library provides functions for easily running
stepper motors but also DC motors connected via MM
modules.

A project showing its usage also exists in the "Demo Projects" section.

V1.36.0
New:
- target position was sometimes not reached exactly
- with repeating relative movements, there was a cumulative
position error
- performance improvements

V1.37.0
New:
- SM, DS: scaling was not working

V2.00.0
New:
- working for AS3 and Compiler 4.1.1

V2.01.0
New:
- SM, DS: scaling was not working
Verze Jazyk
Operační systém
Datum
Velikost
Typ Stáhnout
2.00.0 * Win98SE, Sonstige 26.06.2008 229 KB ZIP Motorky_V2.00.0.zip
Popis Stepper Motor and DC motor library (Motorky)

SW: Automation Studio 3
generated for Compiler 4.1.1
HW: SG3, SG4 targets

The library provides functions for easily running
stepper motors but also DC motors connected via MM
modules.

A project showing its usage also exists in the "Demo Projects" section.

V1.36.0
New:
- target position was sometimes not reached exactly
- with repeating relative movements, there was a cumulative
position error
- performance improvements

V2.00.0
New:
- working for AS3 and Compiler 4.1.1
Verze Jazyk
Operační systém
Datum
Velikost
Typ Stáhnout
1.40.0 * Sonstige 12.11.2008 238 KB ZIP Motorky_V1.40.0.zip
Popis Stepper Motor and DC motor library(Motorky)

SW: Automation Studio
HW: SG3, SG4 targets

The library provides functions for easily running
stepper motors but also DC motors connected via MM
modules.

A project showing its usage also exists in the "Demo Projects" section.

V1.40.0
New:
- DS: DS1x19 module signalized errors when the DS FUB was called
in 1 ms

V1.39.0
New:
- on SW limits the library was braking with
"init.maxAcceleration" instead of "param.deceleration"

V1.38.0
New:
- data type of all HOMING_* constants changed from UINT to USINT

V1.37.0
New:
- SM, DS: scaling was not working

V1.36.0
New:
- target position was sometimes not reached exactly
- with repeating relative movements, there was a cumulative
position error
- performance improvements
Verze Jazyk
Operační systém
Datum
Velikost
Typ Stáhnout
1.39.0 * Sonstige 12.11.2008 238 KB ZIP Motorky_V1.39.0.zip
Popis Stepper Motor and DC motor library(Motorky)

SW: Automation Studio
HW: SG3, SG4 targets

The library provides functions for easily running
stepper motors but also DC motors connected via MM
modules.

A project showing its usage also exists in the "Demo Projects" section.

V1.39.0
New:
- on SW limits the library was braking with
"init.maxAcceleration" instead of "param.deceleration"

V1.38.0
New:
- data type of all HOMING_* constants changed from UINT to USINT

V1.37.0
New:
- SM, DS: scaling was not working

V1.36.0
New:
- target position was sometimes not reached exactly
- with repeating relative movements, there was a cumulative
position error
- performance improvements
Verze Jazyk
Operační systém
Datum
Velikost
Typ Stáhnout
1.38.0 * Sonstige 25.08.2008 237 KB ZIP Motorky_V1.38.0.zip
Popis Stepper Motor and DC motor library (Motorky)

SW: Automation Studio
HW: SG3, SG4 targets

The library provides functions for easily running
stepper motors but also DC motors connected via MM
modules.

A project showing its usage also exists in the "Demo Projects" section.

V1.38.0
New:
- data type of all HOMING_* constants changed from UINT to USINT

V1.37.0
New:
- SM, DS: scaling was not working

V1.36.0
New:
- target position was sometimes not reached exactly
- with repeating relative movements, there was a cumulative
position error
- performance improvements
Verze Jazyk
Operační systém
Datum
Velikost
Typ Stáhnout
1.37.0 * Sonstige 30.06.2008 236 KB ZIP Motorky_V1.37.0.zip
Popis Stepper Motor and DC motor library (Motorky)

SW: Automation Studio 3
generated for Compiler 4.1.1
HW: SG3, SG4 targets

The library provides functions for easily running
stepper motors but also DC motors connected via MM
modules.

A project showing its usage also exists in the "Demo Projects" section.

V1.36.0
New:
- target position was sometimes not reached exactly
- with repeating relative movements, there was a cumulative
position error
- performance improvements

V1.37.0
New:
- SM, DS: scaling was not working

V2.00.0
New:
- working for AS3 and Compiler 4.1.1
Verze Jazyk
Operační systém
Datum
Velikost
Typ Stáhnout
1.36.0 * Sonstige 25.06.2008 234 KB ZIP Motorky_V1.36.0.zip
Popis Stepper Motor and DC motor library (Motorky)

SW: Automation Studio
HW: SG3, SG4 targets

The library provides functions for easily running
stepper motors but also DC motors connected via MM
modules.

A project showing its usage also exists in the "Demo Projects" section.

V1.36.0
New:
- target position was sometimes not reached exactly
- with repeating relative movements, there was a cumulative
position error
- performance improvements
Verze Jazyk
Operační systém
Datum
Velikost
Typ Stáhnout
1.34.0 * Sonstige 30.05.2008 237 KB ZIP Motorky_V1.34.0.zip
Popis Stepper Motor and DC motor library (Motorky)

SW: Automation Studio
HW: SG3, SG4 targets

The library provides functions for easily running
stepper motors but also DC motors connected via MM
modules.

A project showing its usage also exists in the "Demo Projects" section.
Loading
Zpět k seznamu

Vyberte prosím zemi a jazyk

B&R Logo