DWL@DWL10000045093

Wersja Język
System operacyjny
Data
Rozmiar
Typ Pobierz
1.12 * DOS 03/05/2005 41 KB ZIP PPx00_aPCI_Upgrade_V1_12.zip
Opis aPCI Firmware Upgrade

You can update the firmware for aPCI modules on a B&R Power Panel 100 device with this disk.

----------------------------------------------------------------
Version 1.12 / 14.04.2005 / HOH
----------------------------------------------------------------

Contents

Autoexec.bat
Config.sy
Liesmich.txt NEW
Readme.txt NEW
SavApci.bat
UpdApci.bat
Xflash.exe 1.08

Changes

- Built as separate disk (removed from Power Panel BIOS Upgrade
Disks version 1.11).
Wersja Język
System operacyjny
Data
Rozmiar
Typ Pobierz
1.02 * DOS 12/03/2007 38 KB ZIP PP300_400_BIOS_aPCI_Firmware_Upgrade_Disk_V0102.zip
Opis aPCI Firmware Upgrade

You can update and save the FPGA firmware for aPCI modules on a
B&R Power Panel 300/400 with this disk.

----------------------------------------------------------------
UPDATE PROCEDURE
----------------------------------------------------------------

1. Copy all files to a bootable disk.

2. If you want to update the aPCI FPGA firmware copy the new aPCI FPGA firmware files for the aPCI modules to the disk.
Contact B&R to get the proper aPCI firmware files.

3. Insert the disk in a (USB) floppy drive connected to the Power Panel and re-boot the device.

4. A boot menu with following options is shown after booting:


1. Update aPCI FPGA (autoselect)

The FPGA firmware of both aPCI slots will be updated automatically (default after 5 sec).
The aPCI modules are required. The aPCI FPGA firmware files are selected automatically according to the plugged in aPCI modules.

2. Update aPCI FPGA of slot 1
The FPGA firmware of aPCI slot 1 will be updated automatically.
If no aPCI modul is plugged in, the aPCI FPGA firmware file must be renamed to "apci1.pci" (for aPCI slot 1) before updating.

3. Update aPCI FPGA of slot 2
The FPGA firmware of aPCI slot 2 will be updated automatically.
If no aPCI modul is plugged in, the aPCI FPGA firmware file must be renamed to "apci2.pci" (for aPCI slot 2) before updating.

4. Save aPCI FPGA (directory SAVED)
The FPGA firmware of both aPCI slots will be saved automatically in the SAVED directory.

***********************************************************
There must be up to 640 kbytes free space left on the disk.
***********************************************************

5. Exit
Exit to the Shell (MS-DOS).


5. Select the desired action.

6. Remove disk and reboot system after successful update.


----------------------------------------------------------------
Version 1.02
----------------------------------------------------------------

Contents:
MTCXSVC.EXE 3.01 NEW
CONFIG.SYS NEW

Fixes:
- None.

Changes:
- MTCXSVC.EXE: Newest version.
- CONFIG.SYS: Text optimizations for QVGA devices.
Wersja Język
System operacyjny
Data
Rozmiar
Typ Pobierz
1.01 * DOS 13/12/2006 34 KB ZIP PP300_400_BIOS_aPCI_Firmware_Upgrade_Disk_V0101.zip
Opis aPCI Firmware Upgrade

----------------------------------------------------------------
GENERAL INFORMATION
----------------------------------------------------------------

You can update and save the FPGA firmware for aPCI modules on a
B&R Power Panel 300/400 with this disk.

----------------------------------------------------------------
UPDATE PROCEDURE
----------------------------------------------------------------

1. Copy all files to a bootable disk.

2. If you want to update the aPCI FPGA firmware copy the new aPCI FPGA firmware files for the aPCI modules to the disk.

Contact B&R to get the proper aPCI firmware files.

3. Insert the disk in a (USB) floppy drive connected to the Power Panel and re-boot the device.

4. A boot menu with following options is shown after booting:

1. Update FPGA firmware automatically (aPCI modules required)

The FPGA firmware of both aPCI slots will be updated
automatically (default after 5 sec).

The aPCI modules are required. The aPCI FPGA firmware files are selected automatically according to the plugged in aPCI modules.

2. Update FPGA firmware of aPCI slot 1

The FPGA firmware of aPCI slot 1 will be updated
automatically.

If no aPCI modul is plugged in, the aPCI FPGA firmware
file must be renamed to "apci1.pci" (for aPCI slot 1)
before updating.

3. Update FPGA firmware of aPCI slot 2

The FPGA firmware of aPCI slot 2 will be updated
automatically.

If no aPCI modul is plugged in, the aPCI FPGA firmware
file must be renamed to "apci2.pci" (for aPCI slot 2)
before updating.

4. Save FPGA firmware of both aPCI slots

The FPGA firmware of both aPCI slots will be saved
automatically in the SAVED directory.

***********************************************************
There must be up to 640 kbytes free space left on the disk.
***********************************************************

5. Exit

Exit to the Shell (MS-DOS).

5. Select the desired action.

6. Remove disk and reboot system after successful update.


----------------------------------------------------------------
Version 1.01
----------------------------------------------------------------

Contents:
MTCXSVC.EXE 2.11 NEW

Fixes:
- MTCXSVC.EXE: A error during programming the last block could
cause a checksum error.
- MTCXSVC.EXE: Bugfix with aPCI module dependant problems during
programming and verify.

Changes:
- MTCXSVC.EXE: New LPC bus detection.
Loading
Powrót do listy

Wybierz kraj i język

B&R Logo