Good automation runs deep

Bauer Maschinen GmbH has automated a unique research drill rig for exploring the seabed. It was made possible by B&R automation components that function reliably, even 2,500 meters below the surface of the ocean.

Built to perform at a depth of 2,500 meters: The seabed exploration drill rig MeBo 200

Descending through the darkness, four plate-footed legs extend in preparation for contact with the landscape below and ensure the ten-ton apparatus comes to rest in a solid stance. A robotic drill extends to probe the layers of sediment and rock below.

What sounds like a landing on a distant planet is actually mission much closer to home, though the terrain is almost equally unexplored. It is a research drill rig taking samples from the ocean floor at depths of nearly 3,000 meters.

Destination: Seabed

The rig is called MeBo 200, and it is the result of a joint development project by MARUM – the Center for Marine Environmental Sciences at the University of Bremen – and Bauer Maschinen GmbH. MeBo 200 is capable of working at depths of up to 2,500 meters, where it can drill 200 meters into the seabed. The core samples it obtains provide valuable insight into the sediment structure and geology of the seabed.

MeBo 200 is capable of working at depths of up to 2,500 meters, where it can drill 200 meters into the seabed.

MeBo 200 is mounted in a frame that fits nicely into a 20-foot container and is carried by a research vessel to the location that is to be studied. When it arrives, the exploratory drill rig is lowered to the seabed by 2,700 meters of steel-armored cable. The cable is MeBo 200's lifeline to the ship, supplying it with both power and control commands.

A water-cooled winch is used to wind and unwind the 35.5 mm steel-armored cable. An X20 module from B&R seamlessly integrates the winch into MeBo 200's automation architecture.

Modern automation technology

The first two MeBo generations were used successfully in research projects for many years. For commercial use around the world, Bauer wanted to make further improvements and equip it with the following elements:

  • State-of-the-art control technology
  • An extended communication network
  • Interfaces for external automation components
  • An updated diagnostics and maintenance system

As its partner for upgrading the automation architecture, Bauer relied on B&R. "We've been working successfully with B&R for a very long time, and have been using their technology in our deep drilling rigs for decades," says Bauer's Lothar Schirmel.

Performance under harsh conditions

In order to reliably collect data from the seabed and send it to the ship, kilometers above, MeBo 200 requires extremely resilient technology. "At 2,500 meters below sea level, conditions are extreme," says Schirmel, "so all the components used must be robust and reliable. That's why we chose B&R's X90 mobile control system, which easily withstands these extreme conditions."

The X90 controllers are easy to adapt to different requirements using option modules. For the MeBo 200, they were configured as intelligent POWERLINK bus controllers with numerous integrated I/O connections. The POWERLINK protocol is transmitted on single-mode fiber cable via wave-division multiplexing media converters and converted back when it reaches the ship.

"Operating a reliably functioning real-time network under these extreme conditions is a major challenge," says Schirmel. But together with B&R it was one Bauer was able to solve. "They provided expert guidance in the selection of converters, and they knew just how to tweak the network settings to get the initial communication interruptions under control. That's exactly what you want from an automation partner."

Software updates on deck

The integrated Ethernet interfaces on the X90 controllers are accessible from the ship's deck via fiber optics. "That's key, because it allows us to update the software on the rig without having to bring it up to the surface or open the pressure vessel to access the controllers," Schirmel points out.

Electrical signals into the pressure vessel are secured with special plug-in connectors able to withstand up to 400 bar of pressure. In this way, nearly 100 proportional valves, absolute encoders, displacement sensors and more are connected to the I/Os on the X90 devices.

All at a glance

The drilling unit is controlled from a container on the deck of the research vessel. The completely revamped operator station features a seat with joystick controls mounted on the armrests, like you would find in the cab of a tractor or crane. Additional controls are found on three 19-inch touchscreen monitors, which Bauer selected from B&R's Automation Panel 5000 series.

The X90 mobile controllers are housed in sealed pressure vessels that protect the electronics from seawater.

The three panels display all the important information needed to control the MeBo 200 drilling rig and other auxiliary equipment. Above them, two more monitors display live video from eight underwater cameras, so the operators can keep a close eye on the largely manual drilling process.

All the data comes together in the B&R APROL process control system, which runs on two redundant Automation PC 910 units. Three more industrial PCs from the Automation PC 3100 series are used as remote HMI servers.

The drilling process is controlled via joystick, control panel and touchscreen operation from a container on the ship's deck. Live video streams from eight underwater cameras help operators keep an eye on the drilling process.

"We've been using APROL as a powerful HMI, data acquisition and data management solution in our oil and gas deep drilling rigs since 2005," Schirmel explains. "A key element is the high-performance data storage and long-term archiving that APROL offers. That includes the Trend Viewer, which lets us visualize the recorded data and analyze error causes."

Progressive commissioning

Bauer's control solution runs on a PLC from the B&R X20 system. With control and HMI running separately, they are able to start up, test and operate the drilling rig and auxiliary units progressively, even without an APROL server.

Bauer also uses the X20 system to integrate a variety of auxiliary units. These include a hydraulic power unit, a radio remote control for deck-based operation of the MeBo 200 and the power center with transformers for the drilling rig's high-voltage supply.

Simple connection of 3rd-party components

"Some of the auxiliary units are bought-in parts," Schirmel says. "For those, we have no say in what fieldbus is used. That's why we really appreciate that B&R offers interfaces and libraries for all common fieldbuses." That made it easy for Schirmel and his team to connect the remote control receiver, the joysticks and the associated control panel.

An ocean of computing power: Five industrial PCs from B&R guarantee that HMI operation and data storage always function reliably.

"The flexibility and consistency of everything in the B&R world allows us to seamlessly capture all the necessary data and transfer it to the HMI and data management systems without having to define or implement all the different interfaces ourselves," praises Schirmel. "Together with the openness and size of the product portfolio, those are the reasons we rely on B&R as an automation partner – especially for particularly large or unique automation projects like our new offshore applications."

Author: Franz Rossmann, technology journalist from near Munich

  • Benefits of the new MeBo generation
  • Industrial quality
  • Powerful, open architecture
  • Comprehensive connectivity
  • Consistent data management and seamless data storage


国と言語を選ぶ

B&R Logo