Synchronous motor 8LS, self-cooling, construction type A, 400 VAC - Number of pole pairs: 4 - Nominal speed: 6000 rpm - Nominal torque: 1.600 Nm - Stall torque: 2.300 Nm - Centering diameter: 80.00 mm
Synchronous motor 8LS, self-cooling, construction type A, 400 VAC - Number of pole pairs: 4 - Nominal speed: 3000 rpm - Nominal torque: 11.600 Nm - Stall torque: 12.500 Nm - Centering diameter: 130.00
Power Panel T30, 5.7", landscape format. CPU and memory: 600 MHz (ARM Cortex-A8), 512 MB onboard flash drive. Display and touch screen: 5.7", 640 x 480 (VGA) resolution, analog resistive touch screen,
and supported by all of the necessary certifications. About B&R B&R has its head-office at Pune, Maharashtra and four other offices in India. B&R is fully equipped to cater to your application, supply and [...] Automation Studio software development environment, B&R is constantly redefining the future of automation engineering. The global headquarters of B&R as well as the manufacturing center is at Eggelsberg [...] from the automotive sector. A highlight of the exhibition was a seminar held by Ninad Deshpande of B&R, in which he addressed the concerns of industrial specialists and automotive plant owners with regard
B&R at the 2013 SPS IPC Drives trade fair in Nuremberg This year's SPS IPC Drives trade fair in Nuremberg will be taking place November 26–28, 2013. B&R will be taking advantage of the opportunity offered [...] 110 and 206. Two main topics are on the B&R agenda this year: maximizing scalability and minimizing response time. Unprecedented scalability With Scalability+, B&R is establishing a new philosophy for [...] of the machine without having to make compromises along the way. A new series of compact controllers B&R has developed a whole new series of hardware components that further enhances the interoperability
X20 interface module, 1 CAN bus interface, max. 1 Mbit/s, electrically isolated, order 1x terminal block TB2105 separately!
global network of value providers. B&R value providers work seamlessly with B&R to bring our products and services to your location. They combine in-depth knowledge of B&R technology with a deep understanding [...] environmental performance. Connectivity for third-party systems - What does B&R offer? Connectivity for third-party systems - What does B&R offer? Connectivity secures the future! It offers the opportunity to [...] expert Additional contact options for B&R: Local value provider Find a partner near you Take advantage of our global network for end customers. In addition to more than 200 B&R subsidiaries in over 70 countries
ACOPOSmulti power supply module, 44 A, AS, wall mounting
including activation of listed Aprol Licenses - Pill is by default fitted to USB-iButton Adapter DS9490B. - AP.SW1-APR-3.4 APROL -SETUP & DOCUMENTATION R3.4-DVDs with actual Setup and actual APROL-Documentation
interfaces: 2x CAN bus. CPU and memory of the controller: 766 MHz (ARM Cortex-A9), 512 MB DRAM, 64 kB FRAM, 2 GB onboard flash drive. CPU and memory of the terminal: 800 MHz (ARM Cortex-A9), 1 GB DRAM.
国と言語を選ぶ