ACOPOSinverter X64, 3x 380-500 V, 15 kW, integrated EMC filter and brake chopper, shield plate included in delivery, X2X Link interface
Synchronous motor 8LS, self-cooling, construction type A, 400 VAC - Number of pole pairs: 4 - Nominal speed: 3000 rpm - Nominal torque: 17.500 Nm - Stall torque: 20.000 Nm - Centering diameter: 130.00
functions in Automation Studio B&R continues to advance the integration of OPC UA in the B&R Automation Studio development software. With POWERLINK, openSAFETY and OPC UA, B&R offers its customers the perfect
B&R servo actuator with advanced safety functions B&R now offers its compact ACOPOSmotor servo actuator with integrated network-based safety functions. Advanced safety solutions can now be implemented [...] functions are certified up to SIL 3 / PL e / Cat 4. Intelligent encoder system For the encoder system, B&R uses safety encoders with an EnDat 2.2 interface. The digital encoders are resistant to interference
Service Center. The HMI Service Center is a software tool used to test B&R's industrial PCs and Automation Panels. Industrial PCs from B&R have always offered extensive system diagnostics that go above and [...] Performance data and diagnostics in B&R's HMI Service Center To offer optimum support whenever service is required, all informational and diagnostics features will be provided via the newly developed HMI
B&R software has now also received PLCopen certification for Coordinated Motion. B&R's Automation Studio development platform now makes programming and configuring multi-axis systems easier than ever before [...] PLCopen-certified Coordinated Motion function blocks to the proven Generic Motion Control approach. B&R has constantly been adding to its portfolio of certified PLCopen blocks since 2004. "Standardization [...] structure – as it is to set up single axes," explains Gernot Bachler, technical manager of Motion at B&R. Identical command execution is guaranteed by the use of standardized interfaces. "Not a single line
CAD configurator for B&R servo motors and gearboxes It's now easier than ever for B&R customers to design their machines and systems using CAD programs. B&R's web configurator allows you to generate CAD [...] changes and prevents unnecessary wear and tear. Optional features included The CAD configurator on the B&R website allows you to select all the optional features, such as cooling type, size, encoder system
B&R presents optimized yaw control at WindEurope. Automation expert B&R will be presenting its ACOPOS P3 servo drive for optimized yaw control at this year's WindEurope conference and exhibition, Booth [...] more profitable. Implementing Maritime 4.0 Visitors will also experience B&R's solutions for smart ships. These are based on B&R's business intelligence and IIoT solutions: Orange Box and APROL PDA. These
B&R at the K fair: Monitoring and analytics for improved machine performance At the K 2019 trade fair (Hall 12 / Booth B16), B&R will be demonstrating how analysis of operating data can help detect and [...] implementation. In addition to the company' s well-established complete solutions for machine automation, B&R will present a portfolio that creates added value for the plastics industry through connectivity,
B&R: Fredrik Holmberg to drive business in the field of medical device assembly B&R has added Fredrik Holmberg to its business development team as an expert in the field of medical device assembly . Holmberg [...] sales at B&R Sweden. During this time, he gained years of experience working with customers in the field of medical device assembly. This experience will serve him well in his new position on B&R's int
国と言語を選ぶ