|
0TG1000.01
|
Technology Guard (MSD)
|
|
|
0TG1000.02
|
Technology Guard (HID)
|
|
|
1TG4600.10-5
|
Automation Runtime Windows TG license
|
|
|
1TG4601.06-5
|
Automation Runtime Embedded TG license
|
|
|
1TGAP42CDRV9992UPG
|
PROFIBUS DP PROFINET/CTRL, UPG
|
|
|
1TGAP42CDRV9993NEW
|
Modbus-RTU/ TCP/CTRL/CC, NEW Important notice: The driver for the Control Computer (CC) is still in the prototype phase, use only permitted for non-productive systems after release by product management!
|
|
|
1TGAP42CDRV9993UPG
|
Modbus-RTU/ TCP/CTRL/CC, UPG Important notice: The driver for the Control Computer (CC) is still in the prototype phase, use only permitted for non-productive systems after release by product management!
|
|
|
1TGAP42CDRV9998UPG
|
IEC 60870-5-104/CTRL/CC, UPG Important note: The driver for the control computer (CC) is still in the prototype phase. Use is only permitted for non-productive systems after approval by the product management!
|
|
|
1TGAP42CDRV9999NEW
|
IEC 60870-5-101 / CTRL, NEW
|
|
|
1TGAP42CDRV9999UPG
|
IEC 60870-5-101 / CTRL, UPG
|
|
|
1TGAP42CLIB9995NEW
|
MPC signal (MIMO) / CTRL, NEW APROL MPC (multiple In / multiple Out) / CTRL This license is valid for activation of 1 controlled variable (X), 1 manipulated variable (Y) or 1 disturbance variable input (Z). Example: 7 licenses are therefore needed for an MPC with 2xX, 3xZ and 2xY. The license allows the use of APROL basic functions on a B&R controller (SG4 target system). To use the license on a controller, a dongle of type 0TG1000.02 (Technology Guard) is required.
|
|
|
1TGAP42CLIB9997NEW
|
Process Automation Lib. (PAL) / CTRL, NEW
|
|
|
1TGAP42CLIB9997UPG
|
Process Automation Lib. (PAL) / CTRL, UPG
|
|
|
1TGAP42CLIB9998UPG
|
Basic Library/CTRL, UPG
|
|
|
1TGAP42CLIB9999NEW
|
SelfTuningAlgorithm-MinInvasive/CTRL, NEW
|
|
|
1TGAP42E0000000NEW
|
Engineering,NEW Engineering system is used to prepare configuration data for the whole project before it is deployed to runtime server.
|
|
|
1TGAP42E0000000OEM
|
Engineering,OEM Engineering system is used to prepare configuration data for the whole project before it is deployed to runtime server.
|
|
|
1TGAP42E0000000UPG
|
Engineering,UPG Engineering system is used to prepare configuration data for the whole project before it is deployed to runtime server.
|
|
|
1TGAP42EAS-0000NEW
|
Engineering AS Edition APROL,NEW
|
|
|
1TGAP42EAS-0000UPG
|
Engineering AS Edition APROL,UPG
|
|
|
1TGAP42O0000000NEW
|
Operator,NEW Operations stations provide the user interface for operators (process graphics, faceplates, trend displays, alarm & event lists, etc.).
|
|
|
1TGAP42O0000000OEM
|
Operator,OEM
|
|
|
1TGAP42O0000000UPG
|
Operator,UPG Operations stations provide the user interface for operators (process graphics, faceplates, trend displays, alarm & event lists, etc.).
|
|
|
1TGAP42ONET0001UPG
|
Operator via Net, UPG
|
|
|
1TGAP42R0001111NEW
|
ParameterCenter, NEW
|
|
|
1TGAP42R0001111UPG
|
ParameterCenter, UPG
|
|
|
1TGAP42RBI-1111NEW
|
Business Intellig. R (+E)- SOLUTIONS, NEW License for one instance of Report Server(R) and Report Designer(E). The report server generates reports from the data in use, data at rest or data in transit. Provides report creation and viewing, ad hoc reports and mobile access. Includes a license for "TIBCO JasperReports Server Professional Edition" for APROL (package/bundle for OEM). - B&R offers this license as an integrated software vendor (OEM) exclusively as an optional license for APROL. This license is only permitted to be used together with APROL. - This license is a 1-year subscription and permits the operation of the "TIBCO JasperReports Server Professional Edition" software that is shipped with APROL for an unlimited period of time (OEM license does not expire). - The 1-year subscription begins with the delivery of the APROL system by B&R. - If the "TIBCO JasperReports Server Professional Edition" software is updated/upgraded after the 1-year subscription has expired, a new license (subscription) is required (e.g. caused by the APROL update/upgrade). - Customers who will use the monthly AutoYaST update via license "GPOS- Security update- 202x/ CC" in the future must ensure that a "JRS BI- Security update- 202x" license may also have to be purchased. Note: - The service life of the "TIBCO JasperReports Server Professional Edition" software is not limited. - If the software is updated, however the control computer must have a valid 1-year subscription at that moment.
|
|
|
1TGAP42RBI-1111UPG
|
Business Intellig. R (+E)- SOLUTIONS, UPG License for one instance of Report Server(R) and Report Designer(E). The report server generates reports from the data in use, data at rest or data in transit. Provides report creation and viewing, ad hoc reports and mobile access. Includes a license for "TIBCO JasperReports Server Professional Edition" for APROL (package/bundle for OEM). - B&R offers this license as an integrated software vendor (OEM) exclusively as an optional license for APROL. This license is only permitted to be used together with APROL. - This license is a 1-year subscription and permits the operation of the "TIBCO JasperReports Server Professional Edition" software that is shipped with APROL for an unlimited period of time (OEM license does not expire). - The 1-year subscription begins with the delivery of the APROL system by B&R. - If the "TIBCO JasperReports Server Professional Edition" software is updated/upgraded after the 1-year subscription has expired, a new license (subscription) is required (e.g. caused by the APROL update/upgrade). - Customers who will use the monthly AutoYaST update via license "GPOS- Security update- 202x/ CC" in the future must ensure that a "JRS BI- Security update- 202x" license may also have to be purchased. Note: - The service life of the "TIBCO JasperReports Server Professional Edition" software is not limited. - If the software is updated, however the control computer must have a valid 1-year subscription at that moment.
|
|
|
1TGAP42RBI-9999NEW
|
Business Intelligence R (+E)- DCS, NEW License for one instance of Report Server(R) and Report Designer(E). The report server generates reports from the data in use, data at rest or data in transit. Provides report creation and viewing, ad hoc reports and mobile access. Includes a license for "TIBCO JasperReports Server Professional Edition" for APROL (package/bundle for OEM). - B&R offers this license as an integrated software vendor (OEM) exclusively as an optional license for APROL. This license is only permitted to be used together with APROL. - This license is a 1-year subscription and permits the operation of the "TIBCO JasperReports Server Professional Edition" software that is shipped with APROL for an unlimited period of time (OEM license does not expire). - The 1-year subscription begins with the delivery of the APROL system by B&R. - If the "TIBCO JasperReports Server Professional Edition" software is updated/upgraded after the 1-year subscription has expired, a new license (subscription) is required (e.g. caused by the APROL update/upgrade). - Customers who will use the monthly AutoYaST update via license "GPOS- Security update- 202x/ CC" in the future must ensure that a "JRS BI- Security update- 202x" license may also have to be purchased. Note: - The service life of the "TIBCO JasperReports Server Professional Edition" software is not limited. - If the software is updated, however the control computer must have a valid 1-year subscription at that moment.
|
|
|
1TGAP42RBI-9999UPG
|
Business Intelligence R (E)- DCS, UPG License for one instance of Report Server(R) and Report Designer(E). The report server generates reports from the data in use, data at rest or data in transit. Provides report creation and viewing, ad hoc reports and mobile access. Includes a license for "TIBCO JasperReports Server Professional Edition" for APROL (package/bundle for OEM). - B&R offers this license as an integrated software vendor (OEM) exclusively as an optional license for APROL. This license is only permitted to be used together with APROL. - This license is a 1-year subscription and permits the operation of the "TIBCO JasperReports Server Professional Edition" software that is shipped with APROL for an unlimited period of time (OEM license does not expire). - The 1-year subscription begins with the delivery of the APROL system by B&R. - If the "TIBCO JasperReports Server Professional Edition" software is updated/upgraded after the 1-year subscription has expired, a new license (subscription) is required (e.g. caused by the APROL update/upgrade). - Customers who will use the monthly AutoYaST update via license "GPOS- Security update- 202x/ CC" in the future must ensure that a "JRS BI- Security update- 202x" license may also have to be purchased. Note: - The service life of the "TIBCO JasperReports Server Professional Edition" software is not limited. - If the software is updated, however the control computer must have a valid 1-year subscription at that moment.
|
|
|
1TGAP42RGV-0050NEW
|
GV-License-Runtime 0050 GVs, NEW
|
|
|
1TGAP42RGV-0050UPG
|
GV-License-Runtime 0050 GVs, UPG
|
|
|
1TGAP42RGV-1000NEW
|
GV-License-Runtime 1000 GVs, NEW
|
|
|
1TGAP42RGV-1000UPG
|
GV-License-Runtime 1000 GVs, UPG
|
|
|
1TGAP42RIO-0050NEW
|
IO-License-Runtime 0050 I/Os, NEW
|
|
|
1TGAP42RIO-0050UPG
|
IO-License-Runtime 0050 I/Os, UPG
|
|
|
1TGAP42RIO-1000NEW
|
IO-License-Runtime 1000 I/Os, NEW
|
|
|
1TGAP42RIO-1000UPG
|
IO-License-Runtime 1000 I/Os, UPG
|
|
|
1TGAP42RLIB9996NEW
|
PAL Edition PDA (PAL-PDA)/CC, NEW
|
|
|
1TGAP42RLIB9996UPG
|
PAL Edition PDA (PAL-PDA)/CC, UPG
|
|
|
1TGAP42RNET1111NEW
|
SQL access Historian Database, NEW
|
|
|
1TGAP42RNET1111UPG
|
SQL access Historian Database, UPG
|
|
|
1TGAP42RNET1112NEW
|
OPC access Realtime-Database, NEW
|
|
|
1TGAP42RNET1112UPG
|
OPC access Realtime-Database, UPG
|
|
|
1TGAP42RRED0000NEW
|
Runtime Redundancy,NEW
|
|
|
1TGAP42RRED0000OEM
|
Runtime redundancy,OEM
|
|
|
1TGAP42RRED0000UPG
|
Runtime redundancy,UPG
|
|
|
1TGAP42RREDEDUCAT
|
Runtime redundancy,Education key
|
|
|
1TGAP42RREDINTERN
|
Runtime redundancy,Internal use key
|
|
|
1TGAP42RREDPARTNER
|
Runtime redundancy,Partner key
|
|
|
1TGAP42RRGV0050NEW
|
GV-License-Red.Capability 0050 GVs, NEW
|
|
|
1TGAP42RRGV0050UPG
|
GV-License-Red.Capability 0050 GVs, UPG
|
|
|
1TGAP42RRGV1000NEW
|
GV-License-Red.Capability 1000 GVs, NEW
|
|
|
1TGAP42RRGV1000UPG
|
GV-License-Red.Capability 1000 GVs, UPG
|
|
|
1TGAP42RRIO0050NEW
|
IO-License-Red.Capability 0050 I/Os, NEW
|
|
|
1TGAP42RRIO0050UPG
|
IO-License-Red.Capability 0050 I/Os, UPG
|
|
|
1TGAP42RRIO1000NEW
|
IO-License-Red.Capability 1000 I/Os, NEW
|
|
|
1TGAP42RRIO1000UPG
|
IO-License-Red.Capability 1000 I/Os, UPG
|
|
|
1TGAP42RSVR0000NEW
|
Runtime server,NEW Runtime server provides the system’s runtime core DCS functions (alarm system, trend system, realtime database).
|
|
|
1TGAP42RSVR0000OEM
|
Runtime server,OEM Runtime server provides the system’s runtime core DCS functions (alarm system, trend system, realtime database).
|
|
|
1TGAP42RSVR0000UPG
|
Runtime server,UPG Runtime server provides the system’s runtime core DCS functions (alarm system, trend system, realtime database).
|
|
|
1TGAP42XEDUCATION
|
Runtime/Operator/Engineering, Education
|
|
|
1TGAP42XPARTNER
|
Runtime/Operator/Engineering, partner key This license is intended for engineering and commissioning purposes for B&R Qualified Partners. It is not permitted to be used permanently on productive systems.
|
|
|
1TGAP42XSITEONLY
|
Runtime/Operator/Engineering, site-only This license is intended for engineering and commissioning purposes for OEMs / plant builders. It is not permitted to be used permanently on productive systems.
|
|
|
1TGAP4XCDRV9992NEW
|
PROFIBUS DP/PROFINET/CTRL,NEW Driver license for PROFIBUS DP / PROFINET driver (per controller).
|
|
|
1TGAP4XCDRV9992OEM
|
PROFIBUS DP / PROFINET / CTRL,OEM Driver license for PROFIBUS DP / PROFINET driver (per controller).
|
|
|
1TGAP4XCDRV9992UPG
|
PROFIBUS DP / PROFINET / CTRL,UPG Driver license for PROFIBUS DP / PROFINET driver (per controller).
|
|
|
1TGAP4XCDRV9993NEW
|
Modbus RTU/TCP/CTRL/CC,NEW Driver license for Modbus RTU/TCP driver (per controller).
|
|
|
1TGAP4XCDRV9993OEM
|
Modbus RTU/TCP/CTRL/CC,OEM Driver license for Modbus RTU/TCP driver (per controller).
|
|
|
1TGAP4XCDRV9993UPG
|
Modbus RTU/TCP/CTRL/CC,UPG Driver license for Modbus RTU/TCP driver (per controller).
|
|
|
1TGAP4XCDRV9997NEW
|
S5/S7-TC/PIP/CTRL,NEW Driver license for S5/S7 TCP/IP driver (per controller).
|
|
|
1TGAP4XCDRV9997OEM
|
S5/S7-TC/PIP/CTRL,OEM Driver license for S5/S7 TCP/IP driver (per controller).
|
|
|
1TGAP4XCDRV9997UPG
|
S5/S7-TC/PIP/CTRL,UPG Driver license for S5/S7 TCP/IP driver (per controller).
|
|
|
1TGAP4XCDRV9998NEW
|
IEC 60870-5-104/CTRL/CC,NEW This license authorizes the use of the IEC 60870-5-104 driver on a B&R controller.
|
|
|
1TGAP4XCDRV9998OEM
|
IEC 60870-5-104/CTRL/CC,OEM This license authorizes the use of the IEC 60870-5-104 driver on a B&R controller.
|
|
|
1TGAP4XCDRV9998UPG
|
IEC 60870-5-104/CTRL/CC,UPG This license authorizes the use of the IEC 60870-5-104 driver on a B&R controller.
|
|
|
1TGAP4XCDRV9999NEW
|
IEC 60870-5-101/CTRL,NEW This license authorizes the use of the IEC 60870-5-101 driver on a B&R controller.
|
|
|
1TGAP4XCDRV9999OEM
|
IEC 60870-5-101/CTRL,OEM This license authorizes the use of the IEC 60870-5-101 driver on a B&R controller.
|
|
|
1TGAP4XCDRV9999UPG
|
IEC 60870-5-101/CTRL,UPG This license authorizes the use of the IEC 60870-5-101 driver on a B&R controller.
|
|
|
1TGAP4XCLIB9995NEW
|
MPC Signal (MIMO)/CTRL,NEW The license is valid for the activation of 1 controlled variable (X), 1 manipulated variable (Y) or 1 disturbance variable input (Z). 7 licenses are therefore required for an MPC with e.g. 2x X,3x Z,2x Y.
|
|
|
1TGAP4XCLIB9995OEM
|
MPC Signal (MIMO)/CTRL,OEM The license is valid for the activation of 1 controlled variable (X), 1 manipulated variable (Y) or 1 disturbance variable input (Z). 7 licenses are therefore required for an MPC with e.g. 2x X,3x Z,2x Y.
|
|
|
1TGAP4XCLIB9995UPG
|
MPC signal (MIMO)/CTRL,UPG The license is valid for the activation of 1 controlled variable (X), 1 manipulated variable (Y) or 1 disturbance variable input (Z). 7 MPC signal licenses are required for an MPC with e.g.2x X,3x Z and 2x Y!
|
|
|
1TGAP4XCLIB9997NEW
|
PAL Library/CTRL,NEW This license authorizes the use of the Process Automation Library (PAL) on a B&R controller.
|
|
|
1TGAP4XCLIB9997OEM
|
PAL Library/CTRL,OEM This license authorizes the use of the Process Automation Library (PAL) on a B&R controller.
|
|
|
1TGAP4XCLIB9997UPG
|
PAL Library/CTRL,UPG This license authorizes the use of the Process Automation Library (PAL) on a B&R controller.
|
|
|
1TGAP4XCLIB9998NEW
|
Basic library/CTRL,NEW This license authorizes the use of a B&R controller with complete engineering.
|
|
|
1TGAP4XCLIB9998OEM
|
Basic library/CTRL,OEM This license authorizes the use of a B&R controller with complete engineering.
|
|
|
1TGAP4XCLIB9998UPG
|
Basic library/CTRL,UPG This license authorizes the use of a B&R controller with complete engineering.
|
|
|
1TGAP4XCRED0000NEW
|
Controller redund./CTRL,NEW This license authorizes the use of controller redundancy on a B&R controller (required for primary and secondary).
|
|
|
1TGAP4XCRED0000OEM
|
Controller redund./CTRL,OEM This license authorizes the use of controller redundancy on a B&R controller (required for primary and secondary).
|
|
|
1TGAP4XCRED0000UPG
|
Controller redund./CTRL,UPG This license authorizes the use of controller redundancy on a B&R controller (required for primary and secondary).
|
|
|
1TGAP4XE0000000NEW
|
Engineering,NEW The engineering system is used to create configuration data for the entire project before it is distributed to the runtime server, operator station and controller / field device target systems.
|
|
|
1TGAP4XE0000000OEM
|
Engineering,OEM The engineering system is used to create configuration data for the entire project before it is distributed to the runtime server, operator station and controller / field device target systems.
|
|
|
1TGAP4XE0000000UPG
|
Engineering,UPG The engineering system is used to create configuration data for the entire project before it is distributed to the runtime server, operator station and controller / field device target systems.
|
|
|
1TGAP4XEAS-0000NEW
|
Engineering AS Edition APROL, NEW ≤ R4.4-01 Enables the creation of the controller hardware configuration and the configuration of the fieldbuses for all APROL releases ≤ R4.4-01. Note: For APROL releases ≥ R4.4-65, reseller license 1TGSWAS.SNG.01-01 is required.
|
|
|
1TGAP4XEAS-0000OEM
|
Engin. AS edition APROL,OEM Enables the creation of the controller hardware configuration and configuration of the fieldbuses.
|
|
|
1TGAP4XO0000000NEW
|
Operator,NEW The operator station provides the user interface for the operators (process graphics, faceplates, trend displays, alarm and event lists, etc.).
|
|
|
1TGAP4XO0000000OEM
|
Operator,OEM The operator station provides the user interface for the operators (process graphics, faceplates, trend displays, alarm and event lists, etc.).
|
|
|
1TGAP4XO0000000UPG
|
Operator,UPG The operator station provides the user interface for the operators (process graphics, faceplates, trend displays, alarm and event lists, etc.).
|
|
|
1TGAP4XONET0001NEW
|
Operator via Net, NEW Enables the operation of an operator station via remote access (VNC client, etc.)
|
|
|
1TGAP4XONET0001OEM
|
Operator via Net, OEM Enables the operation of an operator station via remote access (VNC client, etc.)
|
|
|
1TGAP4XONET0001UPG
|
Operator via Net, UPG Enables the operation of an operator station via remote access (VNC client, etc.)
|
|
|
1TGAP4XR0001111NEW
|
ParameterCenter,NEW Enables operation of the ParameterCenter for parameter management (recipe management).
|
|
|
1TGAP4XR0001111OEM
|
ParameterCenter,OEM Enables operation of the ParameterCenter for parameter management (recipe management).
|
|
|
1TGAP4XR0001111UPG
|
ParameterCenter,UPG Enables operation of the ParameterCenter for parameter management (recipe management).
|
|
|
1TGAP4XRGV-0050NEW
|
GV-Lic-R 0050 GVs,NEW GV license for the non-redundant runtime server, for 0050 gateway variable data points.
|
|
|
1TGAP4XRGV-0050OEM
|
GV-Lic-R 0050 GVs,OEM GV license for the non-redundant runtime server, for 0050 gateway variable data points.
|
|
|
1TGAP4XRGV-0050UPG
|
GV-Lic-R 0050 GVs,UPG GV license for the non-redundant runtime server, for 0050 gateway variable data points.
|
|
|
1TGAP4XRGV-1000NEW
|
GV-Lic-R 1000 GVs,NEW GV license for the non-redundant runtime server, for 1000 gateway variable data points.
|
|
|
1TGAP4XRGV-1000OEM
|
GV-Lic-R 1000 GVs,OEM GV license for the non-redundant runtime server, for 1000 gateway variable data points.
|
|
|
1TGAP4XRGV-1000UPG
|
GV-Lic-R 1000 GVs,UPG GV license for the non-redundant runtime server, for 1000 gateway variable data points.
|
|
|
1TGAP4XRGV-5000NEW
|
GV-Lic-R 5000 GVs,NEW GV license for the non-redundant runtime server, for 5000 gateway variable data points.
|
|
|
1TGAP4XRGV-5000OEM
|
GV-Lic-R 5000 GVs,OEM GV-Lizenz für den nicht-redundanten Runtime Server, für 5000 Gateway-Variablen-Datenpunkte.
|
|
|
1TGAP4XRGV-5000UPG
|
GV-Lic-R 5000 GVs,UPG GV license for the non-redundant runtime server, for 5000 gateway variable data points.
|
|
|
1TGAP4XRIO-0050NEW
|
I/O-Lic-R 0050 I/OS,NEW I/O license for the non-redundant runtime server for 0050 I/O data points.
|
|
|
1TGAP4XRIO-0050OEM
|
I/O-Lic-R 0050 I/Os,OEM I/O license for the non-redundant runtime server for 0050 I/O data points.
|
|
|
1TGAP4XRIO-1000NEW
|
I/O-Lic-R 1000 I/Os,NEW I/O license for the non-redundant runtime server for 1000 I/O data points.
|
|
|
1TGAP4XRIO-1000OEM
|
I/O-Lic-R 1000 I/Os,OEM I/O license for the non-redundant runtime server for 1000 I/O data points.
|
|
|
1TGAP4XRIO-1000UPG
|
I/O-Lic-R 1000 I/Os,UPG I/O license for the non-redundant runtime server for 1000 I/O data points.
|
|
|
1TGAP4XRIO-5000NEW
|
I/O-Lic-R 5000 I/Os,NEW I/O license for the non-redundant runtime server for 5000 I/O data points.
|
|
|
1TGAP4XRIO-5000OEM
|
I/O-Lic-R 5000 I/Os,OEM I/O license for the non-redundant runtime server for 5000 I/O data points.
|
|
|
1TGAP4XRIO-5000UPG
|
I/O-Lic-R 5000 I/Os,UPG I/O license for the non-redundant runtime server for 5000 I/O data points.
|
|
|
1TGAP4XRLIB9996NEW
|
PAL Lib Edition PDA/CTRL,NEW4X This license authorizes the use of the Process Automation Library (PAL) on a B&R control computer (PDA coupling).
|
|
|
1TGAP4XRLIB9996OEM
|
PAL Lib Edition PDA/CTRL,OEM4X This license authorizes the use of the Process Automation Library (PAL) on a B&R control computer (PDA coupling).
|
|
|
1TGAP4XRLIB9996UPG
|
PAL Lib Edition PDA/CTRL,UPG4X This license authorizes the use of the Process Automation Library (PAL) on a B&R control computer (PDA coupling).
|
|
|
1TGAP4XRNET1111NEW
|
SQL access Historian DB,NEW Driver license for SQL access to APROL historical data.
|
|
|
1TGAP4XRNET1111OEM
|
SQL access Historian DB,OEM Driver license for SQL access to APROL historical data.
|
|
|
1TGAP4XRNET1111UPG
|
SQL access Historian DB,UPG Driver license for SQL access to APROL historical data.
|
|
|
1TGAP4XRNET1112NEW
|
OPC access RT database,NEW Driver license for OPC access to the real-time database
|
|
|
1TGAP4XRNET1112OEM
|
OPC access RT database,OEM Driver license for OPC access to the real-time database
|
|
|
1TGAP4XRNET1112UPG
|
OPC access RT database,UPG Driver license for OPC access to the real-time database
|
|
|
1TGAP4XRRED0000NEW
|
RTS redundancy capability/RTS,NEW The RTS redundancy capability license for the runtime server (RTS) enables redundant operation of a runtime server to increase system availability. For a redundant runtime server, two runtime server licenses (1x master/ 1x slave) and two RTS redundancy capability licenses (1x master/ 1x slave) are required.
|
|
|
1TGAP4XRRED0000OEM
|
RTS redundancy capability/RTS,OEM The RTS redundancy capability license for the runtime server (RTS) enables redundant operation of a runtime server to increase system availability. For a redundant runtime server, two runtime server licenses (1x master/ 1x slave) and two RTS redundancy capability licenses (1x master/ 1x slave) are required.
|
|
|
1TGAP4XRRED0000UPG
|
RTS redundancy capability/RTS,UPG The RTS redundancy capability license for the runtime server (RTS) enables redundant operation of a runtime server to increase system availability. For a redundant runtime server, two runtime server licenses (1x master/ 1x slave) and two RTS redundancy capability licenses (1x master/ 1x slave) are required.
|
|
|
1TGAP4XRRGV0050NEW
|
GV-Lic-rRCap 0050 GVs,NEW GV license for redundancy capability, for the redundant runtime server, for 0050 gateway variable data points.
|
|
|
1TGAP4XRRGV0050OEM
|
GV-Lic-rRCap 0050 GVs,OEM GV license for redundancy capability, for the redundant runtime server, for 0050 gateway variables-data point.
|
|
|
1TGAP4XRRGV1000NEW
|
GV-Lic-rRCap 1000 GVs,NEW GV license for redundancy capability, for the redundant runtime server, for 1000 gateway variable data points.
|
|
|
1TGAP4XRRGV1000OEM
|
GV-Lic-rRCap 1000 GVs,OEM GV license for redundancy capability, for the redundant runtime server, for 1000 gateway variable data points.
|
|
|
1TGAP4XRRGV5000NEW
|
GV-Lic-rRCap 5000 GVs,NEW GV license for redundancy capability, for the redundant runtime server, for 5000 gateway variable data points.
|
|
|
1TGAP4XRRGV5000OEM
|
GV-Lic-rRCap 5000 GVs,OEM GV license for redundancy capability, for the redundant runtime server, for 5000 gateway variable data points.
|
|
|
1TGAP4XRRIO0050NEW
|
I/O-Lic-rRCap 0050 I/Os,NEW I/O license for redundancy capability,, for the redundant runtime server for 0050 I/O data points.
|
|
|
1TGAP4XRRIO0050OEM
|
I/O-Lic-rRCap 0050 I/Os,OEM I/O license for redundancy capability,, for the redundant runtime server for 0050 I/O data points.
|
|
|
1TGAP4XRRIO0050UPG
|
I/O-Lic-rRCap 0050 I/Os,UPG I/O license for redundancy capability,, for the redundant runtime server for 0050 I/O data points.
|
|
|
1TGAP4XRRIO1000NEW
|
I/O-Lic-rRCap 1000 I/Os,NEW I/O license for redundancy capability,, for the redundant runtime server for 1000 I/O data points.
|
|
|
1TGAP4XRRIO1000OEM
|
I/O-Lic-rRCap 1000 I/Os,OEM I/O license for redundancy capability,, for the redundant runtime server for 1000 I/O data points.
|
|
|
1TGAP4XRRIO1000UPG
|
I/O-Lic-rRCap 1000 I/Os,UPG I/O license for redundancy capability,, for the redundant runtime server for 1000 I/O data points.
|
|
|
1TGAP4XRRIO5000NEW
|
I/O-Lic-rRCap 5000 I/Os,NEW I/O license for redundancy capability,, for the redundant runtime server for 5000 I/O data points.
|
|
|
1TGAP4XRRIO5000OEM
|
I/O-Lic-rRCap 5000 I/Os,OEM I/O license for redundancy capability,, for the redundant runtime server for 5000 I/O data points.
|
|
|
1TGAP4XRRIO5000UPG
|
I/O-Lic-rRCap 5000 I/Os,UPG I/O license for redundancy capability,, for the redundant runtime server for 5000 I/O data points.
|
|
|
1TGAP4XRSVR0000NEW
|
Runtime server,NEW The runtime server provides the runtime core functions of the system (alarm system, trend system, real-time database).
|
|
|
1TGAP4XRSVR0000OEM
|
Runtime server,OEM The runtime server provides the runtime core functions of the system (alarm system, trend system, real-time database).
|
|
|
1TGAP4XRSVR0000UPG
|
Runtime server,UPG The runtime server provides the runtime core functions of the system (alarm system, trend system, real-time database).
|
|
|
1TGAP4XXBI-9990SU2
|
BI platform Jasper RS,SU2 Subscription from Cloud Software Group Inc. to unlock JasperReports Server. The 2-year subscription starts with delivery to B&R. This results in a duration of 1.5 years after delivery to the customer.
|
|
|
1TGAP4XXBI-9999SU2
|
Jaspersoft platform use, 2 years - FTL, SU2 Service description Subscription from Cloud Software Group Inc. to activate the JasperReports Server (Jaspersoft platform use). Contains "Platform Usage / Customer User License / Standard Subscription / Enterprise Edition" - License for end customers. Term and license type The 2-year subscription begins with delivery or activation by the customer. This is a Fixed-Term License (FTL) with a limited right of use. End of use After expiry of the 2-year subscription, the applications activated by this subscription can no longer be used/launched.
|
|
|
1TGAP4XXOS-0000SU2
|
Operating system + 3rd-party licenses per CC Includes two SUSE Linux Enterprise Server (SLE) OEM licenses (support through ABB only) and other installed OEM licenses. The SLE license is of type SUSE Linux Enterprise Server, x86 and x86-64, 1-2 sockets or 1-2 virtual machines, basic subscription, 1 year. This ensures a maximum period of 2 years for ABB security updates via APROL AutoYaST Update. The subscription begins after delivery by ABB. The useful life of SLES is not limited, but a valid subscription is required for update rights.
|
|
|
1TGAP4XXOS-0000SU4
|
Operating system + 3rd-party licenses per CC Includes four SUSE Linux Enterprise Server (SLE) OEM licenses (support through ABB only) and other installed OEM licenses. The SLE license is of type SUSE Linux Enterprise Server, x86 and x86-64, 1-2 sockets or 1-2 virtual machines, basic subscription, 1 year. This ensures a maximum period of 4 years for ABB security updates via APROL AutoYaST Update. The subscription begins after delivery by ABB. The useful life of SLES is not limited, but a valid subscription is required for update rights.
|
|
|
1TGMPASSET.20-01
|
mapp Asset Intensity calculates the effectiveness of a machine based on its production data. The calculated data is then prepared for display in the form of a list or graph or made available for export.
|
|
|
1TGMPAUDIT.10-01
|
mapp Audit collects and manages a wide range of different events. These include when user-defined events occur, when machine operators log in/out or when an alarm occurs. All events are collected and can be exported with password protection to protect them from tampering.
|
|
|
1TGMPBRCLNT.10-01
|
License for one additional client on B&R hardware.
|
|
|
1TGMPCLIENT.10-01
|
License for one additional client.
|
|
|
1TGMPCODEBOX.10-01
|
mapp CodeBox makes it possible to program directly at the machine via the HMI application. The behavior of the machine can thus be changed without an additional engineering tool. There is basic access via Ladder Diagram and high-level language access via Structured Text.
|
|
|
1TGMPDATA.10-01
|
mapp Data makes it possible log process data. The user defines which process data should be persisted and in which time grid. In addition, data can be displayed in table form or evaluated statistically.
|
|
|
1TGMPENERGY.02
|
B&R software license for MpEnergy - Single-user license - Collect energy and power data - Display energy and power data via HMI application - Integrate external energy consumers - Support for modular software concepts - Web-based diagnostics and XML configuration The use of mapp flat-rate 1TGMPFLAT.02 is possible as an alternative.
|
|
|
1TGMPENERGY.10-01
|
mapp Energy collects energy data from various modules in the machine and prepares the data so that energy consumption can be visualized. In addition, data is collected and made available as a file for analysis.
|
|
|
1TGMPOEE.02
|
B&R software license - MpOee - Single license - Records overall equipment effectiveness (KPI) for measuring productivity - Display of measured values as list, timeline or graph - Export of measured values in CSV format - Support for modular software concepts - Web-based diagnostics and XML configuration The use of mapp flat-rate 1TGMPFLAT.02 is possible as an alternative.
|
|
|
1TGMPOEE.10-01
|
mapp OEE calculates overall equipment effectiveness based on the performance, availability and quality of the machine. The calculated data is then prepared for display in the form of a list or graph or made available for export.
|
|
|
1TGMPPACKML.10-01
|
mapp PackML provides support when implementing the OMAC PackML standard. Special focus is placed on the state model as well as managing the various operating modes. In addition, the current machine state can be shared with other machines/stations in the network using PackTags.
|
|
|
1TGMPREPORT.20-01
|
mapp Report makes it possible to generate PDF reports directly at the machine. A wide range of data can be included in the report, such as diagnostic data or current production values. These reports can then be localized and exported in a user-specified design.
|
|
|
1TGMPROBOX.02
|
B&R software license - MpRoboX - Single license - Flexible use of various robot kinematics - Starting programs, jogging, etc. - Various coordinate systems - Support for modular software concepts - Web-based diagnostics and XML configuration The use of mapp flat-rate 1TGMPFLAT.02 is possible as an alternative. The license for the CNC channel and transformation must be ordered separately.
|
|
|
1TGMPSAFETYX.00-01
|
B&R software license MpSafetyX - Single license - For interacting with B&R safety components - Provides secure data exchange between HMI elements and the SafeLOGIC controller - Transfer of safe parameters from an HMI application to the safe application - Support for modular software concepts - Web-based diagnostics and XML configuration
|
|
|
1TGMPSRV.00-01
|
Basic license for mapp Services. Required to use extended functions of the mapp Technology Package. This license includes mapp AlarmX (alarm management), mapp IO (dynamic hardware configuration), mapp User (user management), mapp Alarm (alarm management with reference to VC4), mapp File (file explorer), mapp Skyline (visualization of a machine line in combination with a mapp View widget), mapp J1939 (SAE J1939 protocol) and mapp Recipe (recipe management).
|
|
|
1TGMPTWEET.20-01
|
mapp Tweet makes it possible to transmit messages directly from the machine. This allows service technicians to be informed of emergencies involving the machine via SMS text message. Quick responses to critical situations are possible via a direct connection to mapp AlarmX.
|
|
|
1TGMPUSERX.02
|
B&R software license - MpUserX - Single-user license - User and role management - Password management (e.g. expiration date) - Password encryption - Import and export of users and roles - Support for modular software concepts - Web-based diagnostics and XML configuration The use of mapp flat-rate 1TGMPFLAT.02 is possible as an alternative.
|
|
|
1TGMPUSERX.10-01
|
mapp UserX allows the implementation of user management based on the Automation Studio user role system. This includes logging in/out, creating and editing users and saving additional user data (e.g. telephone numbers). Changes to user data can also be recorded as audit events.
|
|
|
1TGMPVIEW.00-01
|
Contains mapp View server, one client license and a standard set of widgets
|
|
|
1TGSWAS.STE.E0-01
|
This Automation Studio license permits the licensing of any number of users for research and educational purposes at the site of the educational facility. The license expires automatically after 400 calendar days and cannot be extended. The license also includes the use of the software on private PCs belonging to students as long as this is permitted and desired by the educational institution. The educational license is not permitted to be used for commercial purposes.
|
|