New dimensions in decentralized drive architecture
valuable space in the control cabinet, but also cuts costs for logistics and commissioning. This new system unites all of the important components such as the motor, positioning sensor (encoder), precision [...] actuator, we are continuing on the path to decentralized motion control," explains Alois Holzleitner, manager of B&R's Motion business unit. "We now offer the entire drive spectrum – from frequency inverters [...] assembly can be retrofitted for a performance boost of up to 100%. 100% compatibility with B&R drive systems The ACOPOSmulti65m is fully compatible with the entire ACOPOS drive series. As a result, it is possible