Secure Remote Maintenance -SiteManager, 1x Ethernet 100BASE-T uplink connection, 1x Wi-Fi uplink connection, 3x device connections, 10 device agents, integrated firewall, 2x digital inputs, 2x digital
Secure Remote Maintenance -SiteManager, LTE/4G/3G, for global, 1x Ethernet 100BASE-T uplink port, 1x GPRS/3G/4G uplink port, 5 device agents, 2x digital inputs, 2x digital outputs, 24 VDC
Secure Remote Maintenance -SiteManager, 1x Ethernet 100BASE-T uplink connection, 1x GPRS/3G/4G uplink connection, 3x device connections, 10 device agents, integrated firewall, 2x digital inputs, 2x digital
Secure Remote Maintenance -SiteManager, LTE/4G/3G, for region EMEA 1x Ethernet 100BASE-T uplink port, 1x GPRS/3G uplink port, 5 device agents, integrated firewall, 2x digital inputs, 2x digital outputs
Secure Remote Maintenance -SiteManager, LTE/4G/3G, for region CHINA 1x Ethernet 100BASE-T uplink port, 1x GPRS/3G uplink port, 5 device agents, integrated firewall, 2x digital inputs, 2x digital outputs
Secure Remote Maintenance -SiteManager, LTE/4G/3G, for region JAPAN 1x Ethernet 100BASE-T uplink port, 1x GPRS/3G uplink port, 5 device agents, integrated firewall, 2x digital inputs, 2x digital outputs
Secure Remote Maintenance -SiteManager, LTE/4G/3G, for US region 1x Ethernet 100BASE-T uplink port, 1x GPRS/3G uplink port, 5 device agents, integrated firewall, 2x digital inputs, 2x digital outputs,
up to 10,000 machines are stored. A comprehensive machine pool management solution can be set up easily. Integrated firewall The SiteManager has integrated digital inputs and outputs. These could be used [...] in the world. In addition, a certified and encrypted VPN connection is established between the SiteManager on the machine and a gateway, which is usually located at the machine manufacturer's service center [...] diagnostics and maintenance functions of the B&R system can be used via a secure VPN connection. The SiteManager is easy to configure in B&R's Automation Studio engineering software, making it perfectly suited
level to a database, regardless of whether that database is located on site or in the cloud. This drastically simplifies the management of large volumes of data. Data archiving directly from the controller [...] B&R optimizes data management with the mapp Technology software toolbox It is now easier than ever to implement databases in applications. With mapp Database, it is possible to archive data directly from [...] audit events, all data is sent automatically via mapp Links to a database where it can be easily managed.
infrastructure and workforce expansion. At the Hannover Messe trade fair, Managing Director Hans Wimmer and General Manager Peter Gucher announced B&R's plans to up production capacity. The company will [...] Group and will continue to operate on the market as a legally independent entity. "That means our management structures and points of contact with our customers will remain unchanged," emphasized Wimmer. [...] capacity at its headquarters in Eggelsberg by 20 percent. A few kilometers away, the company's Gilgenberg site will be expanded to accommodate production lines for its mechatronic solutions. Further expansion
Välj land och språk