Secure Remote Maintenance -SiteManager, Wi-Fi 1x Ethernet 100BASE-T uplink port, 1x Wi-Fi uplink port, 5 device agents, integrated firewall, 2x digital inputs, 2x digital outputs, 24 VDC
B&R introduces new master modules for digital communication B&R is introducing two new master modules that each use IO-Link 1.1 to communicate digitally with four intelligent field devices: The X20DS438A [...] X67DS438A with IP67 protection for use outside the control cabinet. The vision advanced by "Industry 4.0" – of workpieces moving independently through the production process and controlling their own production [...] digital parameter sets continue to take the place of adjustable potentiometers. Intelligent connections B&R has long relied on the IO-Link communication standard to cover the final stretch from the I/O module
X20 multifunction digital signal processor, 4 digital input channels, 4 digital channels configurable as inputs or outputs, 2 event counters 1 universal counter pair as AB counter or up/down counter, linear
X20 interface module, 1 RS422/485 interface, max. 115.2 kbit/s, electrically isolated
Power Panel PP420, 15" XGA color TFT display with touch screen (resistive), 1 aPCI slot, 128 MB SDRAM, 512 kB SRAM CompactFlash slot (type I), ETH 10/100, RS232, 2x USB, IP65 protection (front), 24 VD
Accessory terminal block, 2-pin (3.81), cage clamp terminal block 1.5 mm²
B&R customers benefit from cooperation between the OPC Foundation and the EPSG B&R customers will now be able to benefit from integrating communication from the sensor layer to the ERP layer without any [...] definition for open interfaces between their technologies. B&R has been relying on the open-source POWERLINK protocol for years, so all future B&R automation solutions will allow communication without interfaces [...] developed by both the OPC Foundation and the Ethernet POWERLINK Standardization Group (EPSG). Industry 4.0 and the Internet of Things (IoT) require seamless and consistent communication both within the digital
B&R simplifies machine-to-machine safety communication B&R now makes it easier than ever to implement safety communication between machines and machine modules. An update to its mapp Safety software now [...] effort – greatly reducing the time spent implementing systemwide safety functions. To achieve Industry 4.0 functionality, modern manufacturing equipment needs to be densely interconnected. Devices, machines [...] implementation with mapp Safety This added overhead is no longer necessary. The software components in B&R's mapp Safety package significantly improve communication between safety controllers and greatly simplify
Theis added that B&R plans to offer dual education at the university level in collaboration with higher education institutions. B&R unveils new brand identity With the new campus, B&R has also unveiled [...] creating a visual connection between B&R and ABB. “Our new visual design underscores ABB’s strong commitment to B&R as a category brand and shows the strength of B&R and ABB as we grow together and work [...] well as global training facilities for up to 4,000 people per year in collaboration with universities. ABB invested EUR 100 million in the expansion of the B&R headquarters. Campus innovations around artificial
EnDat 2.1 cable, length 2 m, 10x 0.14 mm² + 2x 0.5 mm², 17-pin female Intercontec EnDat connector, 15-pin male DSUB servo connector, can be used in cable drag chains
Välj land och språk