SO-DIMM DDR RAM 1024 MB PC2700.
Mobile Panel 7100 wall mount - For MP7140
highlights firsthand Industry 4.0, real-time applications with microsecond responsiveness and modular panel PCs – these were just some of the many topics explored at the 2014 B&R User Meeting. On May 20-21 [...] Salzburg Conference Center, B&R product information was presented ad-free – straight from the development teams themselves. Participants will get to hear application reports from B&R users and have the opportunity [...] plant and factory automation as well as process control technology. Specialists from B&R, industry experts and B&R customers were on hand to discuss current trends in industrial automation, including
Wimmer and Kastinger led the ambassador on a tour of B&R's own smart manufacturing operations. "What I've seen here at B&R has been very impressive. Industry 4.0 and Industrial IoT are the talk of global industry [...] Kastinger, who oversees B&R's sales activities in North America. "With our offices in Toronto and Montreal, we are close to our customers in the hotbeds of Canadian machine building." B&R's impressive production [...] Ambassador to Austria Mark Bailey recently visited industrial automation provider Bernecker + Rainer (B&R) in Eggelsberg. Meeting with Managing Director Hans Wimmer, Bailey learned about the company's latest
Experience automation highlights firsthand The 2014 B&R User Meeting is being held in June and July in four German cities and will explore topics such as Industry 4.0, modular panel PCs and real-time applications [...] responsiveness. Information about B&R products will be presented ad-free – straight from the development teams themselves. Participants will get to hear application reports from B&R users and have the opportunity [...] after the official program – the perfect opportunity to check out B&R's wide range of hardware and software tools first-hand. Anmeldung B&R User Meeting dates Tuesday, June 24 Chemnitz Wednesday, July 2 Bad
ACOPOSmulti3 SafeMOTION EnDat 2.2 Gen2 inverter module, 3.8 A, AS, wall mounting, 2 axes, optimized for applications with decentralized, computationally intensive open-loop and closed-loop control req
PPC2200 system unit - Intel Atom E3930 1.30 GHz - Dual core - 2 GB SDRAM
Power Panel PP420, 5.7" VGA color TFT display with touch screen (resistive), 1 aPCI slot, 128 MB SDRAM, 512 kB SRAM CompactFlash slot (type I), ETH 10/100, RS232, 2x USB, IP65 protection (front), 24 V
Accessory terminal block (3.5), 4-pin, cage clamp terminal block, 1.5 mm², protected against vibration by the screw flange
X20 Edge with built-in 4G modem A new variant of the B&R X20 Edge features an integrated 4G modem. This opens up vast new possibilities and use cases for connecting machine control to enterprise systems [...] Memory: 4 GB RAM Storage: 64 GB microSD card included for application memory Network / Interfaces: • 2 × Ethernet ports • 1 × USB port • Integrated 4G modem (global) with SIM slot With built-in 4G modem [...] computing platform that extends the B&R X20 system with powerful local processing and versatile connectivity. Now it has been enhanced with the addition of an integrated 4G global modem. This eliminates the
Välj land och språk