aPCI interface module, 1 PROFIBUS DP interface, electrically isolated and network-capable, 1 RS232 interface
SDL flex cable - 25 m
5 CDs 1A43S1:UU 20 CDs 4) Extending the Upgrade Service After the 12 months has passed, the Upgrade Service will be automaticall extended by B&R for another 12 months unless B&R is requested by the customer [...] the Upgrade Service The Upgrade deliveries from B&R will be ended if B&R is requested by the customer in written form to end the Upgrade Service agreement 4 weeks before the 12 months have passed. [...] B&R SafeDESIGNER maintenance single upgrade -------- B&R Automation Software Upgrade Service Agreement Agreement between the purchaser of the Upgrade Service Package, called Customer in the following text
5 CDs 1A43S1:UU 20 CDs 4) Extending the Upgrade Service After the 12 months has passed, the Upgrade Service will be automaticall extended by B&R for another 12 months unless B&R is requested by the customer [...] the Upgrade Service The Upgrade deliveries from B&R will be ended if B&R is requested by the customer in written form to end the Upgrade Service agreement 4 weeks before the 12 months have passed. [...] B&R SafeDESIGNER maintenance multiple upgrade -------- B&R Automation Software Upgrade Service Agreement Agreement between the purchaser of the Upgrade Service Package, called Customer in the following
5 CDs 1A43S1:UU 20 CDs 4) Extending the Upgrade Service After the 12 months has passed, the Upgrade Service will be automaticall extended by B&R for another 12 months unless B&R is requested by the customer [...] the Upgrade Service The Upgrade deliveries from B&R will be ended if B&R is requested by the customer in written form to end the Upgrade Service agreement 4 weeks before the 12 months have passed. [...] B&R SafeDESIGNER maintenance company upgrade -------- B&R Automation Software Upgrade Service Agreement Agreement between the purchaser of the Upgrade Service Package, called Customer in the following
Accessory 3-pin cage clamp terminal block, pitch 3.5
Power Panel PP320, 5.7" QVGA TFT color display with touch screen (resistive), 128 MB SDRAM, CompactFlash slot (type I), ETH 10/100, RS232, 2x USB, IP65 protection (front), 24 VDC (order screw clamp te
X2X keypad module, anthracite, 5 B&R illuminated ring keys, with 4-color illumination: Green, yellow, red, white (4 keys) / green, yellow, red, blue (1 key), X2X interface, 24 VDC, terminal blocks included
with this license key must be permanently stored in the customer account on the B&R licensing server. Support ≥ R4.2-05 P4 [...] permitted to be used if you have a valid 1TGAP42* dongle license for R, O or E systems. As soon as B&R makes a software container available in APROL for existing 1TGAP42* licenses, this license is no longer
SDL cable - 25 m
Välj land och språk