Provit 5000 Controller bus unit 4 slots (1 BR ISA, 3 half size ISA/PCI). 24 VDC power supply. For 5C5001.xx system units.
40 GB SATA hard disk, slide-in compact, 24/7 hard disk with extended temperature range. Note: See the manual for information about using this hard disk.
Provit 5000 Controller bus unit 4 slots (1 BR ISA, 3 half size ISA/PCI). 100-240 VAC power supply. For 5C5001.xx system units.
RS232/422/485 interface, for installation in an APC620, APC810 or PPC700.
Power Panel C30, 4.3", landscape format, fieldbus interfaces: 2x CAN bus. CPU and memory: 1 GHz (ARM Cortex-A8), 256 MB DDRAM, 8 kB FRAM, 512 MB onboard flash drive. Display and touch screen: 4.3", 480 x 272
SDL cable - 30 m
128 GB SSD MLC - Slide-in compact - Innodisk - SATA
1A43S0:U1 1 CD 1A43S0:U5 5 CDs 4) Extending the Upgrade Service After the 12 months has passed, the Upgrade Service will be automaticall extended by B&R for another 12 months unless B&R is requested by the customer [...] the Upgrade Service The Upgrade deliveries from B&R will be ended if B&R is requested by the customer in written form to end the Upgrade Service agreement 4 weeks before the 12 months have passed. [...] B&R SafeDESIGNER engineering multiple upgrade -------- B&R Automation Software Upgrade Service Agreement Agreement between the purchaser of the Upgrade Service Package, called Customer in the following
1A43S0:U1 1 CD 1A43S0:U5 5 CDs 4) Extending the Upgrade Service After the 12 months has passed, the Upgrade Service will be automaticall extended by B&R for another 12 months unless B&R is requested by the customer [...] the Upgrade Service The Upgrade deliveries from B&R will be ended if B&R is requested by the customer in written form to end the Upgrade Service agreement 4 weeks before the 12 months have passed. [...] B&R SafeDESIGNER engineering single upgrade -------- B&R Automation Software Upgrade Service Agreement Agreement between the purchaser of the Upgrade Service Package, called Customer in the following text
with this license key must be permanently stored in the customer account on the B&R licensing server. Support = R4.2-05 P4 [...] is only permitted to be used if you have a valid dongle license 1TGAP42* for Jaspersoft. As soon as B&R makes a software container in APROL available for existing 1TGAP42* Jaspersoft licenses, this license
Välj land och språk