period of one year. With the corporate license, it is permitted to license Automation Studio on a B&R Automation PC that is delivered with the machine if it can be guaranteed that only service personnel
Power Panel T80, 12.1", glass front, 2x Gigabit Ethernet (integrated switch). CPU and memory: 1.3 GHz dual core (Atom E3930), 1 GB RAM, 512 MB onboard flash drive. Display and touch screen: 12.1", 128
USB-iButton Adapter DS9490B. Notice: This Upgrade replaces existing APROL-license, old license(Dongle)is unvalid after recieving Upgrade-license, and must be returned to responsible B&R Sales Office. - AP.SW1-APR-3 [...] SW1-APR-3.2 APROL -SETUP & DOCUMENTATION R3.2 DVDs with actual Setup and actual APROL-Documentation, this package will be delivered independent of ordered SW-release as Release3.2! - WITH License for "Operating
www.stiftung-fbj.ch About B&R: B&R is a privately owned company with headquarters in Austria and offices all around the world. As a global leader in industrial automation, B&R combines state-of-the-art [...] Automation Studio software development environ-ment, B&R is constantly redefining the future of automation engineering. The innovative spirit that keeps B&R at the forefront of industrial automation is driven [...] B&R Switzerland supports young people starting their careers The foundation is now active with ten branches throughout Switzerland. With the "lehre4you" (teaching4you) training/coaching program, this
"The development of this new generation is an important step for B&R's PC/HMI portfolio and a clear signal to our customers that B&R takes the growing demands their applications in the areas of edge-based [...] IT networks, which is crucial for data-intensive tasks. Check out the B&R website to learn more about the Automation PC 3200 and B&R's full range of powerful, scalable, future-proof industrial PC and HMI [...] system adaptability. The new Automation PC 3200 delivers exactly that. As the latest generation of B&R's proven 3000 series, it brings 13th-generation Intel Core i processing, seamless system integration
B&R introduces new master modules for digital communication B&R is introducing two new master modules that each use IO-Link 1.1 to communicate digitally with four intelligent field devices: The X20DS438A [...] digital parameter sets continue to take the place of adjustable potentiometers. Intelligent connections B&R has long relied on the IO-Link communication standard to cover the final stretch from the I/O module
8LS motor series from B&R now even more powerful Motors from B&R's 8LS series have been completely revamped and are now more powerful than ever. A more compact housing, optimized design and additional [...] sizes are only some of the features that make these motors even more attractive and universal. B&R has improved the already very powerful and dynamic servo motors from the 8LS series in many details.
B&R offers servo drives with safety function Safely Limited Torque The B&R ACOPOS P3 servo drive is now also available with safety function Safely Limited Torque (SLT). This makes B&R one of the first
Continuous, secure monitoring of machine data from a distance with B&R B&R enables machine builders to establish a continuous connection to plants and machinery in the field. With LogTunnel, data from [...] in performance can be detected early to help maintain maximum availability. LogTunnel is feature of B&R's Secure Remote Maintenance solution . Secure Remote Maintenance lets you check in on plants and machinery
X20 bus module, coated, for double-width modules, 240 VAC keyed, internal I/O power supply connected through
Välj land och språk