drive components into the machine is a fundamental requirement for modular machine manufacturing. B&R has designed the ACOPOSremote distributed drive system to meet this requirement, allowing implementation
USB-iButton Adapter DS9490B. Notice: This Upgrade replaces existing APROL-license, old license(Dongle)is unvalid after recieving Upgrade-license, and must be returned to responsible B&R Sales Office. - AP.SW1-APR-3 [...] SW1-APR-3.2 APROL -SETUP & DOCUMENTATION R3.2 DVDs with actual Setup and actual APROL-Documentation, this package will be delivered independent of ordered SW-release as Release3.2! - WITH License for "Operating
X20 energy metering module, coated, 3 analog inputs, 480 VAC, 50/60 Hz, 4 analog inputs, 5 A AC, calculates effective, reactive and apparent power/energy, calculates RMS values, 240 V keyed, NetTime f
#ThinkAdaptive B&R portfolio B&R portfolio B&R has the most comprehensive automation portfolio on the market and the right solution for every industry. Seamless coordination between B&R products gives [...] quality. The B&R software ecosystem provides a powerful combination of integration and open standards that unlocks exciting possibilities. #ThisIsAutomation Open Connectivity Open Connectivity B&R's automation [...] B&R at drinktec 2025 September 15th - 19th, 2025 Trade fair Munich Claim your free ticket The world's leading trade fair for the beverage and liquid food industry Visit us at this year's drinktec 2025
B&R presenting solutions for tomorrow's machines in Hanover According to the Industry 4.0 working group, Smart Factories and the Internet of Things will be reality by 2025. B&R customers will not have [...] of open technologies," explains Markus Sandhöfner, managing director of B&R Germany. This requirement is already being met by B&R's Automation Studio software and the open-source POWERLINK and openSAFETY [...] technologies and solutions that make it possible to implement tomorrow's machines and systems today. B&R will be presenting their innovative range of products at the Hannover Messe in Hall 9, Booth D28. "The
based on PackML – B&R makes it easy With just a few mouse clicks, a convenient line monitoring system can be implemented using the APROL process and factory automation system from B&R. The solution is based
Interface card - 2x CAN interfaces - 1x X2X Link interface - 1x POWERLINK interface - 512 kB nvSRAM - For APC2x00/PPC2x00 - Only available with a new device
X20c PLC, coated, Atom 0.4 GHz (compatible), 512 MB DDR4 RAM, 1 MB SRAM, 1 GB onboard flash drive, removable application memory: CompactFlash, 1 insert slot for X20 interface modules, 2 USB interfaces
now be directly operated with B&R controllers. This is possible thanks to a POWERLINK interface on Stäubli's uniVAL drives that allows Generic Motion Control programs from B&R controllers to be transferred [...] this way, robotics engineers can use the uniform programming and operating environment provided by B&R controllers. Robots are connected to the network using POWERLINK, the real-time Ethernet standard.
B&R reduces development time by 67% with mapp technology B&R will be presenting its revolutionary new mapp technology at this year's SPS IPC Drives trade show. These modular software blocks simplify the [...] machine or system processes in the application software. mapp blocks are seamlessly integrated into B&R's automation software landscape. This means that any developer who works with Automation Studio can
Välj land och språk