1.6 GHz 4 GB RAM, 2x ETH, 1x USB removable application memory: 64 GB microSD card (included) with B&R-specific software image, terminal block 0TB1102.2100-01 included
X20 temperature input module, 2 thermocouple inputs, type J, K, N, S, B, R, E, C, T, single-channel galvanically isolated, NetTime function, 2x PT1000 integrated in terminal block X20TB1E for temperature
This helps fit the inverter perfectly into the B&R Motion concept and allows movements to be synchronized with the servo drives. Thanks to the integrated B&R Automation Studio environment, no other software [...] For complex machines and systems, B&R offers the ACOPOSinverter P84 with an integrated POWERLINK interface. It has a performance range of 0.37 to 500 kW. The P84 has a selection of onboard digital and
B&R's process control system offers manipulation-proof logging With B&R's APROL process control system, all configurations, operations and modifications performed throughout the system can be seamlessly [...] manipulation of signed logs and process documents. The workflow remains as intuitive and convenient as B&R customers have come to expect. Protect signed reports against manipulation Authorized personnel sign
summer interns working at Bernecker + Rainer More than 200 students will take part in internships at B&R's HQ in Eggelsberg this summer. They work in many different departments such as development, production [...] the personnel department. "In the district of Braunau, we are one of the most popular employers. At B&R, interns are provided assistance and trained to handle their new responsibilities. Individual assistance [...] all interns before being introduced to the respective area of responsibility by their supervisors. B&R works closely with HTL Braunau, as well as other educational institutes, in order to provide the best
B&R presents reACTION technology for ultrafast safety applications B&R is heralding a breakthrough in response times for safety technology. At the Hannover Messe, the automation specialists presented [...] reACTION technology achieves safety response times down to 100 microseconds. With this advancement, B&R is extending the use of reACTION technology into the area of safety applications. This technology makes
EWEA: B&R safety technology saves up to 50% At the EWEA trade show in Paris, France, B&R will present integrated safety technology that allows operators of wind turbines to save 30 to 50% in costs for [...] possible to perform comprehensive remote diagnostics on the safety application. Easier on the equipment B&R safety technology is completely integrated in the automation solution, giving it full access to data
B&R presents new product line at bauma At this year's bauma, B&R will be presenting its newly developed modular control and I/O system for mobile automation. Another highlight at Booth 314 in Hall A3 will [...] will be B&R's revolutionary mapp technology, which accelerates software development by an average of 67%. mapp technology simplifies development by encapsulating functionality in modular components. Simply
B&R's industrial controllers take performance to a whole new level. The new B&R X20CP3687X controller combines the performance of an industrial PC with the compact design of the X20 controller series [...] capabilities, the new module has exactly the same design and dimensions as all the other controllers in B&R's X20 series.
Impressionen User Meeting 2014 280 participants at the B&R USER Meeting in Salzburg The B&R User Meeting in Salzburg was met with great interest. Around 280 visitors from the machine and system manufacturing [...] department-wide automation concepts. At the two-day event, B&R showcased a mix of corporate speakers, independent experts and case studies from B&R customers. "The consistently high attendance figures prove [...] prove that this mix works well," said Hermann Obermair, Sales manager for B&R Austria, with satisfaction after the event. "Our customers know that we are not just presenting a product show, but are also
Välj land och språk