g reliably. But how sure are you that your cooling system is doing its job? A new I/O module from B&R's X20 series puts uncertainty to rest. It monitors environmental conditions in the control cabinet [...] module and immediately feeds condition data into the control application. Whether it's an existing B&R-automated machine or a new one, there is no extra wiring or any other hardware required. In larger [...] application. The added overhead causes many to shy away from a solution. But there is an easier way. B&R proves that with its X20CMR011 I/O module . The module is mounted on the DIN rail just as easily as
Braking resistor, 790 W, 33 R, IP20, terminals
New software package suppresses rotational sway. B&R has introduced a new function for crane control. Cranes that transport payloads suspended from sling systems can be particularly sensitive to rotation
simplifies management of machine variants Modular applications can now be implemented even more easily. B&R's new software component , mapp IO, makes it possible to add I/O modules at any time. This can happen
M.2 memory means faster access and higher capacity B&R is adding new mass memory options for its Automation PC 3100 and Panel PC 3100 industrial PCs. In addition to CFast cards, it is now also possible
Unique stepping movements controlled by B&R technology The Technical University of Liberec has introduced the second generation of its special service robot, the ROBOTUL® Vertical Climber 02, which uses [...] as the glass walls of buildings. Its safe and highly precise operation is guaranteed by an advanced B&R control system with compact ACOPOSmicro servo drives. The new approach taken by the Institute for
current protocol for communication security and associate its functionality with security goals Find the B&R cybersecurity support channels and know how to use them Create and manage self-signed and 3rd-party [...] Create firewall rules to make controllers harder to discover in the network Describe the use cases for B&R libraries ArCert and ArSsl Learning format Digital Classroom Online Duration 9 hours 1 day The duration
B&R recently announced plans to strengthen its presence in the medical device assemblymarket. We sat down with industry expert Fredrik Holmberg to learn how these companies have been dealing with the struggle [...] small batch sizes, and how adaptive manufacturing could provide relief. Fredrik Holmberg oversees B&R's global sales activities in the area of medical device assembly. Fredrik, let's start with the term [...] together. That process – called medical device assembly – can benefit enormously from automation. Why has B&R decided to enter the market now? Holmberg: The main reason is that our portfolio now includes specific
ACOPOSmulti auxiliary supply module, 32 A, AS, wall mounting
ACOPOS P3 servo drive, 1 digital multi-standard encoder interface per axis, 3x 200-480 VAC, 4.5 A, 1 axis, wall mounting, 2-row connector set
Välj land och språk