With the comprehensive Automation Studio 4 software package, B&R has forged an entirely new path when it comes to smart engineering. Many convenient automated functions as well as true-to-life architecture [...] complex programs," explains Dr. Hans Egermeier, who is the manager responsible for Automation Studio at B&R. He works in close cooperation with external usability experts to make sure that Automation Studio [...] During development, predefined visualization templates also accelerate the design of user interfaces. "B&R Automation Studio 4 not only helps create clearly structured software architecture when a project is
B&R presents the new ACOPOS P3 three-axis servo drive B&R presented the new ACOPOS P3 at the 2015 SPS IPC Drives trade show. With a power density of 6 amps per liter of space, this innovative system is [...] be implemented using virtual sensor technology. Safety included The ACOPOS P3 fits seamlessly into B&R's modular and fully scalable automation portfolio, allowing the creation and implementation of especially
Automation Studio calculates I/O power requirements The new Power Calculation function in Version 4.11 of B&R's Automation Studio engineering environment shows developers exactly where power supply modules are
our new campus and factory. In the upcoming two days we will take you into our world and show you B&R's strategic investments, clear srategies and the latest automation technologie innovations. Your direct
Real-time Ethernet onboard – Unlimited expansion possibilities B&R has expanded the X20 system to include a new series of compact controllers with integrated I/O. As with all X20 CPUs, additional I/O modules [...] different CPU frequencies: 200 MHz and 400 MHz. Depending on the variant, up to 256 MB RAM and 16 kB nonvolatile onboard RAM is available. A built-in flash drive is available to store up to 4 GB of application [...] times down to 1 μs using a function block library. Programming using the standard FBD editor in the B&R Automation Studio development environment is completely compliant with IEC 61131.
X20 energy metering module, coated, 3 analog inputs, 480 VAC, 50/60 Hz, 4 analog inputs, 5 A AC, calculates effective, reactive and apparent power/energy, calculates RMS values, 240 V keyed, NetTime f
Pick&Place pairs up perfectly with B&R's intelligent track systems," says Sebastian Brandstetter, product manager for integrated robotics at B&R. Robot and machine become one B&R is the world's only single-source [...] system and introduction of a new software solution, B&R is now changing that. "Pick-and-place applications have one very big advantage," explains B&R's product manger for integrated robotics, Sebastian [...] ace is basically a matter of logistics," says Brandstetter. You need to transport things from A to B as efficiently as possible. Simple as that may sound, it relies on some very complex calculations and
Interface card - 2x CAN interfaces - 1x X2X Link interface - 1x POWERLINK interface - 512 kB nvSRAM - For APC2x00/PPC2x00 - Only available with a new device
X20c PLC, coated, Atom 0.4 GHz (compatible), 512 MB DDR4 RAM, 1 MB SRAM, 1 GB onboard flash drive, removable application memory: CompactFlash, 1 insert slot for X20 interface modules, 2 USB interfaces
Power Panel T80, 12.1", glass front, 2x Gigabit Ethernet (integrated switch). CPU and memory: 1.3 GHz dual core (Atom E3930), 1 GB RAM, 512 MB onboard flash drive. Display and touch screen: 12.1", 128
Välj land och språk