B&R streamlines IP69K connectivity Stainless steel motors from B&R meet strict hygienic design standards and are now easier than ever to use. Employing a special connector, the motor can be connected and [...] up to 150°C exhibit a high standard of safety and reliability and therefore fit seamlessly into the B&R environment. Using the hybrid motor cable saves both time and money.
New muting modes from B&R make light curtains flexible With its new function blocks for programming network-integrated light curtains, B&R simplifies production of small batch sizes. Box muting, teach-in [...] Muting modes as function blocks Each muting mode is preprogrammed as a certified function block. B&R's advanced muting modes provide all the most commonly required options and make light curtains considerably
B&R expands motor selection with Hiperface DSL Safety The safety functions of the B&R ACOPOS P3 servo drive are now also available for motors with a safe Hiperface DSL encoder. Machine builders now have [...] transfer between motors and servo drives. Just like EnDat 2.2, HDSL Safety is compatible with all B&R safety functions. That includes functions such as Safely Limited Speed (SLS), Safe Operating Stop (SOS)
ACOPOS P3 With the new generation of the ACOPOS P3, B&R is setting new standards for performance, compact size… Read more TÜV Rheinland confirms B&R’s CRA Guide for POWERLINK The EU Cyber Resilience Act [...] a stent that ensures blood flow. Manufacturing these… Read more Our next steps for your step ahead B&R offers the products and services you need to succeed in a rapidly changing industry. Let's work together
industries. Thanks to its long-standing partnership with B&R, KSK is able to equip its machines with the latest automation technology. With B&R controllers and POWERLINK for communication, the PTA machines [...] Additional contact options for B&R: Local value provider Find a partner near you Take advantage of our global network for end customers. In addition to more than 200 B&R offices in over 70 countries around [...] have a global network of partners. B&R Value Providers work seamlessly with B&R to bring our products and services to your door. They combine in-depth knowledge of B&R technology with a deep understanding
summer interns working at Bernecker + Rainer More than 200 students will take part in internships at B&R's HQ in Eggelsberg this summer. They work in many different departments such as development, production [...] the personnel department. "In the district of Braunau, we are one of the most popular employers. At B&R, interns are provided assistance and trained to handle their new responsibilities. Individual assistance [...] all interns before being introduced to the respective area of responsibility by their supervisors. B&R works closely with HTL Braunau, as well as other educational institutes, in order to provide the best
Linux for B&R 12 - 64-bit - Multilingual - APC4100 (UEFI boot) - CPU Celeron C-6600HLE - CPU Core i3-11100HE / i5-11500HE - CPU Xeon w-1115MRE / w-11865MRE - Installation - Only available with a new device
X2X keypad module 6 B&R illuminated ring keys, 3-color (red, green, yellow), X2X interface, emergency switch-off button, 24 VDC power supply, IP65 protection (front), order 1x 0TB1108.8110 and 1x 0TB1104
X2X keypad module, white aluminum, 5 B&R illuminated ring keys, with 4-color illumination: Green, yellow, red, white (4 keys) / green, yellow, red, blue (1 key), X2X interface, 24 VDC, terminal blocks
X2X keypad module, anthracite, 3 B&R illuminated ring keys, with 4-color illumination: Green, yellow, red, white (2 keys) / green, yellow, red, blue (1 key), X2X interface, 24 VDC, terminal blocks included
Välj land och språk