ECAD DWL@DWL10000567774
screen Function keys System keys Front USB interface 5.7" VGA Analog resistive No No No 5.7" VGA No Yes Yes No 7.0" WVGA Analog resistive No No No 10.1" WXGA Analog resistive No No No 10.4" VGA Analog resistive [...] resistive Yes Yes Yes 10.4" VGA Analog resistive Yes Yes Yes 12.1" SVGA Analog resistive No No Yes 12.1" XGA Analog resistive No No No 12.1" WXGA Analog resistive No No No 15.0" XGA Analog resistive No No [...] Panel PC 2100 integrates all important interfaces, including 2x Gigabit Ethernet as well as 1x USB 2.0 and 1x USB 3.0. In addition, fieldbuses such as POWERLINK and CAN can be implemented via modular interface
X20 analog input module, 4 inputs, ±10 V or 0 to 20 mA / 4 to 20 mA, 13-bit converter resolution, configurable input filter
X20 terminal block, 12-pin, 24 VDC keyed
X20 power supply module, for bus controller and internal I/O power supply X2X Link power supply
MCAD DWL@DWL10000015567
Smart Sensor and Smart Camera can each be equipped with one of three image sensors, ranging from 1.3 to 5 megapixels. All three sensors are characterized by their large pixel size, high light sensitivity [...] Integrated into the machine network via an M12 hybrid connector, which also supplies the necessary 24 VDC power, the camera needs only a single cable. A second hybrid connection enables easy daisy-chain
tools needed for flexible production as envisioned in the Industry 4.0 concept." 700 new engineers in 5 years To ensure that its technologies remain on top in the automation industry, B&R invests nearly 15% [...] hours is invested in training and continued education. New subsidiary in Japan B&R is represented by 24 subsidiaries and nearly 200 offices in 75 countries around the world. "Our decentralized structure [...] local language." Just in the last 12 months, B&R has opened many new offices, including the company's 24th subsidiary – this time in Japan. A complete team of support, application and sales engineers started
Zertifikat DWL@DWL10000480475
Zertifikat DWL@DWL10000614385
Välj land och språk