DWL@DWL10000017643
| Version | Language | Operating System | Date | Size | Type | Download |
|---|---|---|---|---|---|---|
| 4.51 | * | Windows10, Windows11 | 05/26/2026 | 46 MB | ZIP | B_R_Key_Editor_4.51.zip |
| Description |
Key Editor With this software the keys and LEDs can be configured. More additional information about the Key Editor can be found in the Key Editor help. Error corrections - The NSIS installation system used by B&R can allow local attackers to extend their rights. CVE-2025-43715, CVSS: 8.1 (high) CVSS:3.1/AV:L/AC:H/PR:N/UI:N/S:C/C:H/I:H/A:H Changes - Added support for Windows 11 IoT Enterprise 2024 LTSC. |
|||||
| Version | Language | Operating System | Date | Size | Type | Download |
| 4.30 | * | Windows10 | 03/16/2022 | 48 MB | ZIP | B_R_Key_Editor_4.30.zip |
| Description |
Key Editor With this software the keys and LEDs can be configured. More additional information about the Key Editor can be found in the Key Editor help. Changes - Added support for PPC1200 devices. - Added support for the SDL to SDL4 3x Converter. For this reason, up to four AP9x3, AP1000 and AP5000 devices can now be added per link connector. - Added support for new AP5000 expansion units: * 5ACCKP03.185B-000 * 5ACCKP03.240C-000 * 5ACCKP05.185B-000 * 5ACCKP05.215C-000 * 5ACCKP05.240C-000 - Added support for new AP1000 panels: * 5AP1130.101D-000 * 5AP1130.121E-010 * 5AP1130.156C-010 * 5AP1130.215C-010 - Removed support for Windows 7 SP1, Windows Embedded Standard 7 SP1, Windows Embedded 8.1 Industry Pro and Windows 10 IoT Enterprise 2015 LTSB. - Removed support for APC620, APC810, APC820, PPC700 and PPC800 devices since these devices have been discontinued. - Removed support for some AP800 panels since these devices were never in serial production: * 5AP820.1505-10 * 5AP880.1505-10 - Removed support for some AP800 extension units since these devices were never in serial production: * 5AC800.EXT1-10 * 5AC800.EXT2-10 * 5AC800.EXT2-11 * 5AC800.EXT3-10 * 5AC800.EXT3-11 * 5AC800.EXT3-12 * 5AC800.EXT3-13 * 5AC800.EXT3-14 * 5AC800.EXT3-15 - Removed support for MP40 devices since these devices have been discontinued. - Removed support for AP830 panels since these devices have been discontinued. - Removed support for AP9xD panels since these devices have been discontinued. Error corrections - The expansion unit of an AP5000 was not displayed in the hardware tree when an existing panel was copied or cut and pasted as a new panel. - The shortcut menu of the panel could not be opened in the hardware tree on an AP5000 with expansion unit. - If an AP5000 with expansion unit was marked in the hardware tree and the DEL key was pressed, a key was deleted instead of the panel. |
|||||