DWL@DWL10000017643

Versión Idioma
Sistema operativo
Fecha
Tamaño
Tipo Descargar
4.51 * Windows10, Windows11 26.05.2026 46 MB ZIP B_R_Key_Editor_4.51.zip
Descripción Key Editor

With this software the keys and LEDs can be configured.

More additional information about the Key Editor can be found in the Key Editor help.

Error corrections

- The NSIS installation system used by B&R can allow local
attackers to extend their rights.
CVE-2025-43715, CVSS: 8.1 (high)
CVSS:3.1/AV:L/AC:H/PR:N/UI:N/S:C/C:H/I:H/A:H

Changes

- Added support for Windows 11 IoT Enterprise 2024 LTSC.
Versión Idioma
Sistema operativo
Fecha
Tamaño
Tipo Descargar
4.30 * Windows10 16.03.2022 48 MB ZIP B_R_Key_Editor_4.30.zip
Descripción Key Editor

With this software the keys and LEDs can be configured.

More additional information about the Key Editor can be found in the Key Editor help.

Changes

- Added support for PPC1200 devices.
- Added support for the SDL to SDL4 3x Converter. For this reason, up to four AP9x3, AP1000 and AP5000 devices can now be added per link connector.
- Added support for new AP5000 expansion units:
* 5ACCKP03.185B-000
* 5ACCKP03.240C-000
* 5ACCKP05.185B-000
* 5ACCKP05.215C-000
* 5ACCKP05.240C-000
- Added support for new AP1000 panels:
* 5AP1130.101D-000
* 5AP1130.121E-010
* 5AP1130.156C-010
* 5AP1130.215C-010
- Removed support for Windows 7 SP1, Windows Embedded Standard 7 SP1, Windows Embedded 8.1 Industry Pro and Windows 10 IoT Enterprise 2015 LTSB.
- Removed support for APC620, APC810, APC820, PPC700 and PPC800 devices since these devices have been discontinued.
- Removed support for some AP800 panels since these devices were never in serial production:
* 5AP820.1505-10
* 5AP880.1505-10
- Removed support for some AP800 extension units since these devices were never in serial production:
* 5AC800.EXT1-10
* 5AC800.EXT2-10
* 5AC800.EXT2-11
* 5AC800.EXT3-10
* 5AC800.EXT3-11
* 5AC800.EXT3-12
* 5AC800.EXT3-13
* 5AC800.EXT3-14
* 5AC800.EXT3-15
- Removed support for MP40 devices since these devices have been discontinued.
- Removed support for AP830 panels since these devices have been discontinued.
- Removed support for AP9xD panels since these devices have been discontinued.

Error corrections

- The expansion unit of an AP5000 was not displayed in the hardware tree when an existing panel was copied or cut and pasted as a new panel.
- The shortcut menu of the panel could not be opened in the hardware tree on an AP5000 with expansion unit.
- If an AP5000 with expansion unit was marked in the hardware tree and the DEL key was pressed, a key was deleted instead of the panel.

Descargas relacionadas

Key Editor help

Loading
Volver al listado

Seleccione país e idioma

B&R Logo