DWL@DWL10000318439
| 版本 | 语言 | 操作系统 | 日期 | 尺寸 | 类型 | 下载 |
|---|---|---|---|---|---|---|
| 1.44 | * | 11/28/2022 | 4 MB | ZIP | UPG_APC2100_PPC2100_BIOS_BRBY_V0144.zip | |
| 描述 |
BIOS Upgrade Bay Trail APC2100/PPC2100 BIOS Upgrade for Bay Trail chipset APC2100 BIOS Upgrade for 5APC2100.BY01-000, 5APC2100.BY11-000, 5APC2100.BY22-000, 5APC2100.BY34-000, 5APC2100.BY44-000, 5APC2100.BY48-000 PPC2100 BIOS Upgrade for 5PPC2100.BY01-000, 5PPC2100.BY11-000, 5PPC2100.BY22-000, 5PPC2100.BY34-000, 5PPC2100.BY44-000, 5PPC2100.BY48-000 PPC2100 BIOS Upgrade for 5PPC2100.BY01-001, 5PPC2100.BY11-001, 5PPC2100.BY22-001, 5PPC2100.BY34-001, 5PPC2100.BY44-001 PPC2100 BIOS Upgrade for 5PPC2100.BY01-002, 5PPC2100.BY11-002, 5PPC2100.BY22-002, 5PPC2100.BY34-002, 5PPC2100.BY44-002, 5PPC2100.BY48-002 ---------------------------------------------------------------- ATTENTION! Possible upgrade problems and version dependency ---------------------------------------------------------------- 1. Do not reset or power off the device during the upgrade process !!! 2. XHCI mode in the USB Configuration Setup page must be set for - Win8.1/Win10 to Enabled and - Win7 to Smart Auto if USB3.0 support is desired. With XHCI mode set to Smart Auto under Win8.1/Win10, only USB2.0 is supported. Default value for XHCI mode option is Smart Auto. 3. If problems occur during shutdown or reboot under Debian 8, it may help to disable the USB 3.0 function. In order to do this, the XHCI controller must be set to disabled in BIOS in the USB configuration page. ---------------------------------------------------------------- Version 01.44 / 10/06/2022 / MIK !MANDATORY UPDATE! ---------------------------------------------------------------- Content LIESMICH.txt 01.44 NEW README.txt 01.44 NEW STARTUP.nsh 01.44 NEW FPT64.efi 01.1.0.1073 FPARTS.txt 02.7.8 BRBYR144.bin 01.44 NEW Change(s) BIOS: - B&R Bootlogo updated (B&R Brand Refresh). - New BIOS setup node Firmware PLL Range in the Graphics (IGD) Configuration setup page. Default value is Auto, sets based on the used resolution the correct value. ATTENTION! Possible upgrade problems and version dependency, see above. |
|||||
| 版本 | 语言 | 操作系统 | 日期 | 尺寸 | 类型 | 下载 |
| 1.43 | * | 03/16/2020 | 4 MB | ZIP | UPG_APC2100_PPC2100_BIOS_BRBY_V0143.zip | |
| 描述 |
BIOS Upgrade Bay Trail APC2100/PPC2100 BIOS Upgrade for Bay Trail chipset APC2100 BIOS Upgrade for 5APC2100.BY01-000, 5APC2100.BY11-000, 5APC2100.BY22-000, 5APC2100.BY34-000, 5APC2100.BY44-000, 5APC2100.BY48-000 PPC2100 BIOS Upgrade for 5PPC2100.BY01-000, 5PPC2100.BY11-000, 5PPC2100.BY22-000, 5PPC2100.BY34-000, 5PPC2100.BY44-000, 5PPC2100.BY48-000 PPC2100 BIOS Upgrade for 5PPC2100.BY01-001, 5PPC2100.BY11-001, 5PPC2100.BY22-001, 5PPC2100.BY34-001, 5PPC2100.BY44-001 PPC2100 BIOS Upgrade for 5PPC2100.BY01-002, 5PPC2100.BY11-002, 5PPC2100.BY22-002, 5PPC2100.BY34-002, 5PPC2100.BY44-002, 5PPC2100.BY48-002 ---------------------------------------------------------------- ATTENTION! Possible upgrade problems and version dependency ---------------------------------------------------------------- 1. Do not reset or power off the device during the upgrade process !!! 2. XHCI mode in the USB Configuration Setup page must be set for - Win8.1/Win10 to Enabled and - Win7 to Smart Auto if USB3.0 support is desired. With XHCI mode set to Smart Auto under Win8.1/Win10, only USB2.0 is supported. Default value for XHCI mode option is Smart Auto. 3. If problems occur during shutdown or reboot under Debian 8, it may help to disable the USB 3.0 function. In order to do this, the XHCI controller must be set to disabled in BIOS in the USB configuration page. ---------------------------------------------------------------- Version 01.43 / 01/31/2020 / MIK !MANDATORY UPDATE! ---------------------------------------------------------------- Content LIESMICH.txt 01.43 NEW README.txt 01.43 NEW STARTUP.nsh 01.43 NEW FPT64.efi 01.1.0.1073 FPARTS.txt 02.7.8 BRBYR143.bin 01.43 NEW Change(s) BIOS: - Intel Microcode for Bay Trail CPUs updated. The Intel microcode used in BIOS version V01.41 caused the behavior of an existing Windows Image that the Ethernet interfaces are renumbered and the screen resolution is set to default. This behavior occurred only with existing Windows images if the BIOS from versions less or equal V01.40 is updated to V01.41. With a new Windows installation this behavior did not occur. For this reason, the BIOS V1.41 is no longer delivered. Described topic can also be observed with a BIOS Update from V1.41 to V1.43. The BIOS V01.43 is now compatible with BIOS V01.40 again. ATTENTION! Possible upgrade problems and version dependency, see above. |
|||||
| 版本 | 语言 | 操作系统 | 日期 | 尺寸 | 类型 | 下载 |
| 1.40 | * | 09/03/2018 | 3 MB | ZIP | UPG_APC2100_PPC2100_BIOS_BRBY_V0140.zip | |
| 描述 |
BIOS Upgrade Bay Trail APC2100/PPC2100 BIOS Upgrade for Bay Trail chipset APC2100 BIOS Upgrade for 5APC2100.BY01-000, 5APC2100.BY11-000, 5APC2100.BY22-000, 5APC2100.BY34-000, 5APC2100.BY44-000, 5APC2100.BY48-000 PPC2100 BIOS Upgrade for 5PPC2100.BY01-000, 5PPC2100.BY11-000, 5PPC2100.BY22-000, 5PPC2100.BY34-000, 5PPC2100.BY44-000, 5PPC2100.BY48-000 PPC2100 BIOS Upgrade for 5PPC2100.BY01-001, 5PPC2100.BY11-001, 5PPC2100.BY22-001, 5PPC2100.BY34-001, 5PPC2100.BY44-001 PPC2100 BIOS Upgrade for 5PPC2100.BY01-002, 5PPC2100.BY11-002, 5PPC2100.BY22-002, 5PPC2100.BY34-002, 5PPC2100.BY44-002, 5PPC2100.BY48-002 ---------------------------------------------------------------- ATTENTION! Possible upgrade problems and version dependency ---------------------------------------------------------------- 1. Do not reset or power off the device during the upgrade process !!! 2. XHCI mode in the USB Configuration Setup page must be set for - Win8.1/Win10 to Enabled and - Win7 to Smart Auto if USB3.0 support is desired. With XHCI mode set to Smart Auto under Win8.1/Win10, only USB2.0 is supported. Default value for XHCI mode option is Smart Auto. 3. If problems occur during shutdown or reboot under Debian 8, it may help to disable the USB 3.0 function. In order to do this, the XHCI controller must be set to disabled in BIOS in the USB configuration page. ---------------------------------------------------------------- Version 01.40 / 07/11/2018 / MIK !MANDATORY UPDATE! ---------------------------------------------------------------- Content LIESMICH.txt 01.40 NEW README.txt 01.40 NEW STARTUP.nsh 01.40 NEW FPT64.efi 01.1.0.1073 FPARTS.txt 02.7.8 BRBYR140.bin 01.40 NEW Change(s) BIOS: - Intel Microcode for Ivy-Bridge CPUs updated (CVE-2017-5715). - Support for B&R Hypervisor. - Support for UEFI PXE Boot. ATTENTION! Possible upgrade problems and version dependency, see above. |
|||||
| 版本 | 语言 | 操作系统 | 日期 | 尺寸 | 类型 | 下载 |
| 1.33 | * | 01/04/2018 | 3 MB | ZIP | UPG_APC2100_PPC2100_BIOS_BRBY_V0133.zip | |
| 描述 |
BIOS Upgrade Bay Trail APC2100/PPC2100 BIOS Upgrade for Bay Trail chipset APC2100 BIOS Upgrade for 5APC2100.BY01-000, 5APC2100.BY11-000, 5APC2100.BY22-000, 5APC2100.BY34-000, 5APC2100.BY44-000, 5APC2100.BY48-000 PPC2100 BIOS Upgrade for 5PPC2100.BY01-000, 5PPC2100.BY11-000, 5PPC2100.BY22-000, 5PPC2100.BY34-000, 5PPC2100.BY44-000, 5PPC2100.BY48-000 PPC2100 BIOS Upgrade for 5PPC2100.BY01-001, 5PPC2100.BY11-001, 5PPC2100.BY22-001, 5PPC2100.BY34-001, 5PPC2100.BY44-001 PPC2100 BIOS Upgrade for 5PPC2100.BY01-002, 5PPC2100.BY11-002, 5PPC2100.BY22-002, 5PPC2100.BY34-002, 5PPC2100.BY44-002, 5PPC2100.BY48-002 ---------------------------------------------------------------- ATTENTION! Possible upgrade problems and version dependency ---------------------------------------------------------------- 1. Do not reset or power off the device during the upgrade process !!! 2. XHCI mode in the USB Configuration Setup page must be set for - Win8.1/Win10 to Enabled and - Win7 to Smart Auto if USB3.0 support is desired. With XHCI mode set to Smart Auto under Win8.1/Win10, only USB2.0 is supported. Default value for XHCI mode option is Smart Auto. 3. If problems occur during shutdown or reboot under Debian 8, it may help to disable the USB 3.0 function. In order to do this, the XHCI controller must be set to disabled in BIOS in the USB configuration page. ---------------------------------------------------------------- Version 01.33 / 08/01/2017 / MIK !MANDATORY UPDATE! ---------------------------------------------------------------- Contents LIESMICH.txt 01.33 NEW README.txt 01.33 NEW STARTUP.nsh 01.33 NEW FPT64.efi 01.1.0.1073 FPARTS.txt 02.7.8 BRBYR133.bin 01.33 NEW Change(s) BIOS: - Enhancements DMI-BIOS in Type 1 (System Information), the entry "SKU Number" is now filled with the MAIN BIOS Version or OEM BIOS Version if present. The entry "Family" is filled with the CPU board name. - Reserved MTCX memory is enhanced with the io-area starting at 4000h with a length of 256 bytes. - New B&R bootlogo. ATTENTION! Possible upgrade problems and version dependency, see above. |
|||||
| 版本 | 语言 | 操作系统 | 日期 | 尺寸 | 类型 | 下载 |
| 1.32 | * | 09/06/2016 | 3 MB | ZIP | UPG_APC2100_PPC2100_BIOS_BRBY_V0132.zip | |
| 描述 |
BIOS Upgrade Bay Trail APC2100/PPC2100 BIOS Upgrade for Bay Trail chipset APC2100 BIOS Upgrade for 5APC2100.BY01-000, 5APC2100.BY11-000, 5APC2100.BY22-000, 5APC2100.BY34-000, 5APC2100.BY44-000 PPC2100 BIOS Upgrade for 5PPC2100.BY01-000, 5PPC2100.BY11-000, 5PPC2100.BY22-000, 5PPC2100.BY34-000, 5PPC2100.BY44-000 PPC2100 BIOS Upgrade for 5PPC2100.BY01-001, 5PPC2100.BY11-001, 5PPC2100.BY22-001, 5PPC2100.BY34-001, 5PPC2100.BY44-001 PPC2100 BIOS Upgrade for 5PPC2100.BY01-002, 5PPC2100.BY11-002, 5PPC2100.BY22-002, 5PPC2100.BY34-002, 5PPC2100.BY44-002 ---------------------------------------------------------------- ATTENTION! Possible upgrade problems and version dependency ---------------------------------------------------------------- 1. Do not reset or power off the device during the upgrade process !!! 2. XHCI mode in the USB Configuration Setup page must be set for - Win8.1/Win10 to Enabled and - Win7 to Smart Auto if USB3.0 support is desired. With XHCI mode set to Smart Auto under Win8.1/Win10, only USB2.0 is supported. Default value for XHCI mode option is Smart Auto. 3. If problems occur during shutdown or reboot under Debian 8, it may help to disable the USB 3.0 function. In order to do this, the XHCI controller must be set to disabled in BIOS in the USB configuration page. ---------------------------------------------------------------- Version 01.32 / 09/05/2016 / MIK !MANDATORY UPDATE! ---------------------------------------------------------------- Contents LIESMICH.txt 01.32 NEW README.txt 01.32 NEW STARTUP.nsh 01.32 NEW FPT64.efi 01.1.0.1073 FPARTS.txt 02.7.8 BRBYR132.bin 01.32 NEW Change(s) BIOS: - Bugfix: in very rare cases, short sporadic display flickering can occur. Until now this effect is only seen on panels with HD or FHD resolution in combination with the PPC2100. APC2100 system is not affected. ATTENTION! Possible upgrade problems and version dependency, see above. |
|||||
| 版本 | 语言 | 操作系统 | 日期 | 尺寸 | 类型 | 下载 |
| 1.31 | * | 08/25/2016 | 3 MB | ZIP | UPG_APC2100_PPC2100_BIOS_BRBY_V0131.zip | |
| 描述 |
BIOS Upgrade Bay Trail APC2100/PPC2100 BIOS Upgrade for Bay Trail chipset APC2100 BIOS Upgrade for 5APC2100.BY01-000, 5APC2100.BY11-000, 5APC2100.BY22-000, 5APC2100.BY34-000, 5APC2100.BY44-000 PPC2100 BIOS Upgrade for 5PPC2100.BY01-000, 5PPC2100.BY11-000, 5PPC2100.BY22-000, 5PPC2100.BY34-000, 5PPC2100.BY44-000 PPC2100 BIOS Upgrade for 5PPC2100.BY01-001, 5PPC2100.BY11-001, 5PPC2100.BY22-001, 5PPC2100.BY34-001, 5PPC2100.BY44-001 PPC2100 BIOS Upgrade for 5PPC2100.BY01-002, 5PPC2100.BY11-002, 5PPC2100.BY22-002, 5PPC2100.BY34-002, 5PPC2100.BY44-002 ---------------------------------------------------------------- ATTENTION! Possible upgrade problems and version dependency ---------------------------------------------------------------- 1. Do not reset or power off the device during the upgrade process !!! 2. XHCI mode in the USB Configuration Setup page must be set for - Win8.1/Win10 to Enabled and - Win7 to Smart Auto if USB3.0 support is desired. With XHCI mode set to Smart Auto under Win8.1/Win10, only USB2.0 is supported. Default value for XHCI mode option is Smart Auto. 3. If problems occur during shutdown or reboot under Debian 8, it may help to disable the USB 3.0 function. In order to do this, the XHCI controller must be set to disabled in BIOS in the USB configuration page. ---------------------------------------------------------------- Version 01.31 / 06/13/2016 / MIK !MANDATORY UPDATE! ---------------------------------------------------------------- Contents LIESMICH.txt 01.31 NEW README.txt 01.31 NEW STARTUP.nsh 01.31 NEW FPT64.efi 01.1.0.1073 FPARTS.txt 02.7.8 BRBYR131.bin 01.31 NEW Change(s) BIOS: - Updated Phoenix BIOS for Baytrail Platform to the newest version. - Updated microcode for Baytrail CPUs. - Updated Intel vBIOS. - All BIOS setup strings and options simplified to Enabled/ Disabled. - All known problems regarding "Load Setup Defaults" fixed. - Optimized settings of the PME-Mode for the internal function test. - The firmware version of a connected SDLT/SDL3T transmitter is shown in the OEM features setup page. - Optimized LVDS power sequenzing and timing. ATTENTION! Possible upgrade problems and version dependency, see above. |
|||||
| 版本 | 语言 | 操作系统 | 日期 | 尺寸 | 类型 | 下载 |
| 1.23 | * | 11/16/2015 | 3 MB | ZIP | UPG_APC2100_PPC2100_BIOS_BRBY_V0123.zip | |
| 描述 |
BIOS Upgrade Bay Trail APC2100/PPC2100 BIOS Upgrade for Bay Trail chipset APC2100 BIOS Upgrade for 5APC2100.BY01-000, 5APC2100.BY11-000, 5APC2100.BY22-000, 5APC2100.BY34-000, 5APC2100.BY44-000 PPC2100 BIOS Upgrade for 5PPC2100.BY01-000, 5PPC2100.BY11-000, 5PPC2100.BY22-000, 5PPC2100.BY34-000, 5PPC2100.BY44-000 PPC2100 BIOS Upgrade for 5PPC2100.BY01-001, 5PPC2100.BY11-001, 5PPC2100.BY22-001, 5PPC2100.BY34-001, 5PPC2100.BY44-001 ---------------------------------------------------------------- ATTENTION! Possible upgrade problems and version dependency ---------------------------------------------------------------- 1. Do not reset or power off the device during the upgrade process !!! 2. XHCI mode in the USB Configuration Setup page must be set for - Win8.1 to Enabled and - Win7 to Smart Auto if USB3.0 support is desired. With XHCI mode set to Smart Auto under Win8.1, only USB2.0 is supported. Default value for XHCI mode option is Smart Auto. ---------------------------------------------------------------- Version 01.23 / 10/19/2015 !MANDATORY UPDATE! ---------------------------------------------------------------- Contents LIESMICH.txt 01.23 NEW README.txt 01.23 NEW STARTUP.nsh 01.23 NEW FPT64.efi 01.1.0.1073 FPARTS.txt 02.7.8 BRBYR123.bin 01.23 NEW Change(s) BIOS: - Bugfix: Realtime Environment. The C1E power mode state was active on the CPU although the Realtime Environment was enabled in BIOS. - Optimized memory allocation for EFI boot services. Default about 130MB more main memory was reserved for full EFI boot service Support, this is typically not necessary. Now it is possible to configure the EFI memory allocation in BIOS using the BIOS setup option "EFI BS Memory Allocation". The default value is disabled. - Updated microcode for Baytrail CPUs. - The brightness setting in the BIOS for every Panel is now written to the MTCX at every boot, independent of the SDL status. ATTENTION! Possible upgrade problems and version dependency, see above. |
|||||
| 版本 | 语言 | 操作系统 | 日期 | 尺寸 | 类型 | 下载 |
| 1.21 | * | 06/16/2015 | 3 MB | ZIP | UPG_APC2100_PPC2100_BIOS_BRBY_V0121.zip | |
| 描述 |
BIOS Upgrade Bay Trail APC2100/PPC2100 BIOS Upgrade for Bay Trail chipset APC2100 BIOS Upgrade for 5APC2100.BY01-000, 5APC2100.BY11-000, 5APC2100.BY22-000, 5APC2100.BY34-000, 5APC2100.BY44-000 PPC2100 BIOS Upgrade for 5PPC2100.BY01-000, 5PPC2100.BY11-000, 5PPC2100.BY22-000, 5PPC2100.BY34-000, 5PPC2100.BY44-000 PPC2100 BIOS Upgrade for 5PPC2100.BY01-001, 5PPC2100.BY11-001, 5PPC2100.BY22-001, 5PPC2100.BY34-001, 5PPC2100.BY44-001 ---------------------------------------------------------------- ATTENTION! Possible upgrade problems and version dependency ---------------------------------------------------------------- 1. Do not reset or power off the device during the upgrade process !!! 2. XHCI mode in the USB Configuration Setup page must be set for - Win8.1 to Enabled and - Win7 to Smart Auto if USB3.0 support is desired. With XHCI mode set to Smart Auto under Win8.1, only USB2.0 is supported. Default value for XHCI mode option is Smart Auto. ---------------------------------------------------------------- Version 01.21 / 06/08/2015 !MANDATORY UPDATE! ---------------------------------------------------------------- Contents LIESMICH.txt 01.21 NEW README.txt 01.21 NEW STARTUP.nsh 01.21 NEW FPT64.efi 01.1.0.1073 FPARTS.txt 02.7.8 BRBYR121.bin 01.21 NEW Change(s) BIOS: - Workaround: Hibernate problem under Win8.1 with XHCI mode option set to Smart Auto. XHCI mode in the USB Configuration Setup page must be set for + Win8.1 to Enabled and + Win7 to Smart Auto if USB3.0 support is desired. With XHCI mode set to Smart Auto under Win8.1, only USB2.0 is supported. Default value for XHCI mode option is Smart Auto. ATTENTION! Possible upgrade problems and version dependency, see above. |
|||||
| 版本 | 语言 | 操作系统 | 日期 | 尺寸 | 类型 | 下载 |
| 1.20 | * | 06/03/2015 | 3 MB | ZIP | UPG_APC2100_PPC2100_BIOS_BRBY_V0120.zip | |
| 描述 |
BIOS Upgrade Bay Trail APC2100/PPC2100 BIOS Upgrade for Bay Trail chipset APC2100 BIOS Upgrade for 5APC2100.BY01-000, 5APC2100.BY11-000, 5APC2100.BY22-000, 5APC2100.BY34-000, 5APC2100.BY44-000 PPC2100 BIOS Upgrade for 5PPC2100.BY01-000, 5PPC2100.BY11-000, 5PPC2100.BY22-000, 5PPC2100.BY34-000, 5PPC2100.BY44-000 PPC2100 BIOS Upgrade for 5PPC2100.BY01-001, 5PPC2100.BY11-001, 5PPC2100.BY22-001, 5PPC2100.BY34-001, 5PPC2100.BY44-001 ---------------------------------------------------------------- ATTENTION! Possible upgrade problems and version dependency ---------------------------------------------------------------- 1. Do not reset or power off the device during the upgrade process !!! ---------------------------------------------------------------- Version 01.20 / 04/29/2015 !MANDATORY UPDATE! ---------------------------------------------------------------- Contents LIESMICH.txt 01.20 NEW README.txt 01.20 NEW STARTUP.nsh 01.20 NEW FPT64.efi 01.1.0.1073 FPARTS.txt 02.7.8 BRBYR120.bin 01.20 NEW Change(s) BIOS: - Updated Phoenix BIOS for Baytrail Platform to the newest version. - Added support P-State features. - Added lock mechansim XHCI to EHCI controller, therefor it is not possible to lock the BIOS. - Added Support for OEM Logo feature. - Added Support for Extended Temperature Memory Feature. - Bugfix: Eject Media Tray icon. - Bugfix: CTP (Ctritical Trip Point). - Folllowing setup entrys removed, not valid for Baytrail CPU or Gfx: + Spread Spectrum Clock option from dem Gfx menu. + Turbo Mode option from CPU menu. + Hyperthreading option from CPU menu. - Realtime Environment switch shifted from OEM menu to Miscellaneous menu. - Bugfix: it was possible to remove a IF-Option using the "safely remove HW icon" in Windows OS systems. - Bugfix: removed the braces for the USB devices under Boot Device Configuration (some tools may have problems with this special characters). - Updated microcode for Baytrail CPUs. - CSM Support set fix to YES. ATTENTION! Possible upgrade problems and version dependency, see above. |
|||||
| 版本 | 语言 | 操作系统 | 日期 | 尺寸 | 类型 | 下载 |
| 1.14 | * | 12/17/2014 | 3 MB | ZIP | UPG_APC2100_PPC2100_BIOS_BRBY_V0114.zip | |
| 描述 |
BIOS Upgrade Bay Trail APC2100/PPC2100 BIOS Upgrade for Bay Trail chipset APC2100 BIOS Upgrade for 5APC2100.BY01-000, 5APC2100.BY11-000, 5APC2100.BY22-000, 5APC2100.BY34-000, 5APC2100.BY44-000 PPC2100 BIOS Upgrade for 5PPC2100.BY01-000, 5PPC2100.BY11-000, 5PPC2100.BY22-000, 5PPC2100.BY34-000, 5PPC2100.BY44-000 ---------------------------------------------------------------- Version 01.14 / 12/05/2014 !MANDATORY UPDATE! ---------------------------------------------------------------- Contents LIESMICH.txt 01.14 NEW README.txt 01.14 NEW STARTUP.nsh 01.14 NEW FPT64.efi 01.1.0.1073 FPARTS.txt 02.7.8 BRBYR114.bin 01.14 NEW Change(s) BIOS: - BIOS enhancement for the Realtime Environment node implemented. For that also a MTCX version starting with V00.20 is necessary. - Default value changed from enable to disable for all PCIe Root Ports. - Auto mode for PCI MMIO size implemented. - Bugfix: S3 (suspend to RAM) under Win7. - Bugfix: Security in user mode. - Bugfix: Default values for the serial comports. - Bugfix: Reading day of week from RTC. ATTENTION! Possible upgrade problems and version dependency, see above. |
|||||