Good automation runs deep
and Bauer Maschinen GmbH. MeBo 200 is capable of working at depths of up to 2,500 meters, where it can drill 200 meters into the seabed. The core samples it obtains provide valuable insight into the sediment [...] and geology of the seabed. MeBo 200 is capable of working at depths of up to 2,500 meters, where it can drill 200 meters into the seabed. MeBo 200 is mounted in a frame that fits nicely into a 20-foot container [...] Above them, two more monitors display live video from eight underwater cameras, so the operators can keep a close eye on the largely manual drilling process. All the data comes together in the B&R APROL