DWL@DWL10000724404
| Version | Langue | Système d'exploitation | Date | Taille | Type | Téléchargement |
|---|---|---|---|---|---|---|
| 6.5.0.3 | * | 06/03/2026 | 53 Mo | EXE | AS6_TP_mappFramework_6.5.0.3.exe | |
| Description |
mapp Framework Now only on Github as a Community project, please open this link: https://github.com/br-automation-community/mapp-Framework-6 |
|||||
| Version | Langue | Système d'exploitation | Date | Taille | Type | Téléchargement |
| 1.5.0.0 | * | 03/04/2024 | 143 Mo | EXE | AS4_TP_mappFramework_1.5.0.0.exe | |
| Description |
mapp Framework Github link: https://github.com/br-automation-com/mapp-Framework/releases/tag/V1.5.0 Framework - Description mapp Audit: Improved the usability of the audit configuration dialog box mapp Axis / Cockpit: The AxisMgr template task is now not added to the software configuration, as opposed to before where it was automatically added but disabled mapp File: Improved the usability of the FIFO dialog box mapp Recipe: General reorganization and optimization to make the recipe system more robust and easier to extend Import Tool: Import the file device definitions depending on the AR version, in order to allow AR versions less than A4.91. For AR =A4.91, the file devices use USER_PATH. Updated the import tool to allow mixing mapp versions starting with version 5.24 and beyond Improved the error message if the import fails due to a previous git reset command The import tool will now detect existing .vis files within sub-packages of the mapp View package, as opposed to only .vis files in the root directory Misc: Updated to the new mapp Framework logo |
|||||
| Version | Langue | Système d'exploitation | Date | Taille | Type | Téléchargement |
| 1.4.0.0 | * | 03/07/2023 | 139 Mo | EXE | AS4_TP_mappFramework_1.4.0.0.exe | |
| Description |
mapp Framework Github link: https://github.com/br-automation-com/mapp-Framework/releases/tag/V1.4.0 Framework - Description VC4: Added a new VC4 front end for all available framework components mapp Axis / Cockpit: Updated the reference file organization to make it easier to add additional axes Updated the conditions to get into the READY state (checks if the Parameter and/or Configuration change option is used or not, and if so, wait until it is finished) Separated the HomeRestorePos variable to make it easier to add additional axes Added an alarm line to the mapp View front end mapp PackML: New framework component mapp Recipe: Improved the process for editing the default recipe names mapp Report: Bugfix - advanced reports were getting created as simple reports Import Tool: Updates to support the option for a VC4 front end Automatically increase the stack size of task class 8 Bugfix - TrakMap was not importing correctly via the framework importer Documentation: Improved the German translation of the Help file |
|||||
| Version | Langue | Système d'exploitation | Date | Taille | Type | Téléchargement |
| 1.3.1.0 | * | 21/03/2023 | 94 Mo | EXE | AS4_TP_mappFramework_1.3.1.0.exe | |
| Description |
mapp Framework Github link: https://github.com/br-automation-com/mapp-Framework/releases/tag/v1.3.1 Framework - Description mapp Axis: Improved the documentation regarding the necessary requirements for converting from a pure virtual axis to a physical axis New type member for v1.3 (ModeManual) was missing from the AxisMgr.typ file in the AxisTemplate Miscellaneous: Improved transfer robustness for the situation that you use transfer settings "Keep PV Values" along with "Installation during task operation" |
|||||
| Version | Langue | Système d'exploitation | Date | Taille | Type | Téléchargement |
| 1.3.0.0 | * | 01/03/2023 | 94 Mo | EXE | AS4_TP_mappFramework_1.3.0.0.exe | |
| Description |
mapp Framework Github link: https://github.com/br-automation-com/mapp-Framework/releases/tag/V1.3.0 Framework - Description mapp AlarmX: Added a Python script to be able to export/import the alarm configuration to/from Excel mapp Axis / Cockpit: Enhanced the Automatic Mode mapp View content Added configuration for SLO traces mapp Backup: Added visual feedback that a backup is in progress, so you cannot trigger another one Fixed the backup list so that it automatically refreshes when an automatic backup is generated, to include the new backup in the list mapp File: Added more feedback on the HMI to indicate if an invalid operation was attempted mapp Recipe: Fixed the popup that warns you that the default recipe is missing, so that it doesn't appear twice Improved the behavior of the recipe page up/down buttons The user is no longer permitted to delete the default recipe mapp Report: Added the ability to sort the file list on the HMI mapp UserX: Added a confirmation pop-up for deleting a user Added a visual indication that you cannot delete the Anonymous user Added a popup to inform users if they were automatically logged out |
|||||
| Version | Langue | Système d'exploitation | Date | Taille | Type | Téléchargement |
| 1.2.0.1 | * | 07/12/2022 | 49 Mo | EXE | AS4_TP_mappFramework_1.2.0.1.exe | |
| Description |
mapp Framework Github link: https://github.com/br-automation-com/mapp-Framework/releases/tag/V1.2.0 Framework - Description mapp Audit: Fixed the automatic archive implementation Made the automatic archive settings persistent mapp Axis / Cockpit: Reorganized the MoveVelocity parameter mapp Backup: Fixed permissions issue with create button if no backups existed yet on the file device Improved the behavior of the info box on the mapp View content Made the automatic backup settings persistent mapp File: Improved the state machine of the FIFO mapp Report: New framework component mapp UserX: Automatically refresh the UserX content if you import a user list mapp View: Improved some German translations and text visibility Added the new B&R logo for the boot logo Import Tool: Optimizations to reduce the file size of the .exe Changes to reduce the likelihood of the following two errors during import: "The process cannot access the file '...Visualizat.vis' because it is being used by another process." "Error adding , Operation failed 0" Miscellaneous: Unified tabs vs spaces implementation (tabs) Removed MachineGrp.mpcomgroup |
|||||
| Version | Langue | Système d'exploitation | Date | Taille | Type | Téléchargement |
| 1.1.0.1 | * | 05/09/2022 | 66 Mo | EXE | AS4_TP_mappFramework_1.1.0.1.exe | |
| Description |
mapp Framework The mapp Framework provides a universal starting point for mapp Technology. It is designed to streamline your implementation of mapp Services and mapp Axis by reducing the amount of application code that must be written by the application engineer. The Framework includes programming tasks and supporting configuration files with built-in best practices and application know-how. It is designed to be modular, so the user can easily add the specific parts that are relevant to the machine to an existing project. After installing the mapp Framework, view the documentation and revision history directly in the AS Help file at the following path: mapp Technology -> mapp Framework The mapp Framework is a community driven / open source resource. Input from the community is used to continually refine and improve the mapp Framework. It is not an official product from B&R. The Github repository which holds the Framework source project is available at the following link: https://github.com/br-automation-com/mapp-Framework Applications engineers can therefore suggest modifications or new functionality directly via Github. In this way, the mapp Framework is constantly evolving and improving via input from the community. The mapp Framework uses standard mapp components, and general questions about mapp should continue to be directed to 1st level / 2nd level support. However, since the Framework itself is a community driven resource, questions about the mapp Framework contents / design / documentation / etc should be sent directly to the following email address (NOT the Support Team): mappframework@br-automation.com |
|||||
| Version | Langue | Système d'exploitation | Date | Taille | Type | Téléchargement |
| 1.0.2 | * | 31/05/2022 | 59 Mo | EXE | AS4_TP_mappFramework_1.0.2.0.exe | |
| Description |
mapp Framework The mapp Framework provides a universal starting point for mapp Technology. It is designed to streamline your implementation of mapp Services and mapp Axis by reducing the amount of application code that must be written by the application engineer. The Framework includes programming tasks and supporting configuration files with built-in best practices and application know-how. It is designed to be modular, so the user can easily add the specific parts that are relevant to the machine to an existing project. After installing the mapp Framework, view the documentation and revision history directly in the AS Help file at the following path: mapp Technology -> mapp Framework The mapp Framework is a community driven / open source resource. Input from the community is used to continually refine and improve the mapp Framework. It is not an official product from B&R. The Github repository which holds the Framework source project is available at the following link: https://github.com/br-automation-com/mapp-Framework Applications engineers can therefore suggest modifications or new functionality directly via Github. In this way, the mapp Framework is constantly evolving and improving via input from the community. The mapp Framework uses standard mapp components, and general questions about mapp should continue to be directed to 1st level / 2nd level support. However, since the Framework itself is a community driven resource, questions about the mapp Framework contents / design / documentation / etc should be sent directly to the following email address (NOT the Support Team): mappframework@br-automation.com |
|||||