ACOPOSmulti inverter module, 44 A, AS, cold plate or pass-through mounting
X67 stepper motor module, I/O power supply 24 VDC ±25%, 4 motor connections, 1 A continuous current, 1.5 A peak current, NetTime function
industry, the B&R Education Network partnered with the Dr. D. Y. Patil Institute of Technology in Pimpri-Pune to organize the Open Automation Challenge 2024. The event paired engineering students with B&R mentors [...] innovative approach and application. The selected teams completed training on B&R's Automation Studio engineering software and other B&R technologies to finally execute their projects and bring their ideas to [...] their mentor assigned by B&R. The group of students participating in the challenge embarked on a two-week educational adventure that included project development and training on B&R Automation Studio and
about the hotel on the website - www.wyndhamgrandsalzburg.com B&R Headquarter B&R Industrial Automation, B&R Straße 1, 5142 Eggelsberg, Austria B&R is an innovative automation company with headquarters in [...] is a new concept designed for B&R’s customers, inspired by B&R’s worldwide annual Innovations Day. This spring, Innovations Tour will take place at the Hannover Messe where B&R will be present. Among others [...] things, you will see some of B&R’s most recent innovations, followed by a second day with hands-on workshops at the B&R Headquarters in Eggelsberg. On behalf of all participants, B&R has arranged direct flights
X67 universal mixed module, 1 input for evaluating full-bridge strain gauge, 24-bit, 4 digital inputs 24 VDC, sink, 1 digital output, 0.5 A, source, 1 digital output, 1 A, source
ACOPOSmicro inverter module, POWERLINK interface, 2x resolver, 24-64 VDC ±25% power supply, 2 motor connections, 8 A continuous current, 2 digital inputs 24 VDC, sink, can be used as trigger inputs, 1
Transponder 13.56 MHz, ISO 15693 and MIFARE Classic, read/write unit, mounting diameter 22.5 mm, USB cable length 1200 mm, IP65 protection.
Synchronous motor 8LS, self-cooling, construction type A, 400 VAC - Number of pole pairs: 4 - Nominal speed: 3000 rpm - Nominal torque: 11.600 Nm - Stall torque: 12.500 Nm - Centering diameter: 130.00
B&R develops function block for dynamic applications B&R continues to drive the development of vendor-independent communication with OPC UA . The company has developed a PLCopen function block that makes [...] fully networked factories," explains Karl Mayr, technical manager of automation software at B&R. That explains B&R's years of involvement in OPC Foundation working groups helping to advance the standard
COMAU and B&R assimilate robotics into machine control With the introduction of openROBOTICS, partners COMAU and B&R are opening up new dimensions of robotics integration for machinery and production lines [...] lines equipped with B&R automation components. "The customer simply selects the desired COMAU robot in the Automation Studio engineering environment," explains Walter Burgstaller, B&R's European sales director
请选择国家和语言