Transponder tag, red housing, read/write, 4150, 928-bit, 125 kHz
ACOPOSmulti3 SafeMOTION EnDat 2.2 Gen2 inverter module, 22 A, AS, wall mounting, optimized for applications with decentralized, computationally intensive open-loop and closed-loop control requirements
B&R process control with redundant servers, fieldbus networks and controllers Starting with Release 4.0, B&R's APROL process control system provides maximum protection against system failure. APROL allows [...] reliability and ensures consistent output quality. Redundancy with standard hardware For some time, B&R has provided the option of using standard components from the X20 control system to establish controller [...] redundancy. This eliminates the need for costly specialized hardware. Standard control computers from B&R's Automation PC series are also well-suited for constructing redundant server systems. Since the servers
B&R User Meeting in Shanghai points the way into the future In light of increasing pressure for end users and OEMs to implement "smart factory" solutions that merge automation and IT technology, B&R China's [...] automation suppliers, OEMs, end users and system integrators. Sustainable solutions Managing director of B&R China, Xiao Weirong, presented his vision of how industrial automation can respond to the challenges [...] solutions that include training, support and operations management." Equipped for the challenges to come B&R presented the APROL process control system – and its turnkey solutions for energy monitoring, condition
B&R introduces the mapp View HMI solution at the SPS IPC Drives B&R will be taking advantage of this year's SPS IPC Drives to introduce its new HMI solution – mapp View – showcasing for the very first [...] display at the B&R booth (Hall 7 / Booth 206) include a new generation of swing arm operator panels as well as innovative safety solutions involving intelligent light curtains. With mapp View, B&R opens up [...] multi-touch user interface are just some of the other highlights being presented. To round it all off, B&R will be introducing brand new safety concepts based on a network-integrated light curtain .
B&R Hypervisor saves space in mobile machines B&R now equips its PC for mobile machinery with B&R Hypervisor software. This enables it to serve simultaneously as both a high-performance controller and [...] makes more efficient use of available hardware resources. Option board for an external I/O connection B&R also offers a new option board for connecting external I/O modules or sensors in combination with [...] with three CAN POWERLINK interfaces and one real-time POWERLINK interface. Standardized communication B&R offers an option board with four additional Ethernet interfaces in order to further network the PC
global network of value-added partners. B&R Value Providers work seamlessly with B&R to bring our products and services to your door. They combine in-depth knowledge of B&R technology with a deep understanding [...] respond quickly, eliminate costly downtime and improve product quality. B&R, your partner when it comes to packaging Adaptive manufacturing B&R supports its customers with adaptive manufacturing solutions that [...] vision and digital twins for simulation are perfectly synchronized components. B&R's seamless automation With a complete solution, B&R offers everything needed for machine and system automation. The key is that
much: We've begun a very exciting journey and there's no end in sight. Machine vision by B&R Machine vision by B&R B&R has developed a machine vision solution from the ground up as an integral element of [...] camera is synchronized with axis movements with microsecond precision. The B&R lighting portfolio The B&R lighting portfolio B&R's lighting portfolio includes flexible light bars, ringlights and backlights [...] market is already spoiled for choice. Nevertheless, automation specialist B&R chose to launch its own portfolio of integrated lighting. B&R's machine vision expert, Andreas Waldl, explains why this was the only
2005 programmable I/O processor, 850 kB SRAM, 1.5 MB FlashPROM, 1 RS232 interface, 1 CAN interface, CAN: Electrically isolated, network-capable, max. 12 digital inputs 24 VDC, sink, max. 12 digital outputs
screen (resistive), 12 soft keys, 20 function keys and 92 system keys, 1 aPCI slot, 64 MB SDRAM, 256 kB SRAM CompactFlash slot (type I), ETH 10/100, RS232, 2xUSB, battery, metal housing, IP65 protection (front)
请选择国家和语言