Hannover Messe: New B&R portfolio with OPC UA over TSN At the Hannover Messe (Hall 9 / Booth D26), B&R will be the first to present an automation portfolio that speaks OPC UA over TSN. And with that, the [...] development both easier and more agile. The new B&R portfolio sets the stage for OEMs to start enjoying the benefits of the open standard today. Visitors to the B&R booth can dive into the world of OPC UA over [...] vendor and enjoy greater freedom in the design of their machines. Another exhibition highlight will be B&R's full integration of robotics in the machine control system. The unified communication standard OPC
B&R presents solutions for a new generation of energy at Smarter E Europe 2024 At Smarter E Europe 2024 from June 19-21 in Munich, Germany, B&R is showing how intelligent automation can address the new [...] challenges that come with widespread adoption of renewable energy. Visitors to Booth 490 in Hall B2 will see how B&R technology is helping to make green grids more reliable and deliver clean fuel to hard-to [...] produced with renewable energy. Automating a new generation Visitors to Booth 490 in Hall B2 will experience firsthand how B&R is helping lead the charge with this new generation of energy solutions – by optimizing
X20 digital output module, coated, 12 outputs, 24 VDC, 0.5 A, source, 1-wire connections
2x RS232, 4x USB 2.0, Smart Display Link/DVI-I, 1x ETH 10/100, 1x POWERLINK, 1x CAN, 1x X2X, 1024 kB SRAM, 24 VDC. (order screw clamp terminal block 0TB103.9 or cage clamp terminal block 0TB103.91 separately)
for 2x RS232, 4x USB 2.0, Smart Display Link/DVI-I, 1x ETH 10/100, 1x POWERLINK, 1x CAN, 1x X2X, 512 kB SRAM, 24 VDC. (order screw clamp terminal block 0TB103.9 or cage clamp terminal block 0TB103.91 separately)
unit, connections for 2x RS232, 4x USB 2.0, DVI-A, 1x ETH 10/100, 1x POWERLINK, 1x CAN, 1x X2X, 512 kB SRAM, 24 VDC. (order screw clamp terminal block 0TB103.9 or cage clamp terminal block 0TB103.91 separately)
inputs 24 V, optional for use for limit monitoring and position detection (counter functions, 20 kHz A/B/R evaluation), order 1x TB710 and 1x TB718 terminal blocks separately!
fitted to Parallel Port Button Holder DS1410E (parallel interface) - Included USB-iButton Adapter DS9490B is used for USB- interface (Pill must be changed)
X20 Compact-S PLC, ARM Cortex-A9-300, 128 MB DDR3 RAM, 16 kB FRAM, 1 GB onboard flash drive, 2 USB interfaces, 1 RS232 interface, 1 POWERLINK interface, 1 Ethernet interface 10/100BASE-T, can be expanded
请选择国家和语言