mapp Framework

DWL@DWL10000724404

Версия Язык
Операционная система
Дата
Размер
Тип Загрузка
6.5.0.3 * 06.03.2026 53 МБ EXE AS6_TP_mappFramework_6.5.0.3.exe
Описание mapp Framework

Now only on Github as a Community project, please open this link:
https://github.com/br-automation-community/mapp-Framework-6
Версия Язык
Операционная система
Дата
Размер
Тип Загрузка
1.5.0.0 * 03.04.2024 143 МБ EXE AS4_TP_mappFramework_1.5.0.0.exe
Описание mapp Framework

Github link:
https://github.com/br-automation-com/mapp-Framework/releases/tag/V1.5.0

Framework - Description

mapp Audit:
Improved the usability of the audit configuration dialog box

mapp Axis / Cockpit:
The AxisMgr template task is now not added to the software configuration, as opposed to before where it was automatically added but disabled

mapp File:
Improved the usability of the FIFO dialog box

mapp Recipe:
General reorganization and optimization to make the recipe system more robust and easier to extend

Import Tool:
Import the file device definitions depending on the AR version, in order to allow AR versions less than A4.91. For AR =A4.91, the file devices use USER_PATH.
Updated the import tool to allow mixing mapp versions starting with version 5.24 and beyond
Improved the error message if the import fails due to a previous git reset command
The import tool will now detect existing .vis files within sub-packages of the mapp View package, as opposed to only .vis files in the root directory

Misc:
Updated to the new mapp Framework logo
Версия Язык
Операционная система
Дата
Размер
Тип Загрузка
1.4.0.0 * 03.07.2023 139 МБ EXE AS4_TP_mappFramework_1.4.0.0.exe
Описание mapp Framework

Github link:
https://github.com/br-automation-com/mapp-Framework/releases/tag/V1.4.0

Framework - Description

VC4:
Added a new VC4 front end for all available framework components

mapp Axis / Cockpit:
Updated the reference file organization to make it easier to add additional axes
Updated the conditions to get into the READY state (checks if the Parameter and/or Configuration change option is used or not, and if so, wait until it is finished)
Separated the HomeRestorePos variable to make it easier to add additional axes
Added an alarm line to the mapp View front end

mapp PackML:
New framework component

mapp Recipe:
Improved the process for editing the default recipe names

mapp Report:
Bugfix - advanced reports were getting created as simple reports

Import Tool:
Updates to support the option for a VC4 front end
Automatically increase the stack size of task class 8
Bugfix - TrakMap was not importing correctly via the framework importer

Documentation:
Improved the German translation of the Help file
Версия Язык
Операционная система
Дата
Размер
Тип Загрузка
1.3.1.0 * 21.03.2023 94 МБ EXE AS4_TP_mappFramework_1.3.1.0.exe
Описание mapp Framework

Github link:
https://github.com/br-automation-com/mapp-Framework/releases/tag/v1.3.1

Framework - Description

mapp Axis:
Improved the documentation regarding the necessary requirements for converting from a pure virtual axis to a physical axis
New type member for v1.3 (ModeManual) was missing from the AxisMgr.typ file in the AxisTemplate

Miscellaneous:
Improved transfer robustness for the situation that you use transfer settings "Keep PV Values" along with "Installation during task operation"
Версия Язык
Операционная система
Дата
Размер
Тип Загрузка
1.3.0.0 * 01.03.2023 94 МБ EXE AS4_TP_mappFramework_1.3.0.0.exe
Описание mapp Framework

Github link:
https://github.com/br-automation-com/mapp-Framework/releases/tag/V1.3.0

Framework - Description

mapp AlarmX:
Added a Python script to be able to export/import the alarm configuration to/from Excel

mapp Axis / Cockpit:
Enhanced the Automatic Mode mapp View content
Added configuration for SLO traces

mapp Backup:
Added visual feedback that a backup is in progress, so you cannot trigger another one
Fixed the backup list so that it automatically refreshes when an automatic backup is generated, to include the new backup in the list

mapp File:
Added more feedback on the HMI to indicate if an invalid operation was attempted

mapp Recipe:
Fixed the popup that warns you that the default recipe is missing, so that it doesn't appear twice
Improved the behavior of the recipe page up/down buttons
The user is no longer permitted to delete the default recipe

mapp Report:
Added the ability to sort the file list on the HMI

mapp UserX:
Added a confirmation pop-up for deleting a user
Added a visual indication that you cannot delete the Anonymous user
Added a popup to inform users if they were automatically logged out
Версия Язык
Операционная система
Дата
Размер
Тип Загрузка
1.2.0.1 * 07.12.2022 49 МБ EXE AS4_TP_mappFramework_1.2.0.1.exe
Описание mapp Framework

Github link:
https://github.com/br-automation-com/mapp-Framework/releases/tag/V1.2.0

Framework - Description

mapp Audit:
Fixed the automatic archive implementation
Made the automatic archive settings persistent

mapp Axis / Cockpit:
Reorganized the MoveVelocity parameter

mapp Backup:
Fixed permissions issue with create button if no backups existed yet on the file device
Improved the behavior of the info box on the mapp View content
Made the automatic backup settings persistent

mapp File:
Improved the state machine of the FIFO

mapp Report:
New framework component

mapp UserX:
Automatically refresh the UserX content if you import a user list

mapp View:
Improved some German translations and text visibility
Added the new B&R logo for the boot logo

Import Tool:
Optimizations to reduce the file size of the .exe
Changes to reduce the likelihood of the following two errors during import:
"The process cannot access the file '...Visualizat.vis' because it is being used by another process."
"Error adding , Operation failed 0"

Miscellaneous:
Unified tabs vs spaces implementation (tabs)
Removed MachineGrp.mpcomgroup
Версия Язык
Операционная система
Дата
Размер
Тип Загрузка
1.1.0.1 * 05.09.2022 66 МБ EXE AS4_TP_mappFramework_1.1.0.1.exe
Описание mapp Framework

The mapp Framework provides a universal starting point for mapp Technology. It is designed to streamline your implementation of mapp Services and mapp Axis by reducing the amount of application code that must be written by the application engineer. The Framework includes programming tasks and supporting configuration files with built-in best practices and application know-how. It is designed to be modular, so the user can easily add the specific parts that are relevant to the machine to an existing project.

After installing the mapp Framework, view the documentation and revision history directly in the AS Help file at the following path: mapp Technology -> mapp Framework

The mapp Framework is a community driven / open source resource. Input from the community is used to continually refine and improve the mapp Framework. It is not an official product from B&R.
The Github repository which holds the Framework source project is available at the following link: https://github.com/br-automation-com/mapp-Framework
Applications engineers can therefore suggest modifications or new functionality directly via Github. In this way, the mapp Framework is constantly evolving and improving via input from the community.

The mapp Framework uses standard mapp components, and general questions about mapp should continue to be directed to 1st level / 2nd level support. However, since the Framework itself is a community driven resource, questions about the mapp Framework contents / design / documentation / etc should be sent directly to the following email address (NOT the Support Team):
mappframework@br-automation.com
Версия Язык
Операционная система
Дата
Размер
Тип Загрузка
1.0.2 * 31.05.2022 59 МБ EXE AS4_TP_mappFramework_1.0.2.0.exe
Описание mapp Framework

The mapp Framework provides a universal starting point for mapp Technology. It is designed to streamline your implementation of mapp Services and mapp Axis by reducing the amount of application code that must be written by the application engineer. The Framework includes programming tasks and supporting configuration files with built-in best practices and application know-how. It is designed to be modular, so the user can easily add the specific parts that are relevant to the machine to an existing project.

After installing the mapp Framework, view the documentation and revision history directly in the AS Help file at the following path: mapp Technology -> mapp Framework

The mapp Framework is a community driven / open source resource. Input from the community is used to continually refine and improve the mapp Framework. It is not an official product from B&R.
The Github repository which holds the Framework source project is available at the following link: https://github.com/br-automation-com/mapp-Framework
Applications engineers can therefore suggest modifications or new functionality directly via Github. In this way, the mapp Framework is constantly evolving and improving via input from the community.

The mapp Framework uses standard mapp components, and general questions about mapp should continue to be directed to 1st level / 2nd level support. However, since the Framework itself is a community driven resource, questions about the mapp Framework contents / design / documentation / etc should be sent directly to the following email address (NOT the Support Team):
mappframework@br-automation.com
Loading
Вернутся к списку

Укажите страну и язык

B&R Logo