Panel PC 900 multi-touch: The new flagship system from B&R
1" to 19", Panel PC 900 single-touch systems provide full compatibility with the previous device generation with respect to screen resolution and dimensions. Fanless Many Panel PC 900 variants can be operated [...] advantage of state-of-the-art processors – up to and including Intel® Core™ i7 – the new Panel PC 900 with multi-touch functionality offers the absolute highest level of total computing power. Combining [...] versatile than ever, even offering full compatibility with the previous device generation. The Panel PC 900 takes full advantage of the state-of-the-art projected capacitive touch screen also used in the Automation