connection cable - Type A - type B connector - 1.8 m 5CAUSB.0050-00 USB 2.0 connection cable - Type A - type B connector - 5 m 5CAUSB.0075-00 USB 2.0 connection cable - Type A - type B connector - 7.5 m 5CAUSB [...] 5CAUSB.0100-00 USB 2.0 connection cable - Type A - type B connector - 10 m 5E9000.29 Transponder 125 kHz, read/write unit, installation diameter 22.5 mm, USB attachment cable length 800 mm, IP65 protection (front)
as the highest demands on quality and reliability led SEMITOOL to B&R, whose products are now being used in a variety of ways. With B&R Industrial PCs from the APC series and servo drives from the ACOPOS [...] expansion of their manufacturing capacities in the heart of Europe. Together with other local suppliers, B&R provides state-of-the-art technology and fast-paced innovation to help the machines from this Alpine [...] production of an in-house product series at the Salzburg location for a new semiconductor process, B&R technology is being used in SEMITOOL machines all over the world.
Bios DWL@DWL10000075468
Zertifikat DWL@DWL10000569993
and supported by all of the necessary certifications. About B&R B&R has its head-office at Pune, Maharashtra and four other offices in India. B&R is fully equipped to cater to your application, supply and [...] Automation Studio software development environment, B&R is constantly redefining the future of automation engineering. The global headquarters of B&R as well as the manufacturing center is at Eggelsberg [...] from the automotive sector. A highlight of the exhibition was a seminar held by Ninad Deshpande of B&R, in which he addressed the concerns of industrial specialists and automotive plant owners with regard
B&R at the 2013 SPS IPC Drives trade fair in Nuremberg This year's SPS IPC Drives trade fair in Nuremberg will be taking place November 26–28, 2013. B&R will be taking advantage of the opportunity offered [...] 110 and 206. Two main topics are on the B&R agenda this year: maximizing scalability and minimizing response time. Unprecedented scalability With Scalability+, B&R is establishing a new philosophy for [...] of the machine without having to make compromises along the way. A new series of compact controllers B&R has developed a whole new series of hardware components that further enhances the interoperability
2005 digital input module, 16 inputs 24 VDC, 1.2 ms, sink/source, 4 electrically isolated input groups, order 1x terminal block TB170 separately!
POWERLINK/Ethernet connection cable, RJ45 to RJ45, 30 m
X20 digital signal module, 4 digital inputs, 24 VDC, 4 digital outputs, 24 VDC, 0.1 A, oversampling I/O functions, time-triggered I/O functions, NetTime function
X20 digital signal module, 4x IO-Link master V1.1, 4 digital channels configurable as inputs or outputs, 3-wire connections, NetTime function
请选择国家和语言