• 网站
  • 模块号
  • 序列号
登录
登录为用户名登出
载入中...
中文

Please choose your country:

B&R Logo

Groundbreaking innovations in automation

16.10.2012
BuR_SPS IPC Drives

B&R at the 2012 SPS IPC Drives in Nuremberg

This year's SPS IPC Drives will be taking place from the 27th to the 29th of November 2012 in Nuremberg. At this leading trade fair for industrial automation systems and components, B&R's entire product range will be on display at their nearly 1000 m² booth (Hall 7, Booth 206). The spotlight will be on the latest developments from this highly innovative global leader in the field of automation technology. These innovations will open up new opportunities for machine and system manufacturers to build and strengthen their competitive edge.

New B&R Box PC with 3rd generation Intel® Core™ i technology

Users can expect extreme versatility and cost advantages from B&R's robust and reliable line of industrial PCs, including the new Automation PC 910. At the heart of this powerful industrial PC you'll find the latest 3rd generation Intel® Core™ i technology. Core™ i3, Core™ i5 and Core™ i7 CPUs with up to four cores, paired with the newly released QM77 Express chipset, provide the ultimate in state-of-the-art industrial computing performance.

APROL EnMon optimizes energy efficiency

B&R has introduced an all-new energy monitoring solution – APROL EnMon. Helping users implement ISO 50001, this new innovation also provides improved energy efficiency, which means reduced costs and increased competitiveness. In stand-alone operation or integrated in an existing APROL process control system, this solution supports a process of continual improvement by measuring and evaluating all relevant energy consumption data.

Automation Studio 4 supercharges development with sustainable efficiency

In spite of ever increasing product complexity, "Smart Engineering" with Automation Studio 4 helps cut development costs and accelerate time-to-market. The next generation of B&R's development environment provides decisive advantages. For one, it allows you to develop automation solutions with unprecedented efficiency.

Automation Studio 4 is also equipped with revolutionary new features that support optimum development and series production of modular machines in varying configurations. These include complete software modularization, a graphical hardware configuration tool and communication via OPC-UA as well as open interfaces between Automation Studio 4 and various design and simulation software.

In addition, Automation Runtime provides optimal multi-core utilization and supports simultaneous use of multiple operating systems (MultiOS) on a single hardware platform.

CPU redundancy from B&R – Absolutely reliable and cost-efficient

In the past, a failsafe system with redundant processors was a cost-prohibitive solution for many applications. 通过贝加莱X20系统提供并集成在Automation Studio 4开发环境中的处理器冗余,即使机器自动化传统领域中较小的应用现在也可以选用具有成本效益的高可用性系统。The communication protocol used for B&R's redundancy solution is the high-performance POWERLINK real-time fieldbus.

Decentralized drive technology from B&R for optimum use of available space

The ACOPOSmulti65m motor-mounted servo drive with IP65 protection is an innovative addition to B&R's modular ACOPOSmulti drive system. It melds with the motor to form a configurable and easy-to-connect mechatronic servo drive unit with integrated safe motion functions and openSAFETY to deliver power right where it is needed on the machine. This saves valuable space in the control cabinet and, even more importantly, advances the development of decentralized machine architectures.

New milestone in integrated safety

At the 2012 SPS IPC Drives, B&R will be presenting a further milestone for integrated safety technology.

These outstanding highlights will be featured at the B&R booth in a comprehensive exhibition of notable innovations spanning all areas of automation – including brand new developments for operation and HMI as well as robust components and systems for mobile automation.

关于贝加莱

贝加莱是一家私有化公司,总部位于奥地利,并在世界各地设有办事处。作为工业自动化领域的全球领导者,贝加莱结合先进的工程技术经验,为广泛的行业客户提供机械与过程自动化,运动控制,HMI和集成安全技术的完整解决方案。凭借工业现场总线通信标准POWERLINK和openSAFETY以及强大的Automation Studio软件开发环境,贝加莱正在不断地重新定义未来的自动化工程。受简化流程并超越客户预期承诺驱使的创新精神确保贝加莱始终处于工业自动化前沿。

更多信息,请访问www.br-automation.com

在重印本新闻稿时,请发送副本至:

Bernecker + Rainer Industrie-Elektronik Ges.m.b.H.
Corporate Communications
B&R Strasse 1
A-5142 Eggelsberg

BuR_SPS IPC Drives
Download
Download
Ejemplo
Share
This site uses cookies to enable a better customer experience. By continuing to browse the site you are agreeing to our use of cookies. Please find more information about cookies in our Data privacy statement.