• Site
  • Model Numarası
  • Seri Numarası
Üye Girişi
Aktif KullanıcıKullanıcı AdıÇıkış
Yükleniyor...
B&R Logo

Unmatched efficiency with high-speed diverters

02.21.2018
PR SPS Messe 2017
B&R will be showing how the high-speed diverters of its flexible ACOPOStrak transport system can significantly increase the effectiveness of production lines at the Hannover Messe in Hall 9, Booth D26.

B&R presents flexible transport system at Hannover Messe

B&R's new flexible transport system is designed to deliver ultimate production effectiveness – from mass production down to batches of one. Playing a pivotal role in making this possible are the system's purely electromagnetic diverters, which are able to divide and merge product flows at full production speed. B&R will be presenting its transport system from April 23-27 at the Hannover Messe in Hall 9, Booth D26.

Seamless connectivity

The B&R booth will also showcase how OPC UA TSN makes it possible to implement advanced manufacturing concepts with seamless connectivity from the field level up to ERP systems. Another Industrial IoT highlight will be B&R's Orange Box solution. This custom hardware/software package makes it easy to tap into the data of digitally isolated brownfield equipment so it can be utilized by higher-level systems.

Industrial PC premiere

B&R will be presenting a new generation of compact industrial PCs for the first time at the 2018 Hannover Messe. The PCs offer high performance and an extended array of options for connecting display units.

PR SPS Messe 2017
Download
Download
Ejemplo
Share
Um Ihnen benutzerdefinierte Einstellungen auf br-automation.com bereitstellen zu können, speichert B&R Informationen über Ihren Besuch in sogenannten Cookies. Durch die Nutzung dieser Webseite erklären Sie sich mit der Verwendung von Cookies einverstanden. Informationen über den Einsatz von Cookies erhalten Sie in unserer Veri Koruma Bildirimi.