• Site
  • Model Numarası
  • Seri Numarası
Üye Girişi
Aktif KullanıcıKullanıcı AdıÇıkış
Yükleniyor...
B&R Logo

Record number of participants at the B&R User Meeting in Salzburg

10.05.2013
BuR User Meeting 2013
275 participants from machine and plant engineering companies took advantage of the opportunity to find out more about exciting new B&R innovations at the User Meeting in Salzburg.

Workshops and a company exhibition stimulate interactive communication

275 participants from machine and plant engineering companies took advantage of the opportunity to learn firsthand about highly innovative automation solutions at this two-day event. With specialized lectures and interactive workshops, B&R was able to provide detailed information covering all areas of industrial automation – from small machine controllers to complex process control systems.

An interactive program with great diversity

In twelve blocks of presentations, 27 B&R speakers, 20 external experts and B&R customers presented participants with a wide range of information. Ten expert workshops also held during the meeting were a big hit as well. Comprehensive product-independent topic areas such as optimizing engineering workflows, increasing efficiency through simulation and the advantages of integrated safety technology were handled with the help of concrete application examples. "Participants really enjoyed the interactive format," says Hermann Obermair, sales Manager at B&R Austria, with satisfaction. "Not only did they take advantage of the opportunity to ask questions, but they also provided valuable input from the field."

Firsthand product information

Of course, many new developments were on the agenda, not just from B&R, but also from other manufacturers whose products can be integrated in B&R automation solutions via IO-Link or POWERLINK or used in safety solutions via openSAFETY.

During breaks, many participants also took the opportunity to visit the informative company exhibition directly at the venue in order to see hardware products and B&R software tools live in action as well as to discuss specific topics with industry experts.

Innovative real-world solutions

Many successful applications using B&R technology were on display, but an overview of diverse applications from various areas of the automotive industry was especially impressive. The autobahn tunnel through the Pfänder mountain near Bregenz was presented as an example of an automation solution distributed over a wide area in harsh environmental conditions. This solution has proven to be highly resistant to failure and allows systems from other manufacturers connected with ease. A detailed presentation of solutions and applications related to power generation and conversion focused directly on wind power.

Valuable feedback

"Participants at the B&R User Meeting aren't just at the receiving end of information," states Obermaier, "they also help direct the topics by contributing interactively to discussions. This provides valuable feedback that shows us how the market is developing and ensures that we are able to offer solutions that meet everyone's needs."

About B&R

B&R is a privately owned company with headquarters in Austria and offices all around the world. As a global leader in industrial automation, B&R combines state-of-the-art technology with advanced engineering to provide customers in virtually every industry with complete solutions for machine and process automation, motion control, HMI and integrated safety technology. With industrial fieldbus communication standards like POWERLINK and openSAFETY as well as the powerful Automation Studio software development environment, B&R is constantly redefining the future of automation engineering. The innovative spirit that keeps B&R at the forefront of industrial automation is driven by a commitment to simplifying processes and exceeding customer expectations.

For more information, visit www.br-automation.com.

When reprinting this press release, please send a copy to:

Bernecker + Rainer Industrie-Elektronik Ges.m.b.H.
Corporate Communications
B&R Strasse 1
A-5142 Eggelsberg
Austria, Europe

BuR User Meeting 2013
Download
Download
Ejemplo
Share
Um Ihnen benutzerdefinierte Einstellungen auf br-automation.com bereitstellen zu können, speichert B&R Informationen über Ihren Besuch in sogenannten Cookies. Durch die Nutzung dieser Webseite erklären Sie sich mit der Verwendung von Cookies einverstanden. Informationen über den Einsatz von Cookies erhalten Sie in unserer Veri Koruma Bildirimi.