• Site
  • Model Numarası
  • Seri Numarası
Üye Girişi
Aktif KullanıcıKullanıcı AdıÇıkış
Yükleniyor...
B&R Logo

Password-protected FTP access management for B&R systems

30.06.2014
BuR_PR13207_AS4_cmyk
Secure FTP access using usernames and passwords begins with encrypted storage of the passwords on the controller.

Highly secure direct access to the controller

All B&R controllers have an FTP server on board as a standard feature. A protection mechanism with integrated username and password management now makes accessing this server even more secure – without sacrificing ease of operation.

Whether it's to perform maintenance, supply a machine with new recipes or load a new function module, direct access to the controller is becoming increasingly important throughout the entire life cycle of production equipment. Developers of automation applications must maintain a high level of security when preparing the functions involved, while also ensuring that they are simple to learn and easy to operate.

Bringing IT functionality to automation

B&R draws on methods that have proven themselves in the realm of IT to help machine and system developers implement access security. User authentication is managed with usernames and passwords. Management of user data and assigned rights is integrated in Automation Studio. This data is stored on the runtime system in encrypted form to ensure seamless security. User management for FTP access to B&R systems allows an unlimited number of users to be assigned access rights. At runtime, up to eight different users can access the controller at the same time via FTP.

FTP access that is as secure as it is versatile is one of the many ways that B&R systems allow machine and system operators to react quickly and flexibly to new requirements.

About B&R

B&R is a privately owned company with headquarters in Austria and offices all around the world. As a global leader in industrial automation, B&R combines state-of-the-art technology with advanced engineering to provide customers in virtually every industry with complete solutions for machine and process automation, motion control, HMI and integrated safety technology. With industrial fieldbus communication standards like POWERLINK and openSAFETY as well as the powerful Automation Studio software development environment, B&R is constantly redefining the future of automation engineering. The innovative spirit that keeps B&R at the forefront of industrial automation is driven by a commitment to simplifying processes and exceeding customer expectations.

For more information, visit www.br-automation.com.

When reprinting this press release, please send a copy to:

Bernecker + Rainer Industrie-Elektronik Ges.m.b.H.
Corporate Communications
B&R Strasse 1
A-5142 Eggelsberg
Austria, Europe

BuR_PR13207_AS4_cmyk
Download
Download
Ejemplo
Share
Um Ihnen benutzerdefinierte Einstellungen auf br-automation.com bereitstellen zu können, speichert B&R Informationen über Ihren Besuch in sogenannten Cookies. Durch die Nutzung dieser Webseite erklären Sie sich mit der Verwendung von Cookies einverstanden. Informationen über den Einsatz von Cookies erhalten Sie in unserer Veri Koruma Bildirimi.