• Site
  • Model Numarası
  • Seri Numarası
Üye Girişi
Aktif KullanıcıKullanıcı AdıÇıkış
Yükleniyor...
B&R Logo

APROL – High availability at all levels

09.09.2013
Aprol Redundanz_final_CMYK
B&R's process control system, APROL, allows standard components to be constructed into high-availability systems at four different levels: Fieldbus networks, controllers, runtime servers and operator stations.

B&R process control with redundant servers, fieldbus networks and controllers

Starting with Release 4.0, B&R's APROL process control system provides maximum protection against system failure. APROL allows redundant systems to be set up at four different levels: fieldbus networks, controllers, runtime servers and operator stations. If the active system fails, an identical system running in parallel takes over all of its tasks. This prevents production downtime, improves process reliability and ensures consistent output quality.

Redundancy with standard hardware

For some time, B&R has provided the option of using standard components from the X20 control system to establish controller redundancy. This eliminates the need for costly specialized hardware. Standard control computers from B&R's Automation PC series are also well-suited for constructing redundant server systems. Since the servers hold not only historical archives but also critical applications such as the real-time database and the alarm and trend servers, their failure would have severe consequences.

Changeover within a few milliseconds

The primary and secondary controllers or servers exchange data constantly via a redundancy link. Should the primary unit fail, the powerful real-time Ethernet POWERLINK provides a fast and seamless transition to the secondary controller within a few milliseconds.

APROL allows operator stations, which are typically redundant, to be designed using standard components. With POWERLINK, B&R offers flexible options for redundant fieldbus systems. APROL also makes it possible to implement fieldbus redundancy using third-party systems. Configuration options can be used to enable or disable redundancy.

About B&R

B&R is a privately owned company with headquarters in Austria and offices all around the world. As a global leader in industrial automation, B&R combines state-of-the-art technology with advanced engineering to provide customers in virtually every industry with complete solutions for machine and process automation, motion control, HMI and integrated safety technology. With industrial fieldbus communication standards like POWERLINK and openSAFETY as well as the powerful Automation Studio software development environment, B&R is constantly redefining the future of automation engineering. The innovative spirit that keeps B&R at the forefront of industrial automation is driven by a commitment to simplifying processes and exceeding customer expectations.

For more information, visit www.br-automation.com.

When reprinting this press release, please send a copy to:

Bernecker + Rainer Industrie-Elektronik Ges.m.b.H.
Corporate Communications
B&R Strasse 1
A-5142 Eggelsberg
Austria, Europe

Aprol Redundanz_final_CMYK
Download
Download
Ejemplo
Share
Um Ihnen benutzerdefinierte Einstellungen auf br-automation.com bereitstellen zu können, speichert B&R Informationen über Ihren Besuch in sogenannten Cookies. Durch die Nutzung dieser Webseite erklären Sie sich mit der Verwendung von Cookies einverstanden. Informationen über den Einsatz von Cookies erhalten Sie in unserer Veri Koruma Bildirimi.