X20 safe digital mixed module, 8 safe type A digital inputs, configurable input filter, 4 pulse outputs, 24 VDC, 4 safe type A digital outputs, 24 VDC, 3 A, OSSD
Accessory terminal block, 3-pin, screw clamp terminal block 6 mm²
Motor cable, length 10 m, 5x 0.75 mm², 4-pin male connector on the motor side, can be used in cable drag chains, UL listed
X2X Link attachment cable, open-ended on one side, 5 m
X20 stepper motor module, 1 motor connection, 1 A continuous current, 1.2 A peak current, 4 digital inputs 24 VDC, sink, configurable as incremental encoder, NetTime function
ACOPOS P3 hybrid motor cable, length 20 m, 4x 1.5 mm² + 2x 0.75 mm² + 2x 0.30 mm² + 2x 2x 0.15 mm², 13-pin female speedtec hybrid motor connector size 1, can be used in cable drag chains
Connector 300 VDC - 10-pin female - Cage clamp terminal block - Protected against vibration by the screw flange
MES-D.A.CH association event with B&R For two days at the end of January in Eggelsberg, Upper Austria, everything will revolve around Manufacturing Execution Systems (MES). B&R was the host of the second event [...] a chance to experience production at B&R firsthand. They were impressed by how advanced the implementation of factory-wide Industry 4.0 strategies really are at B&R. [...] Industry 4.0. The boundaries of the automation pyramid are dissolving Peter Gucher – General Manager at B&R – noted in his introductory statement that further optimization of production processes are for the
system The enhanced crossover Operating System (exOS) makes it possible to use any Linux code within B&R systems. This gives machine builders unprecedented freedom in the design of their automation solutions [...] easily integrated in the machine application. With the enhanced crossover connection between Linux and B&R's real-time operating system, Automation Runtime, software developers can write, compile and debug [...] Linux code using their preferred tool, such as Eclipse or Visual Studio, and then import it into the B&R system as an exOS package. This lets them use Automation Studio as a central engineering tool. Managing
Swiss Exchange (ABBN) and Nasdaq Stockholm (ABB). B&R , a division of ABB Group, is a global leader in industrial automation headquartered in Austria. B&R combines state-of-the-art technology with advanced [...] openSAFETY as well as its Automation Studio software, B&R is constantly redefining the future of automation engineering. The innovative spirit that keeps B&R at the forefront of industrial automation is driven [...] This integration builds on Machine Automation’s legacy within ABB, including the 2017 acquisition of B&R – now the core of the division. ABB is a global technology leader in electrification and automation
Välj land och språk