• Strona www
  • Numer modelu
  • Numer seryjny
Login
Zalogowany jako UżytkownikWyloguj się
Ładowanie...
B&R Logo

CNC cylindrical grinder by Fermat Machine Tool – Automated by B&R

08.30.2013
BuR_PR13159_Fermat
Fermat Machine Tool developed its BUB E 40/1000 CNC grinder for high-precision universal grinding applications – with automation technology from B&R.

High precision, flexibility and intuitive operation coming to EMO 2013

Integrated HMI, CNC and servo technology from B&R combined with high-performance POWERLINK communication – all of these things have helped Fermat Machine Tool boost the performance of its machines. Not only that, but they have given developers at Fermat the freedom and power to fully utilize their hard-earned grinding expertise. These characteristics will be on display in September at EMO 2013, the world’s leading exhibition for metalworking taking place in Hanover, Germany, when Fermat Machine Tool, s.r.o. introduces its new CNC cylindrical grinder.

Intuitive, flexible and low-maintenance

"The open CNC control allowed us to implement our own processing cycles, supported by graphical visualizations. As a result, the operator doesn’t need any knowledge of CNC programming," says Ondřej Zoubek, director of R&D at Fermat Machine Tool. "The B&R control system allows us to offer our customers a grinder as flexible as it is reliable – with maximum performance and minimum maintenance."

High precision and smooth migration

Fermat has been able to achieve an extremely high surface grinding precision of 1 µm. These high-quality results were made possible by ACOPOSmulti drives from B&R equipped with an external linear measurement system from Heidenhain. An open NC program interpreter ensures extremely smooth migration from the previous system.

Designed for high-precision axial and surface grinding with a fixed or oscillating table, the BUB E 40/1000 CNC grinder is suitable for the production of workpieces in both small and medium size batches.

About B&R

B&R is a privately owned company with headquarters in Austria and offices all around the world. As a global leader in industrial automation, B&R combines state-of-the-art technology with advanced engineering to provide customers in virtually every industry with complete solutions for machine and process automation, motion control, HMI and integrated safety technology. With industrial fieldbus communication standards like POWERLINK and openSAFETY as well as the powerful Automation Studio software development environment, B&R is constantly redefining the future of automation engineering. The innovative spirit that keeps B&R at the forefront of industrial automation is driven by a commitment to simplifying processes and exceeding customer expectations.

For more information, visit www.br-automation.com.

When reprinting this press release, please send a copy to:

Bernecker + Rainer Industrie-Elektronik Ges.m.b.H.
Corporate Communications
B&R Strasse 1
A-5142 Eggelsberg
Austria, Europe

BuR_PR13159_Fermat
Download
Download
Ejemplo
Share
Nasza strona internetowa używa plików cookies (tzw. ciasteczka) w celach statystycznych, reklamowych oraz funkcjonalnych. Dzięki nim możemy indywidualnie dostosować stronę do twoich potrzeb. Każdy użytkownik może zaakceptować pliki cookies albo ma możliwość wyłączenia ich w przeglądarce, dzięki czemu nie będą zbierane żadne informacje. Więcej informacji znajdziesz w Privacy Policy.