Please choose country and language:

Controller redundancy with POWERLINK

B&R is setting new standards with its redundancy solution for X20 control systems, a breakthrough that now allows the advantages of high availability to be enjoyed by smaller applications at much less cost. B&R's solution is based on standard X20 controllers that can be reconfigured at any time with features that reduce downtime using the Automation Studio software development environment. This eliminates the need for specialized redundancy controllers, which are generally very expensive due the small quantities produced. Engineering effort is reduced to declaring the PLC a redundant unit and configuring communication parameters or failure criteria.

With B&R's solution, one controller provides active control, while a second controller runs in the background in standby mode. All network functions are monitored continuously so that when the time comes, the backup controller can quickly take over all of the active PLC's functions. Whichever controller becomes active always uses the same IP address as its predecessor. The switching time of the system is a mere two task cycles – so all of this takes place in a matter of a few milliseconds.

This redundancy solution is powered by the high-performance, real-time Ethernet POWERLINK communication protocol. An independent high-speed fiber optic redundancy link is used to continually synchronize all important data – the I/O image, for example – between the active and inactive controllers.

About B&R

B&R is a privately owned company with headquarters in Austria and offices all around the world. As a global leader in industrial automation, B&R combines state-of-the-art technology with advanced engineering to provide customers in virtually every industry with complete solutions for machine and process automation, motion control, HMI and integrated safety technology. With industrial fieldbus communication standards like POWERLINK and openSAFETY as well as the the powerful Automation Studio software development environment, B&R is constantly redefining the future of automation engineering. The innovative spirit that keeps B&R at the forefront of industrial automation is driven by a commitment to simplifying processes and exceeding customer expectations.

For more information, please visit www.br-automation.com.

When publishing this press release, please send a copy to:

Bernecker + Rainer Industrie-Elektronik Ges.m.b.H.
Corporate Communications
B&R Strasse 1
A-5142 Eggelsberg

Please choose country and language:

B&R Logo