------------------------------------------------------------------ File: Readme.txt Version: 1.7 Date: 18.09.2013 Description: B&R Windows CE5.0 MP40/50 ------------------------------------------------------------------ As follow you will find a short description and information to the version of the delivered software. ------------------------------------------------------------------ GENERAL ------------------------------------------------------------------ ------------------------------------------------------------------ Version V1.7 / 18.09.2013 / PAM ------------------------------------------------------------------ Error corrections - The driver of the illuminated ring key sometimes stucks under heavy system load. The problem has been fixed by a new keyboard driver. - Performance problems at screen updates in B&R VNC Viewer with 32 bit color depth. The performance has been improved by a new version of the B&R VNC Viewer and by a new TCP window size of 8k (32k before). - The B&R Task Manager caused 100% CPU load for measurement of the CPU load (but did not show that). Changes - Updated with B&R VNC Viewer 4.2 - Updated with B&R Task Manager 2.3 - Updated with B&R HMI Diagnostics 1.50 - Updated with B&R Registry Editor 3.6 - Updated with B&R Set Date & Time 1.6.1 - The following Microsoft Windows CE updates have been included: 1. Windows CE 5.0 Update 130831_2013M08 2. Windows CE 5.0 Update 130731_2013M07 3. Windows CE 5.0 Update 130630_2013M06 4. Windows CE 5.0 Update 130331_2013M03 5. Windows CE 5.0 Update 130131_2013M01 6. Windows CE 5.0 Product Update Rollup, December 31, 2012 ------------------------------------------------------------------ Version V1.6 / 22.06.2011 / PAM ------------------------------------------------------------------ Changes - Support for displaying PNG images on Internet Explorer added. - Updated with B&R Configuration Manager 3.5 - Updated with B&R HMI Diagnostics 1.30 - Updated with B&R Screen Capture 1.1 - Updated with B&R Screensaver 2.4 - Updated with B&R Server 3.8.1 - Updated with B&R Task Manager 2.1.2 - Updated with B&R VNC Viewer 4.0.1 - Updated with PVI 3.0.2 ------------------------------------------------------------------ Version V1.5 / 30.09.2010 / PAM ------------------------------------------------------------------ Changes - Support Mobile Panel 40/50 with new flash chip. (old flash chip is still supported) - Added B&R Task Manager to the TCAR image. - Missing B&R Thin Client Control Panel Applet added to the TCAR Image. - Added B&R Screensaver SSBlank 1.3 - Updated with B&R Task Manager 2.1.1 - Updated with B&R HMI Diagnostics 1.20 - Updated with B&R VNC Viewer 3.13 - Updated with PVI 3.0.0.3116 - Updated with TouchScreen Applet 3.8 - Updated with Configuration Manager 3.4 - Updated with CleanScreen 3.0 - Updated with AutoRun 5.2 - Added SQL Compact component (replacement for SQL Mobile) - Added Compact Framework 3.5 component (replacement for Compact Framework 2.0) - The following Microsoft Windows CE updates have been included: 1. Windows CE 5.0 Update 100731_2010M07 2. Windows CE 5.0 Update 100331_2010M03 3. Windows CE 5.0 Update 100228_2010M02 4. Windows CE 5.0 Product Update Rollup, December 31, 2009 ------------------------------------------------------------------ Version V1.4.1 / 30.03.2010 / HOH ------------------------------------------------------------------ Changes - Added all available "Locales" to the TCAR image. ------------------------------------------------------------------ Version V1.4 / 28.10.2009 / KEP ------------------------------------------------------------------ Changes - Added the servers FTP, Web, File, Telnet, RAS and SNTP to the TCAR image. - Added all available "Locales". - Added B&R AutoRun V5.0. - Added B&R HMI Diagnostics V1.10. - Added The B&R Automation Device Interface V1.30. - Added the B&R VNC Viewer 3.11. - Added the PVI V3.0.0.3015. - B&R Zip V1.00 has been added to the Pro- and ProPlus images. - B&R Task Manager V2.1 has been added to the Pro- and ProPlus images. - Added B&R Screen Capture V1.00. - Added the B&R Configuration Manager V3.3. - Added B&R Registry Editor V3.5. - The following Microsoft Windows CE updates have been included: 1. Windows CE 5.0 Update 090731_2009M07 2. Windows CE 5.0 Update 090630_2009M06 3. Windows CE 5.0 Update 090531_2009M05 4. Windows CE 5.0 Update 090430_2009M04 5. Windows CE 5.0 Update 090228_2009M02 6. Windows CE 5.0 Update 090131_2009M01 7. Windows CE 5.0 Product Update Rollup, December 31, 2008 ------------------------------------------------------------------ Version V1.3 / 18.11.2008 / KEP ------------------------------------------------------------------ Error corrections - ID 192448: B&R VNC-Viewer does not support ZLib compression. VNC-Viewer stopps if ZLib compression is used. The problem has been fixed by B&R VNC-Viewer 3.7.0. - ID 179375: Windows CE 5.0/6.0 > SNTP time synchronization does not work. The Windows CE SNTP server did not accept STNP client requests until the server did connect to an NTP server. The SNTP server now uses the local real-time clock. - ID 184620: Missing SIP at Power On dialog. A „Power On“ password cannot be entered using a SIP. Added a button which opens the SIP. - ID 191435: PVI Manager stops if a MP40/50 is conntected to a M68k CPU. The problem has been fixed by PVI V3.0.0.3104. Changes - The serial port S11 was added as COM1. - Added the control panel applet „Server“ V3.7. - Added the Registry Editor V3.4. - Added the VNC viewer 3.7. - The following Microsoft Windows CE updates have been included: 1. Windows CE 5.0 Update 080930_2008M09 2. Windows CE 5.0 Update 080831_2008M08 3. Windows CE 5.0 Update 080731_2008M07 4. Windows CE 5.0 Update 080630_2008M06 5. Windows CE 5.0 Update 080531_2008M05 6. Windows CE 5.0 Update 080430_2008M04 7. Windows CE 5.0 Update 080331_2008M03 8. Windows CE 5.0 Update 080229_2008M02 ------------------------------------------------------------------ Version V1.2 / 10.03.2008 / KEP ------------------------------------------------------------------ Error corrections - ID 175940: The desktop name of the VNC server is shown with random characters. - ID 175930: Command line arguments are not used by VNC Viewer. - ID 175925: The RFB extension starts a process with wrong parameters. - ID 175910: The actuation of matrix keys is not always handled properly. - ID 175870: Memory mapped files are not supported. - ID 175875: The driver smsc911x.dll 3.3.0.0 does not support the ethernet-controller REV0.2. Starting with revision F0 the ethernet controller REV0.2 is used on the Mobile Panel. This controller is not supported by the driver V3.3.0.0. Because of this fact the driver was updated to version V3.4.0.0. Changes - Control Panel Applet Server updated to version 3.4. - B&R VNC Viewer updated to version 3.6.3. - SSFloat updated to version V1.2. - B&R Set Date & Time updated to version V1.6. - Screensaver runtime updated to version V2.1. - Control Panel Applet Screensaver updated to version V2.3. - B&R Registry Editor updated to V3.2. - Automation Device Interface updated to V1.22. - The default settings of the PVI demo have been changed. - The following Microsoft Windows CE updates have been included: 1. Windows CE 5.0 Update 080131_2008M01 2. Networked Media Device Feature Pack Product Update Rollup, December 31, 2007 3. Windows CE 5.0 Product Update Rollup, December 31, 2007 ------------------------------------------------------------------ Version V1.1 / 12.11.2007 / KEP ------------------------------------------------------------------ Error corrections - ID 167722: The "Connection" dialog box does not have a "Cancel" button. - ID 167722: The "Auto reconnect" function for the VNC viewer does not function correctly. - ID 167722: In some rare cases, it's possible that the colors are shown incorrectly on the MP40 via a VNC connection. - ID 164975: If multiple VNC Viewers are active at the same time, the values for handwheel, joystick and potentiometer are transferred multiple times. - ID 166890: If the "Render cursor locally" option is deactivated, then the VNC Viewer transfers the touch screen position in full screen mode incorrectly. - ID 167455: If a VNC connection is established successfully, then the Mobile Panel 40 display flickers. - ID 167335: A registry file could not be imported directly on the device. - ID 167115: In some rare cases, an update was interrupted with the error message "error after clearlock: 50580000". - ID 167055: On the MP40, the display is turned 180° when the "Advanced" dialog box in the Control Center is closed with OK without making a change. - ID 167425: The "Terminal Server Client Licenses" applet could not be used on QVGA devices. - ID 159725: If the display is rotated 90°, the TAB control navigation buttons disappear. Changes - ID 160360: The size of the Internet Explorer cache was increased. - ID 166680: PVI V2.6.0.3101 was integrated in the Pro and ProPlus image. - ID 165555: The "Disconnect Key" for the VNC Viewer is now preset to "not defined" (None). - ID 165555: The key assignments when delivered were revised. Refer to the "Configuration of the keys" section in the online help. - ID 165555: "B&R Set Date & Time" is no longer started automatically. - ID 166675: The "Small Keyboard" SIP was added. - "B&R Set Date & Time" was updated to V1.3. - "B&R AutoRun" was updated to V4.3. - The "B&R Automation Device Interface" was updated to V1.21. - The B&R VNC Viewer was updated to V3.5.0. - The size of the storage memories when delivered were increased. - The following Microsoft Windows CE updates were included: 1. Windows CE 5.0 Update 070930_2007M09 2. Windows CE 5.0 Update 070831_2007M08 3. Windows CE 5.0 Update 070731_2007M07 4. Windows CE 5.0 Update 070630_2007M06 5. Windows CE 5.0 Update 070531_2007M05 6. Windows CE 5.0 Update 070823_KB940981 ------------------------------------------------------------------ Version V1.0 / 26.07.2007 / KEP ------------------------------------------------------------------ - First Version. ------------------------------------------------------------------ Copyright (c) by B&R ------------------------------------------------------------------ Bernecker + Rainer Industrie-Elektronik Ges.m.b.H. B&R Straße 1 A - 5142 Eggelsberg Tel: +43 (0)7748/6586-0 Fax: +43 (0)7748/6586-26 Email: office@br-automation.com Web: http://www.br-automation.com ------------------------------------------------------------------