------------------------------------------------------------------ File: Readme.txt Version: V1.3 Date: 2011-12-06 Description: B&R Windows CE 6.0 APC620 + PPC700 X945 ------------------------------------------------------------------ Below you will find a short description and version information of the software. ------------------------------------------------------------------ GENERAL INFORMATION ------------------------------------------------------------------ This is the B&R Windows CE 6.0 version for B&R Automation PC 620 and B&R Panel PC 700 devices. ------------------------------------------------------------------ INSTALLATION ------------------------------------------------------------------ For further informations, see the Windows CE 6.0 help. The help can be downloaded from the B&R homepage www.br-automation.com. ------------------------------------------------------------------ Version V1.3 / 2011-12-06 / PAM ------------------------------------------------------------------ Attention! This image version is only released for X945 CPU boards! Fixes - The Backlight did not switch off in ScreenSaverBlank. Changes - Updated with Intel® Embedded Graphics Drivers (IEGD) 10.4 - Updated with B&R ADI 1.93. - Updated with B&R ADI SNMP Agent 1.1 - Updated with B&R Autorun 5.4.1 - Updated with B&R Configuration Manager 3.5 - Updated with B&R HMI Diagnostics 1.3 - Updated with B&R PVI 3.0.2 - Updated with B&R Screen Capture 1.1 - Updated with B&R ScreenSaverBlank 1.4.1 - Updated with B&R Server Applet 3.8.1 - Updated with B&R SetDateAndTime 1.6.1 - Updated with B&R Task Manager 2.1.3 - Updated with B&R Touch Applet 4.2.1 - Updated with B&R VNC Viewer 4.02 - Used CE 6.0 updates: * Windows Embedded CE 6.0 R3 * Winodws Embedded CE 6.0 Product Update Rollup 2010 * Windows Embedded CE 6.0 Update 110131_2011M01 * Windows Embedded CE 6.0 Update 110228_2011M02 * Windows Embedded CE 6.0 Update 110331_2011M03 * Windows Embedded CE 6.0 Update 110430_2011M04 * Windows Embedded CE 6.0 Update 110531_2011M05 * Windows Embedded CE 6.0 Update 110630_2011M06 * Windows Embedded CE 6.0 Update 110731_2011M07 * Windows Embedded CE 6.0 Update 110831_2011M08 (without KB2562821) * Windows Embedded CE 6.0 Update 110930_2011M09 * Windows Embedded CE 6.0 Update 111031_2011M10 ------------------------------------------------------------------ Version V1.2 / 2010-10-15 / PAM ------------------------------------------------------------------ Fixes - The COM E Interface did not work with the standard biossettings. - The Intel ATOM CPU was not recognized by the ProcessorInfo. Changes - Used CE 6.0 updates: * Windows Embedded CE 6.0 R3 * Winodws Embedded CE 6.0 Product Update Rollup 2009 * Windows Embedded CE 6.0 Update 100131_2010M01 * Windows Embedded CE 6.0 Update 100228_2010M02 * Windows Embedded CE 6.0 Update 100331_2010M03 * Windows Embedded CE 6.0 Update 100430_2010M04 * Windows Embedded CE 6.0 Update 100531_2010M05 * Windows Embedded CE 6.0 Update 100630_2010M06 * Windows Embedded CE 6.0 Update 100731_2010M07 * Windows Embedded CE 6.0 Update 100831_2010M08 * Windows Embedded CE 6.0 Update 100930_2010M09 - B&R HMI Diagnostics 1.2 added. - B&R Zip 1.0 added. - B&R ADI SNMP Agent 1.0 added. - Updated with B&R AutoRun 5.2 - Updated with B&R Control Center 1.40 - Updated with B&R PVI 3.0.0.3116 - Updated with B&R Registry Editor 3.5 - Updated with B&R Screen Capture 1.0.2 - Updated with B&R Screen Saver 2.4 - Updated with B&R Task Manager 2.1.1 - Updated with B&R Touch Screen 3.8 - Updated with B&R VNC Viewer 3.13 - The USB Drivers (EHCI_ICEG.DLL und USBDISK6.DLL) have been updated with all Microsoft QFEs up to july 2010 (Update 100731_2010M07). - Updated with Intel® Embedded Graphics Drivers (IEGD) 8.0.2 - Font Arial Bold Italic added. - Font Comic Sans MS Bold added. - Font Courier New Bold added. - Font Courier New Bold Italic added. - Font Courier New Italic added. - Font Impact added. - Font Times New Roman Bold added. - Font Times New Roman Bold Italic added. - Font Verdana Bold added. - Font Verdana Bold Italic added. - Font Verdana Italic added. - The Windows style was changed to standard. - The desktop wallpaper was removed. ------------------------------------------------------------------ Version V1.1 / 2009-08-04 / HOH ------------------------------------------------------------------ Fixes - A PS/2 mouse was not recognized. - In sporadic cases a CD/DVD-ROM drive was not mounted correctly. Changes - Support for X945 CPU Boards has been added. - The Intel 82562V Fast Ethernet Controller of the X945 CPU Boards was not supported by the included ethernet driver e100ce.dll. This driver has been replaced by a compatible e100.dll driver which supports the following Fast Ethernet Controllers: 82551ER, 82562GZ and 82562V - The Intel specific USB mass storage driver usbmsc_iceg.dll has been removed. This adapted driver is no longer needed. - The Intel specific driver usbdisk6_iceg.dll has been replaced by a B&R specific version of usbdisk6.dll. This driver has been modified by B&R to support several brands of USB memory sticks. - Updated with B&R ADI driver 1.92. - Updated with APC620/PPC700 CE6.0 BSP 1.10. - Updated with B&R VNC Viewer 3.11. - Updated with B&R Image Viewer 1.2.1. - Updated with B&R PVI 3.0.0.3113. - Updated with Windows Embedded CE 6.0 Update (April 2009). - Updated with Windows Embedded CE 6.0 Update (May 2009). - Updated with Windows Embedded CE 6.0 Update (June 2009). ------------------------------------------------------------------ Version V1.0 / 2009-06-05 / HOH ------------------------------------------------------------------ - First Version. ------------------------------------------------------------------ Copyright (c) by B&R ------------------------------------------------------------------ Bernecker + Rainer Industrie-Elektronik Ges.m.b.H. B&R Straße 1 A - 5142 Eggelsberg Tel: +43 (0)7748/6586-0 Fax: +43 (0)7748/6586-26 Email: office@br-automation.com Web: http://www.br-automation.com ------------------------------------------------------------------