------------------------------------------------------------------ File: Readme.txt Version: V5.3 Date: 10.10.2008 Description: WinCE5.0 PP100/200,MP100/200 ------------------------------------------------------------------ This file contains a short description and version information regarding the delivered software. ------------------------------------------------------------------ GENERAL INFORMATION ------------------------------------------------------------------ ------------------------------------------------------------------ Version V5.3 10/10/2008 / KEP ------------------------------------------------------------------ Changes - The screensaver SSFloat V1.2 has been added. - The screensaver SSBlank V1.3 has been added. - SetDateAndTime V1.6 has been added. - The control panel applet Server V3.5 has been added. - The control panel applet Screensaver V2.30 has been added. - The screensaver runtime V2.10 has been added. - The B&R Registry Editor V3.40 has been added. - The following Microsoft updates have been added: * Windows CE 5.0 Update 080831_2008M08 * Windows CE 5.0 Update 080731_2008M07 * Windows CE 5.0 Update 080630_2008M06 * Windows CE 5.0 Update 080531_2008M05 * Windows CE 5.0 Update 080430_2008M04 * Windows CE 5.0 Update 080331_2008M03 * Windows CE 5.0 Update 080229_2008M02 * Windows CE 5.0 Update 080131_2008M01 * Networked Media Device Feature Pack Product Update Rollup, December 31, 2007 * Windows CE 5.0 Product Update Rollup, December 31, 2007 * Windows CE 5.0 Update 070823_KB940981 * Windows CE 5.0 Update 070930_2007M09 * Windows CE 5.0 Update 070831_2007M08 * Windows CE 5.0 Update 070731_2007M07 * Windows CE 5.0 Update 070630_2007M06 * Windows CE 5.0 Update 070531_2007M05 * Windows CE 5.0 Update 070430_2007M04 * Windows CE 5.0 Update 070331_2007M03 * Windows CE 5.0 Update 070131_2007M01 * Windows CE 5.0 Update 070228_2007M02 * Windows CE 5.0 Product Update Rollup, December 31,2006 Error corrections ID 184620: "Missing SIP at Power-On password dialog." The Power-On password dialog can now be used with the SIP. ID 167425: "The Terminal Server Client Licenses applet can't be used on QVGA devices." The applet was adapted to the QVGA resolution. ID 159725: "Screen Rotate Bug" Dialogs using Tab controls will be drawn correctly after rotating the screen. ID 16036: "Internet Explorer doesn't download" The size of the cache has been adapted. ID 179375: "Windows CE 5.0/6.0 > SNTP time synchronization does not work." This problem has been corrected. ID 144980: "The 5MD900.USB2-00 does not work." This problem has been corrected. ID 152370: "Empty string in SETTINGS.REG crashes the system." AutoRun V4.6 has been added to correct this problem. ID 185740: "After a reboot the matrix keys doesn't work anymore." The Automation Device Interface V2.02 has been added to correct this problem. ------------------------------------------------------------------ Version V5.2 1/24/2006 / KEP ------------------------------------------------------------------ - Windows CE 5.0 Update 060731_2006M07 implemented. - Windows CE 5.0 Update 061031_2006M10 implemented. - Windows CE 5.0 Update 060831_2006M08 implemented. - Windows CE 5.0 Update 060930_2006M09 implemented. - Windows CE 5.0 Update 061031_2006M10 implemented. - The new START.DAT keywords ERRORMSG and SETDATEANDTIME are now supported by AutoRun.exe V3.1. - Added new program Set Date & Time V1.2. This program can be used to configure the SNTP service. - Added Server Applet V3.1. This new applet is a simple way to configure the RAS and SNTP servers. - ID 148875: Integrate MFC8.0 and ATL8.0 to support VS2005 projects Added Microsoft software libraries MFC8.0, ATL8.0, and MSVCRT8.0. - ID 149745: Add SNTP automatic client / SNTP server Added services "SNTP Automatic Updates" and "SNTP Server Synchronization". - ID 145540: Implement PVI 2.5.3.3002 PVI updated to version 2.5.3.3102. - ID 144465: CD-ROM change not recognized If a CD-ROM is changed, this won't be recognized and Explorer crashes. Problem corrected with QFE 060824_KB924154. - ID 140595: Windows CE device freezes when opening a help page in a zenOn 6.20/SP1 demo. Somtimes COPADATA zenOn crashed when opening a help page. Problem corrected with QFE 061005_KB925370. - ID 144675: Integrate the PVI ADI line Added the new PVI ADI line. - ID 144935: The task manager should not be opened when pressing CTRL+ALT+DEL. Function added. Please refer to the online help for additional information. ------------------------------------------------------------------ Version V5.1 7/27/2006 / KEP ------------------------------------------------------------------ - ID 144230: Sometimes the MCX is not initialized on the Mobile Panel - Keys does not work The Automation Device Interface 2.01 fixes this problem (see ID 138580) - ID 143945: Integration of the QFE package Update 060630_2006M06 This update has been integrated. - ID 142085: Integration of the QFE package "May 2006" This update has been integrated. - ID 14770: Remove LMemDebug LMemDebug was removed. - ID 139260: Telnet server enabled after restart If the Web server is enabled in the Server applet in the Control Panel, it and the Telnet server are active after restarting. This problem has been corrected. - ID 138890: Cannot create C++ MFC Smart Device applications with the B&R Windows CE 5.0 Power Panel SDK The error message "Invalid procedure call or argument" appeared when attempting to create a Visual C++ application with Visual Studio 2005 and the B&R Windows CE 5.0 Power and Mobile Panel 100/200 SDK 5.0. This problem have been corrected with Version 5.1 of the SDK. - ID 138580: ADI update Automation Device Interface 2.01 has been integrated. This version corrects the following problems: ID 137210: The B&R Control Center no longer recognizes the B&R Windows CE device if "Keyboard repeat" was disabled in the Control Panel. ID 127940: Error correction for key no. 121 - ID 135475: Function for cleaning the touch screen The "Screen cleaning" function has been implemented in the Touch Screen applet in the Control Panel. - ID 135470: INI files should be linked with PWord INI files are now linked to PWord. - ID 131915: "Remote Desktop Active X Control Interface" not completely implemented The "Windows RDP Control" has been replaced by teh "ActiveX RDP Control". - ID 128990: SCRSAVE.EXE should only be started once AUTORUN.EXE has ended. This behavior has been implemented. - ID 128545: Integration of the QFE package "Q3 2005" This update has been integrated. - ID 139850: Integration of Windows CE 5.0 update 060430_2006M04 This update has been integrated. - ID 128455: Saving the registry on restart The Configuration Manager applet in the Control Panel saves the registry before a restart. - ID 123895: Default interface for the PVI demo The serial interface has been changed to COM1. - ID 123890: The Server applet should enable the integrated server without restarting The Server applet in the Control Panel now enables and disables the server without needing to restart the B&R Windows CE device. - ID 135155: Windows CE for PP deletes Extended CMOS B&R Windows CE deletes the model number of an aPCI module in Slot 1. This problem has been corrected. ------------------------------------------------------------------ Version V5.0 / 28.07.2005 / KEP ------------------------------------------------------------------ - First version. ------------------------------------------------------------------ Copyright (c) by B&R ------------------------------------------------------------------ Bernecker + Rainer Industrie-Elektronik Ges.m.b.H. B&R Strasse 1 A - 5142 Eggelsberg Tel.: +43 (0)7748/6586-0 Fax: +43 (0)7748/6586-26 Email: office@br-automation.com Web: http://www.br-automation.com ------------------------------------------------------------------