2012-01-24
A development computer [1] that must fulfill the following hardware requirements:
A target system [2] that must be one of the B&R automation devices released with Windows Embedded Standard 7:
with:
The development computer must be running one of the following operating systems:
and must have the following software installed:
Modify the the Windows Embedded Standard 7 image for your needs.
Please note: For images without time limit you have to order a product key for OEM Activation from B&R.
For a detailed description of the Windows Embedded Standard 7 development process see:
Windows Embedded Standard 7
http://msdn.microsoft.com/en-us/library/ff795586(v=winembedded.0).aspx
You will find following topics on this page:
Additionally information can be found on the Microsoft Website here:
Developing with Windows Embedded Standard 7 Service Pack 1
http://www.microsoft.com/windowsembedded/en-us/develop/windows-embedded-standard-7-for-developers.aspx
Although this page is for Windows Embedded Standard 7 Service Pack 1 it references useful resources such as white papers, forums, blogs and FAQs:
Windows Embedded Standard 7 White Papers
http://www.microsoft.com/windowsembedded/en-us/develop/windows-embedded-standard-7-white-papers.aspx
Discussion on the tools such as Image Creation Editor (ICE), Image Based
Wizard (IBW) and etc for Windows Embedded Standard 7.
http://social.msdn.microsoft.com/Forums/en-US/quebectools/threads
Windows Embedded Standard Blog
http://blogs.msdn.com/b/embedded/
Windows Embedded Standard 7 Getting Started Technical FAQs
http://www.microsoft.com/windowsembedded/en-us/develop/windows-embedded-standard-7-getting-started-questions.aspx
FAQ: Building and Customizing Images with Windows Embedded Standard 7
http://www.microsoft.com/windowsembedded/en-us/develop/windows-embedded-standard-7-building-customizing-images.aspx
You can also consult a Windows Embedded Standard Training from a Microsoft Training Partner that you can find here:
Windows Embedded Partner Search
http://www.microsoft.com/windowsembedded/en-us/partners/find-windows-embedded-partners.aspx
Windows Embedded Classroom Training
http://www.microsoft.com/windowsembedded/en-us/events/windows-embedded-classroom-training.aspx
[1] The development computer is the
computer where you install the Windows Embedded Standard 7 Toolkit.
[2] The target system is the
computer where you run Windows Embedded Standard 7.
[3] You can download and install Microsoft .NET
Framework from the Microsoft Web site
http://www.microsoft.com.
[4] You can download and install Microsoft
Core XML Services (MSXML) from the Microsoft Web site
http://www.microsoft.com.
[5] You can order the Windows Embedded Standard 7
Toolkit from B&R (B&R model number 0TP500.60). Note that a Toolkit with SP1 integrated is delivered.
Because SP1 is not yet released for B&R automation devices, you need also an
RTM Toolkit to build images without SP1.
You can receive an RTM Toolkit from B&R for free. The product key of the ordered
SP1 Toolkit is also valid for that.
[6] The B&R Windows Embedded Standard 7 BSP contains
all files specific for B&R automation devices and can be downloaded from the B&R
Web site http://www.br-automation.com.
[7] The Image Configuration Editor (ICE) is part of
the Windows Embedded Standard 7 Toolkit and can be used
to create or modify an answer file.
[8] The answer file defines all the files, packages and drivers
that the Windows Embedded Standard 7 image should contain. It can be used to
create a bootable setup medium that installs the image on a target system. Answer
files for B&R automation devices are included in the B&R
Windows Embedded Standard 7 BSP.
[9] You can download the B&R Windows Embedded Standard 7
Development Guide from the B&R Web site http://www.br-automation.com.