------------------------------------------------------------------ File: Readme.txt Version: V1.2 Date: 2010-10-15 Description: B&R Windows CE 6.0 PPC300 ------------------------------------------------------------------ Below you will find a short description and version information of the software. ------------------------------------------------------------------ GENERAL INFORMATION ------------------------------------------------------------------ This is the B&R Windows CE 6.0 version for B&R Panel PC 300 devices. ------------------------------------------------------------------ INSTALLATION ------------------------------------------------------------------ For further informations, see the Windows CE 6.0 help. The help can be downloaded from the B&R homepage www.br-automation.com. ------------------------------------------------------------------ Version V1.2 / 2010-10-15 / PAM ------------------------------------------------------------------ Fixes - Videos could not be played because necessary components were not included in the image. - Various USB flash drives did not work, including the B&R USB flash drive 5MMUSB.2048-01. Changes - Used CE 6.0 updates: * Windows Embedded CE 6.0 R3 * Winodws Embedded CE 6.0 Product Update Rollup 2009 * Windows Embedded CE 6.0 Update 100131_2010M01 * Windows Embedded CE 6.0 Update 100228_2010M02 * Windows Embedded CE 6.0 Update 100331_2010M03 * Windows Embedded CE 6.0 Update 100430_2010M04 * Windows Embedded CE 6.0 Update 100531_2010M05 * Windows Embedded CE 6.0 Update 100630_2010M06 * Windows Embedded CE 6.0 Update 100731_2010M07 * Windows Embedded CE 6.0 Update 100831_2010M08 * Windows Embedded CE 6.0 Update 100930_2010M09 - B&R HMI Diagnostics 1.2 added. - B&R Zip 1.0 added. - B&R ADI SNMP Agent 1.0 added. - Updated with B&R AutoRun 5.2 - Updated with B&R CleanScrean 3.0 - Updated with B&R Image Viewer 1.2.1 - Updated with B&R PVI 3.0.0.3116 - Updated with B&R Registry Editor 3.5 - Updated with B&R Screen Capture 1.0.2 - Updated with B&R Screen Saver 2.4 - Updated with B&R Task Manager 2.1.1 - Updated with B&R VNC Viewer 3.13 - The USB Drivers (EHCI.DLL und USBDISK6.DLL) have been updated with all Microsoft QFEs up to july 2010 (Update 100731_2010M07). - Component WMV/MPEG-4 Video Codec added. - Component Windows Media Technologies added. - Component ASX v1 and M3U File Support added. - Component ASX v2 File Support added. - Component ASX v3 File Support added. - Component NSC File Support added. - Component Windows Media Multicast and Multi-Bit Rate added. - Component Windows Media Streaming from Local Storage added. - Component Windows Media Streaming over HTTP added. - Component Windows Media Streaming over MMS added. - Font Arial Bold Italic added. - Font Comic Sans MS Bold added. - Font Courier New Bold added. - Font Courier New Bold Italic added. - Font Courier New Italic added. - Font Impact added. - Font Times New Roman Bold added. - Font Times New Roman Bold Italic added. - Font Verdana Bold added. - Font Verdana Bold Italic added. - Font Verdana Italic added. - The Windows style was changed to standard. - The desktop wallpaper was removed. ------------------------------------------------------------------ Version V1.1 / 2009-06-24 / HOH ------------------------------------------------------------------ Fixes - The Suspend/Resume feature of the Windows CE EHCI driver has been disabled due to an error of the CS5536 companion device. For further details see the "AMD Geode CS5536 Companion Device Silicon Revision B1 Specification Update" issue 56 "Stability Issues upon USB EHC Port Suspend in S0". - Updated with ELO touchscreen driver 2.00. The previous version of the the touchscreen driver could enter an endless loop trying to resynchronize after communication error. Symptoms ranged from communication failure to apparent system crash. - Updated with B&R control panel applet "Touchscreen" 3.7. This version does not reboot the device if the user cancels the control panel applet. - Updated with B&R control panel applet "Server" 3.7. This version fixes configuration problems of the SNTP service. - Updated with B&R registry editor 3.4. In rare cases an exception was thrown at the time the registry editor was closed. Changes - Execution time of large applications improved. - Component XML Mime Viewer added. - XML files associated with Internet Explorer. - Component PCL Printer Driver added. - Component Animation Control added. - All "Locales" added. - Used CE 6.0 updates: * Windows Embedded CE 6.0 Product Update Rollup 2008 * Windows Embedded CE 6.0 Update 090131_2009M01 * Windows Embedded CE 6.0 Update 090228_2009M02 * Windows Embedded CE 6.0 Update 090331_2009M03 * Windows Embedded CE 6.0 Update 090430_2009M04 * Windows Embedded CE 6.0 Update 090531_2009M05 - B&R Screen Capture 1.0 added. - Updated with B&R Task Manager 2.0.1. - Updated with B&R VNC Viewer 3.11. - Updated with B&R Image Viewer 1.2. - Updated with B&R PVI 3.0.0.3113. - Updated with B&R PVI Demo 3.00. - SNTP settings fixed: trustlocalclock = 0. - SDK: define BR_PPC300 added. - Updated with B&R ADI driver 1.21. - Updated with B&R AutoRun 4.8. The registry file parser now supports semicolons behind a registry value in SETTINGS.REG. - Updated with B&R control panel applet "Configuration Manager" 3.3. This version supports viewing of more than one control panel applet at the same time. - The USB drivers (EHCI.DLL and USBDISK6.DLL) have been updated with all Microsoft QFEs up to march 2009 (Update 090331_2009M03). - The hidden FAT file system now supports partitions with less than 16MB (FAT12, ID=0x11). ------------------------------------------------------------------ Version V1.0 / 2008-08-12 / HOH ------------------------------------------------------------------ - First Version. ------------------------------------------------------------------ Copyright (c) by B&R ------------------------------------------------------------------ Bernecker + Rainer Industrie-Elektronik Ges.m.b.H. B&R Straße 1 A - 5142 Eggelsberg Tel: +43 (0)7748/6586-0 Fax: +43 (0)7748/6586-26 Email: office@br-automation.com Web: http://www.br-automation.com ------------------------------------------------------------------