------------------------------------------------------------------ File: Readme.txt Version: V1.3 Date: 07.05.2008 Description: WinCE5.0 APC620,PPC700 ------------------------------------------------------------------ This file contains a short description and version information regarding the delivered software. ------------------------------------------------------------------ GENERAL INFORMATION ------------------------------------------------------------------ ------------------------------------------------------------------ Version V1.3 / 07.05.2008 / KEP ------------------------------------------------------------------ Changes - Added support for X855 CPU boards. - The Microsoft IDE driver ATAPI.DLL creates sporadic problems. This driver has been replaced by the Intel IDE driver ICHIDE.DLL. - The driver IEGD8.0.0 was added. This drivers supports the IOCTL SETPOWERMANAGEMENT. - DDI_JIGD.DLL 2008.03.26 hase been added. This driver supports the hiding of the mouse cursor. - The driver JInitBM.DLL has been removed. If PCI-Bus Mastering on the PCI-Slots is needed you have to enable this function in the BIOS. The default setting in the BIOS is "enabled". - Added ELO Touchscreen driver V1.16. This driver supports the function "Right mouse button click per time" and the timout of the calibration can be disabled. - Added PVI V2.6.0.3005. - Added SSFloat V1.2. - Added SSBlank V1.2. - Added AutoRun V1.4. - Added Screensaver Control Panel Applet V2.30. - Added Screensaver Runtime V2.10. - Added Process Monitor. - Added Key Extension. - Added VNC Viewer 3.6.3. - Added Set Date & Time V1.6. - Added Server Control Panel Applet V3.4. - Added Touchscreen Control Panel Applet V3.60. - Added Registry Editor V3.20. - Added ADI V1.81. Error corrections - ID160360: Internet Explorer doesn't download PDF files The problem has been fixed. - ID167425: The Terminal Server Client Licenses Control Panel Applet can't be operated in QVGA mode. The problem has been fixed. Windows CE Updates * Windows CE 5.0 Update 080229_2008M02 * Windows CE 5.0 Update 080131_2008M01 * Networked Media Device Feature Pack Product Update Rollup, December 31, 2007 * Windows CE 5.0 Product Update Rollup, December 31, 2007 * Windows CE 5.0 Update 070930_2007M09 * Windows CE 5.0 Update 070831_2007M08 * Windows CE 5.0 Update 070731_2007M07 * Windows CE 5.0 Update 070630_2007M06 * Windows CE 5.0 Update 070531_2007M05 * Windows CE 5.0 Update 070430_2007M04 * Windows CE 5.0 Update 070331_2007M03 * Windows CE 5.0 Update 070131_2007M01 * Windows CE 5.0 Update 070228_2007M02 * Windows CE 5.0 Product Update Rollup, December 31,2006 ------------------------------------------------------------------ Version V1.2 / 08/02/2007 / KEP ------------------------------------------------------------------ Important! Beginning with V1.2, the PS/2 mouse is no longer initialized during booting! To enable PS/2 mouse initialization, uncheck the "Disable PS/2 mouse detection" option in the B&R Control Center. - Set Date & Time 1.2 added. This program can be used to configure the SNTP service. - Updated Server applet to V3.1. This new applet is a simple way to configure the RAS and SNTP servers. - Updated AutoRun to V3.2. This version supports the START.DAT keywords ERRORMSG and SETDATEANDTIME. In addition, the notation "multi_sz:" is supported in multi-string format for registry keys. REG files can also be imported into the registry simply by double-clicking them. - A&P 147425: If no PS/2 mouse is connected, the APC620/PPC700 takes 5 seconds longer to boot PS/2 mouse initialization has been disabled. To re-enable this initialization, use the "Disable PS/2 mouse detection" option in the B&R Control Center. - A&P 152370: Empty string in SETTINGS.REG causing crash This problem has been solved by AutoRun V3.2. - A&P 148095: The version of the image should be saved in a registry key. The version of the image can now be read using the "BrVersion" registry key under the [HKEY_LOCAL_MACHINE\Ident] branch. The image version is also displayed in the Control Center. - A&P 149830: TIMESVC not working. The SNTP service isn't working. This problem has been corrected. - A&P 145545: Implementation of PVI 2.5.3.3002 PVI has been updated to V2.5.3.3102. - A&P 144675: Integrate the PVI ADI line The PVI ADI line has been integrated. - A&P 147200: Mouse cursor positioned, but no trigger via clicking. The touch driver has been updated to the version Elo® Serial Windows CE Embedded Driver Release Candidate 2. - A&P 152295: Network bridging. Added network bridging function. Select the "Enable network bridging (with DHCP)" option in the Control Center to start network bridging. - A&P 149745: Add SNTP automatic client / SNTP server Added functions "SNTP automatic client" and "SNTP server". - A&P 148875: Integrate MFC8.0 and ATL8.0 to support VS2005 projects Added Microsoft software libraries MFC8.0, ATL8.0, and MSVCRT8.0. - A&P 144935: The task manager should not be opened when pressing CTRL+ALT+DEL. Function added. Please refer to the online help for additional information. - A&P 140595: Windows CE device freezes when opening a help page in a zenOn 6.20/SP1 demo. Sometimes COPADATA zenOn crashed when opening a help page. Problem corrected with QFE 061005_KB925370. ------------------------------------------------------------------ Version V1.1 / 5/15/2006 / KEP ------------------------------------------------------------------ - A&P 143945: Integration of the QFE package Update 060630_2006M06 This update has been integrated. - A&P 146205: Implementierung des IEGD 5.1 The Intel® Embedded Graphics driver package for Microsoft Windows CE 5.0 version 5.1 has been integrated. - A&P 142085: Integration of the QFE package "May 2006" This update has been integrated. - A&P 14770: Remove LMemDebug LMemDebug was removed. - A&P 139950: Optimizing available memory in slot 0 Shifting system DLLs to Slot 1 gained new free memory in slot 0 (own process). - A&P 139420: Update Elo driver for APC620, PPC700 image to V1.13 The Elo driver V1.13 has been integrated. - A&P 139260: Telnet server enabled after restart If the Web server is enabled in the Server applet in the Control Panel, it and the Telnet server are active after restarting. This problem has been corrected. - A&P 138580: ADI update Automation Device Interface 1.51 has been integrated. - A&P 135475: Function for cleaning the touch screen The "Screen cleaning" function has been implemented in the Touch Screen applet in the Control Panel. - A&P 135470: INI files should be linked with PWord INI files are now linked to PWord. - A&P 131915: "Remote Desktop Active X Control Interface" not completely implemented The "Windows RDP Control" has been replaced by teh "ActiveX RDP Control". - A&P 129865: The ATAPI driver being used doesn't support DMA transfers. The Microsoft ATAPI driver with DMA support has been implemented. - A&P 128545: Integration of the QFE package "Q3 2005" This update has been integrated. - A&P 139850: Integration of Windows CE 5.0 update 060430_2006M04 This update has been integrated. - A&P 128455: Saving the registry on restart The Configuration Manager applet in the Control Panel saves the registry before a restart. - A&P 123895: Default interface for the PVI demo The serial interface has been changed to COM1. - A&P 123890: The Server applet should enable the integrated server without restarting The Server applet in the Control Panel now enables and disables the server without needing to restart the B&R Windows CE device. ------------------------------------------------------------------ Version V1.0 / 12/14/2005 / KEP ------------------------------------------------------------------ - First version. ------------------------------------------------------------------ Copyright (c) by B&R ------------------------------------------------------------------ Bernecker + Rainer Industrie-Elektronik Ges.m.b.H. B&R Strasse 1 A - 5142 Eggelsberg Tel.: +43 (0)7748/6586-0 Fax: +43 (0)7748/6586-26 Email: office@br-automation.com Web: http://www.br-automation.com ------------------------------------------------------------------