• Site web
  • Référence produit
  • Numéro de série
Identification
Identifié sous le nom Nom d'utilisateurDéconnexion
Chargement en cours...
B&R Logo

Groundbreaking innovations in automation

16.10.2012
BuR_SPS IPC Drives
C'est sur le Stand 206, Hall 7, du salon SPS IPC Drives 2012, que B&R présentera ses innovations révolutionnaires pour tous les domaines de l'automatisation industrielle.

B&R at the 2012 SPS IPC Drives in Nuremberg

This year's SPS IPC Drives will be taking place from the 27th to the 29th of November 2012 in Nuremberg. At this leading trade fair for industrial automation systems and components, B&R's entire product range will be on display at their nearly 1000 m² booth (Hall 7, Booth 206). The spotlight will be on the latest developments from this highly innovative global leader in the field of automation technology. These innovations will open up new opportunities for machine and system manufacturers to build and strengthen their competitive edge.

New B&R Box PC with 3rd generation Intel® Core™ i technology

Users can expect extreme versatility and cost advantages from B&R's robust and reliable line of industrial PCs, including the new Automation PC 910. At the heart of this powerful industrial PC you'll find the latest 3rd generation Intel® Core™ i technology. Core™ i3, Core™ i5 and Core™ i7 CPUs with up to four cores, paired with the newly released QM77 Express chipset, provide the ultimate in state-of-the-art industrial computing performance.

APROL EnMon optimizes energy efficiency

B&R has introduced an all-new energy monitoring solution – APROL EnMon. Helping users implement ISO 50001, this new innovation also provides improved energy efficiency, which means reduced costs and increased competitiveness. In stand-alone operation or integrated in an existing APROL process control system, this solution supports a process of continual improvement by measuring and evaluating all relevant energy consumption data.

Automation Studio 4 supercharges development with sustainable efficiency

In spite of ever increasing product complexity, "Smart Engineering" with Automation Studio 4 helps cut development costs and accelerate time-to-market. The next generation of B&R's development environment provides decisive advantages. For one, it allows you to develop automation solutions with unprecedented efficiency.

Automation Studio 4 is also equipped with revolutionary new features that support optimum development and series production of modular machines in varying configurations. These include complete software modularization, a graphical hardware configuration tool and communication via OPC-UA as well as open interfaces between Automation Studio 4 and various design and simulation software.

In addition, Automation Runtime provides optimal multi-core utilization and supports simultaneous use of multiple operating systems (MultiOS) on a single hardware platform.

CPU redundancy from B&R – Absolutely reliable and cost-efficient

In the past, a failsafe system with redundant processors was a cost-prohibitive solution for many applications. With processor redundancy provided by the B&R X20 System and integrated in the Automation Studio 4 development environment, high availability systems are now a cost-effective option even for smaller applications in the classic areas of machine automation. The communication protocol used for B&R's redundancy solution is the high-performance POWERLINK real-time fieldbus.

Decentralized drive technology from B&R for optimum use of available space

The ACOPOSmulti65m motor-mounted servo drive with IP65 protection is an innovative addition to B&R's modular ACOPOSmulti drive system. It melds with the motor to form a configurable and easy-to-connect mechatronic servo drive unit with integrated safe motion functions and openSAFETY to deliver power right where it is needed on the machine. This saves valuable space in the control cabinet and, even more importantly, advances the development of decentralized machine architectures.

New milestone in integrated safety

At the 2012 SPS IPC Drives, B&R will be presenting a further milestone for integrated safety technology.

These outstanding highlights will be featured at the B&R booth in a comprehensive exhibition of notable innovations spanning all areas of automation – including brand new developments for operation and HMI as well as robust components and systems for mobile automation.

A propos de B&R

B&R Automation est une entreprise financièrement indépendante dont le siège social est basé en Autriche. Son réseau international d’agences lui permet d’être au plus près de ses clients le monde entier. Comptant parmi les leaders de l’automatisation industrielle, l’entreprise offre des solutions à la pointe de la technologie ainsi qu’une ingénierie de haut niveau. Elle fournit à ses clients des solutions complètes, qu’il s’agisse d’automatisation de process, de technologies de contrôle et d’entraînement, ou encore de visualisation. Ses solutions pour la communication industrielle, avec notamment POWERLINK et le standard ouvert openSAFETY, optimisent les performances, et son environnement de développement logiciel Automation Studio préfigure l’ingénierie du futur. Avec ses solutions innovantes, B&R Automation établit de nouveaux standards dans le monde des automatismes, simplifie les process et va au-delà des attentes de ses clients.

Pour plus d'informations, visitez notre site www.br-automation.com

En cas de réimpression de ce communiqué de presse, merci de transmettre une copie à

Bernecker + Rainer Industrie-Elektronik Ges.m.b.H.
Corporate Communications
B&R Strasse 1
A-5142 Eggelsberg

BuR_SPS IPC Drives
Download
Download
Ejemplo
Share
This site uses cookies to enable a better customer experience. By continuing to browse the site you are agreeing to our use of cookies. Please find more information about cookies in our Data privacy statement.