Please choose country and language:

Experience automation highlights firsthand

At the 2013 B&R User Meeting, which is taking place March 12-13 in Salzburg, participants will once again have the chance to experience the latest highlights in industrial automation firsthand. Ad-free product information straight from the various development departments, application reports from users and the possibility to speak with both customers using B&R technology as well as experts from various industries – these are the aspects that give the B&R User Meeting its special flair.

During this two-day event, B&R will be offering an informative program for those interested in technical information related to machine and system manufacturing – from small machine controllers to complex process control systems. B&R speakers, B&R customers and other well-known industry experts will be on-hand to talk about current trends in industrial automation, such as: Optimizing the engineering workflow, increasing overall efficiency using simulation, the advantages of integrated safety technology, the latest communication standards for automation industries and potential benefits of condition and energy monitoring.

In response to overwhelming requests, discussions with industry experts will be offered in groups at the User Meeting 2013 in addition to the main program. This mix of panel discussions and workgroups will be complemented by several practical tasks.

The User Meeting is also a great chance for participants to speak with industry experts during breaks. You can also check out B&R's wide range of hardware and software tools live and in action.

Participants will once again be invited to tour B&R headquarters in Eggelsberg, which is set to include a few new surprises this year.

A propos de B&R

B&R Automation est une entreprise financièrement indépendante dont le siège social est basé en Autriche. Son réseau international d’agences lui permet d’être au plus près de ses clients le monde entier. Comptant parmi les leaders de l’automatisation industrielle, l’entreprise offre des solutions à la pointe de la technologie ainsi qu’une ingénierie de haut niveau. Elle fournit à ses clients des solutions complètes, qu’il s’agisse d’automatisation de process, de technologies de contrôle et d’entraînement, ou encore de visualisation. Ses solutions pour la communication industrielle, avec notamment POWERLINK et le standard ouvert openSAFETY, optimisent les performances, et son environnement de développement logiciel Automation Studio préfigure l’ingénierie du futur. Avec ses solutions innovantes, B&R Automation établit de nouveaux standards dans le monde des automatismes, simplifie les process et va au-delà des attentes de ses clients.

Pour plus d'informations, visitez notre site www.br-automation.com

En cas de réimpression de ce communiqué de presse, merci de transmettre une copie à

Bernecker + Rainer Industrie-Elektronik Ges.m.b.H.
Corporate Communications
B&R Strasse 1
A-5142 Eggelsberg

Please choose country and language:

B&R Logo