Please choose country and language:

An anniversary celebration at B&R Switzerland

Last year, the Swiss subsidiary of the Austrian automation supplier B&R celebrated their 25-year anniversary. Since being founded in the spring of 1987, many well-known Swiss companies from a wide range of industries have relied on B&R's first-class products and technologies. "Our goal is to be the top partner for innovative solutions for machine manufacturers in all industries," says Paolo Salvagno, managing director of B&R Industrie-Automation AG in Switzerland.

Customers are constantly profiting from B&R's know-how as automation specialists, especially when it comes to complex tasks. The development work done by customers is made easier by the top performance, integrated intelligence, easy programming and excellent diagnostic features that are available in connection with Ethernet POWERLINK. "Our philosophy – offering the entire spectrum of automation including drives, controllers, I/O modules, bus systems and visualization devices from a single source – has proven its value in Switzerland," states Salvagno.

As a country with a high-priced economy, Swiss industry has always been forced to secure their position by placing a strong emphasis on innovation and precision. For this reason, many component suppliers see Switzerland as a test market for their new products. This is one reason why B&R opened up a subsidiary in this exciting market early on.

In August 2010, a subsidiary office was opened in Biel with a focus on sales, training and support. Since 2011, the Swiss subsidiary has been home to an in-house hardware development department for motion control. Like all B&R subsidiaries, B&R Switzerland stands out thanks to the excellent quality of their products, and also because of the excellent support provided by highly-qualified technicians.

B&R's Swiss subsidiary has now grown to a team of 35 employees. B&R is also among the front ranks of Swiss automation providers in terms of volume. "Thanks to pioneering solutions for complex automation tasks, we have always been successful in gaining new customers," says Salvagno. B&R Switzerland is confident of continued growth with existing customers as well as new customers, including those in new markets such as the Far East.

A propos de B&R

B&R Automation est une entreprise financièrement indépendante dont le siège social est basé en Autriche. Son réseau international d’agences lui permet d’être au plus près de ses clients le monde entier. Comptant parmi les leaders de l’automatisation industrielle, l’entreprise offre des solutions à la pointe de la technologie ainsi qu’une ingénierie de haut niveau. Elle fournit à ses clients des solutions complètes, qu’il s’agisse d’automatisation de process, de technologies de contrôle et d’entraînement, ou encore de visualisation. Ses solutions pour la communication industrielle, avec notamment POWERLINK et le standard ouvert openSAFETY, optimisent les performances, et son environnement de développement logiciel Automation Studio préfigure l’ingénierie du futur. Avec ses solutions innovantes, B&R Automation établit de nouveaux standards dans le monde des automatismes, simplifie les process et va au-delà des attentes de ses clients.

Pour plus d'informations, visitez notre site www.br-automation.com

En cas de réimpression de ce communiqué de presse, merci de transmettre une copie à

Bernecker + Rainer Industrie-Elektronik Ges.m.b.H.
Corporate Communications
B&R Strasse 1
A-5142 Eggelsberg

Please choose country and language:

B&R Logo