Por favor elija país e idioma:

Conozca las novedades en automatización de primera mano

At the 2013 B&R User Meeting, which is taking place March 12-13 in Salzburg, participants will once again have the chance to experience the latest highlights in industrial automation firsthand. Ad-free product information straight from the various development departments, application reports from users and the possibility to speak with both customers using B&R technology as well as experts from various industries – these are the aspects that give the B&R User Meeting its special flair.

During this two-day event, B&R will be offering an informative program for those interested in technical information related to machine and system manufacturing – from small machine controllers to complex process control systems. B&R speakers, B&R customers and other well-known industry experts will be on-hand to talk about current trends in industrial automation, such as: Optimizing the engineering workflow, increasing overall efficiency using simulation, the advantages of integrated safety technology, the latest communication standards for automation industries and potential benefits of condition and energy monitoring.

In response to overwhelming requests, discussions with industry experts will be offered in groups at the User Meeting 2013 in addition to the main program. This mix of panel discussions and workgroups will be complemented by several practical tasks.

The User Meeting is also a great chance for participants to speak with industry experts during breaks. You can also check out B&R's wide range of hardware and software tools live and in action.

Participants will once again be invited to tour B&R headquarters in Eggelsberg, which is set to include a few new surprises this year.

Acerca de B&R

B&R es una compañía de capital privado con sede en Austria y oficinas en todo el mundo. Como líder mundial en automatización industrial, B&R combina la tecnología de vanguardia con una avanzada ingeniería para proporcionar a los clientes de prácticamente cualquier industria soluciones completas para la automatización de máquinas y procesos, control de movimiento, HMI y tecnología de seguridad integrada. Con estándares industriales de comunicación de bus de campo como POWERLINK y openSAFETY, además del potente entorno de desarrollo de software Automation Studio, B&R está constantemente redefiniendo el futuro de la automatización. El espíritu innovador que mantiene a B&R al frente de la automatización industrial está impulsado por el compromiso de simplificar los procesos y superar las expectativas del cliente.

Para más información, visite www.br-automation.com

Si vuelve a imprimir esta nota de prensa, envíe una copia a:

Bernecker + Rainer Industrie-Elektronik Ges.m.b.H.
Corporate Communications
B&R Strasse 1
A-5142 Eggelsberg

Por favor elija país e idioma:

B&R Logo